<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックQuestion regarding using TPM channel for the TPM external clock input</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-regarding-using-TPM-channel-for-the-TPM-external-clock/m-p/163919#M10165</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with MC9S08SG32 part.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The spec indicates that you can utilize a TPM channel as the input for the TPM external clock signal.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This part allows TPM channels to be routed to different pins.&amp;nbsp; In the case of TPM1C0, it may be routed to either PTC0 or PTA0.&lt;/P&gt;&lt;P&gt;If I configure TPM1C0 to use PTC0 and use TPM1C0 for the external clock, will the external clock signal also be present on the alternate pin for this channel (PTA0)?&amp;nbsp; I ran the test and it looks like it is present on both pins.&amp;nbsp; Is there any method to restrict the signal to a single pin?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 May 2012 20:45:19 GMT</pubDate>
    <dc:creator>mcu_guy2525</dc:creator>
    <dc:date>2012-05-16T20:45:19Z</dc:date>
    <item>
      <title>Question regarding using TPM channel for the TPM external clock input</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-regarding-using-TPM-channel-for-the-TPM-external-clock/m-p/163919#M10165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with MC9S08SG32 part.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The spec indicates that you can utilize a TPM channel as the input for the TPM external clock signal.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This part allows TPM channels to be routed to different pins.&amp;nbsp; In the case of TPM1C0, it may be routed to either PTC0 or PTA0.&lt;/P&gt;&lt;P&gt;If I configure TPM1C0 to use PTC0 and use TPM1C0 for the external clock, will the external clock signal also be present on the alternate pin for this channel (PTA0)?&amp;nbsp; I ran the test and it looks like it is present on both pins.&amp;nbsp; Is there any method to restrict the signal to a single pin?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 May 2012 20:45:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-regarding-using-TPM-channel-for-the-TPM-external-clock/m-p/163919#M10165</guid>
      <dc:creator>mcu_guy2525</dc:creator>
      <dc:date>2012-05-16T20:45:19Z</dc:date>
    </item>
    <item>
      <title>Re: Question regarding using TPM channel for the TPM external clock input</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-regarding-using-TPM-channel-for-the-TPM-external-clock/m-p/163920#M10166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, and welcome to the forum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since TCLK is a lower priority, alternate pin function to TPM1CH0, it would be intuitive that TCLK should follow the the repositioning of the channel pin - is this what you have observed?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, this would seem to be at odds with the datasheet, in Table 2.1.&amp;nbsp; Here, TCLK is shown to be associated with PTA0 only, as an Alt 3 priority.&amp;nbsp; What functionality have you observed for the PTA0 pin,&amp;nbsp;after PTC0 becomes the TPM1C0 channel pin?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Perhaps you should generate a Service Request directly with Freescale, to have the matter clarified.&amp;nbsp; If the datasheet does&amp;nbsp;contain an error or ambiguity, this can be corrected&amp;nbsp;for a future release of the document.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 May 2012 22:34:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-regarding-using-TPM-channel-for-the-TPM-external-clock/m-p/163920#M10166</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2012-05-17T22:34:56Z</dc:date>
    </item>
  </channel>
</rss>