<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Bootloader and Vector redirection(NVOPT_INIT) bean issue.</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-and-Vector-redirection-NVOPT-INIT-bean-issue/m-p/163621#M10105</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is something I was looking for, thanks for your response. However, my application still doesn't start up(it is a serial comm interrupt based application). This is what I am doing:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In Bootloader Vector.c:&lt;/P&gt;&lt;P&gt;ISR(AS1_InterruptTx)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; asm&lt;BR /&gt;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pshh&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ldhx&amp;nbsp;&amp;nbsp; #$DFD4 &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; jmp&amp;nbsp;&amp;nbsp;&amp;nbsp; DO_ISR&lt;BR /&gt;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;}&lt;BR /&gt;.......Similar for other vectors with different address...........&lt;/P&gt;&lt;P&gt;.....................................................................................................&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;void DO_ISR()&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; asm&lt;BR /&gt;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ldhx&amp;nbsp;&amp;nbsp; ,x&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; cphx&amp;nbsp;&amp;nbsp; #$FFFF &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; beq&amp;nbsp;&amp;nbsp;&amp;nbsp; DI1&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; jsr&amp;nbsp;&amp;nbsp;&amp;nbsp; ,x&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;DI1:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pulh&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; rti&lt;BR /&gt;&amp;nbsp; }&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;****************************Application Vector.c***********************************&lt;/P&gt;&lt;P&gt;I changed:&lt;/P&gt;&lt;P&gt;ISR(AS1_InterruptTx)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;...........&lt;/P&gt;&lt;P&gt;...........&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To:&lt;/P&gt;&lt;P&gt;void AS1_InterruptTx()&lt;BR /&gt;{&lt;/P&gt;&lt;P&gt;..........&lt;/P&gt;&lt;P&gt;..........&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;****************************************************************************************&lt;/P&gt;&lt;P&gt;Apart from that, I have kept Vectors at default place ie 0xFFC4 and I have redirected Vector table in Application code to 0xDFC4.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The value of NVPROT_INIT being 0xDE and NVOPT_INIT being 0x7E. Although this conflicts with what should be for Application code (NVOPT = 0x3E for redirection), but we can not overite to this registers as they are protected. However, whenever an interrupt comes it goes to vector table located at 0xFFC4 which further sends it to 0xDFC4.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Logically&amp;nbsp; this seems to be a convincing solution from what all I was trying, however it doesn't seem to work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Nov 2010 02:00:16 GMT</pubDate>
    <dc:creator>Punit</dc:creator>
    <dc:date>2010-11-23T02:00:16Z</dc:date>
    <item>
      <title>Bootloader and Vector redirection(NVOPT_INIT) bean issue.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-and-Vector-redirection-NVOPT-INIT-bean-issue/m-p/163618#M10102</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am creating a USB based bootloader.&lt;/P&gt;&lt;P&gt;I have two hex files or programs. Bootloader code is burned into ROM with P&amp;amp;E micro programmer.&lt;/P&gt;&lt;P&gt;THis bootloader code erases and burns my Application code into ROM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have protected area of 8kb(E000 - FFFF) and I am using vector table at default place in Bootloader code and my Application code has redirected vector tables to DFC4.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Things are pretty fine till here. After I am done with my bootloader I can start my Application code by a Jump to _EntryPoint where my APllication code resides. My Application gets powered up but then doesn't start reason being NVOPT_INIT which still stays "Vector REdirection" is false ie as NVOPT_INIT lies at location FFBF, I can not write to it as it is a protected area. However, as it still contains value from Bootloader code ie 0x7E, which should be 0x3E for Application code,&amp;nbsp; my application fails.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, in short how can I update this NVOPT once I am done with my Bootloader code?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using 9S08JM60 micro controlloer and Code Warrior IDE Version 5.9.0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Nov 2010 03:31:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-and-Vector-redirection-NVOPT-INIT-bean-issue/m-p/163618#M10102</guid>
      <dc:creator>Punit</dc:creator>
      <dc:date>2010-11-18T03:31:28Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader and Vector redirection(NVOPT_INIT) bean issue.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-and-Vector-redirection-NVOPT-INIT-bean-issue/m-p/163619#M10103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not aware of any 'direct' way to have two vector tables -- one for bootloader, and one for application use 'later'.&amp;nbsp; The NVOPT_INIT values can only be set directly at reset from flash.&amp;nbsp; Thus, my bootloaders run 'no interrupts at all'.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 20 Nov 2010 02:45:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-and-Vector-redirection-NVOPT-INIT-bean-issue/m-p/163619#M10103</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2010-11-20T02:45:19Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader and Vector redirection(NVOPT_INIT) bean issue.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-and-Vector-redirection-NVOPT-INIT-bean-issue/m-p/163620#M10104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think that you will not be able to use automatic vector redirection, but will need to determine from within the boot loader, whether particular vector is to be redirected to the application ISR code.&amp;nbsp; For example, the interrupt vector at address 0xFFC4 would point to ISR code within the bootloader, but the boot loader would know in advance that the&amp;nbsp;vector at location 0xDFC4 would point to the corresponding&amp;nbsp;application ISR code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is relatively easy to handle using assembly, but I am not sure about the C coding equivalent.&amp;nbsp; Perhaps others may be able to help in this respect.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;; Part of bootloader codeISR_INT29: ; Vector at $FFC4 points here    pshh        ; Do bootloader ISR processing and exit    ; else handle redirection to application code    ldhx   #$DFC4  ; Relocated vector    jmp    DO_ISR; The above code can be replicatated to suit the other vectors,
; except for the reset vector.DO_ISR: ; Execute application ISR - common code    ldhx   ,x      ; Fetch vector contents    cphx   #$FFFF  ; Test for unprogrammed vector    beq    DI1     ; Branch if unprogrammed    jsr    .x      ; Execute ISRDI1:    pulh    rti
&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;Note that the application ISR code should terminate with RTS, rather than RTI.&amp;nbsp; In C, this means that a normal function should be used for the ISR code, rather than an interrupt function.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 09:10:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-and-Vector-redirection-NVOPT-INIT-bean-issue/m-p/163620#M10104</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2020-10-29T09:10:02Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader and Vector redirection(NVOPT_INIT) bean issue.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-and-Vector-redirection-NVOPT-INIT-bean-issue/m-p/163621#M10105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is something I was looking for, thanks for your response. However, my application still doesn't start up(it is a serial comm interrupt based application). This is what I am doing:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In Bootloader Vector.c:&lt;/P&gt;&lt;P&gt;ISR(AS1_InterruptTx)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; asm&lt;BR /&gt;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pshh&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ldhx&amp;nbsp;&amp;nbsp; #$DFD4 &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; jmp&amp;nbsp;&amp;nbsp;&amp;nbsp; DO_ISR&lt;BR /&gt;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;}&lt;BR /&gt;.......Similar for other vectors with different address...........&lt;/P&gt;&lt;P&gt;.....................................................................................................&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;void DO_ISR()&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; asm&lt;BR /&gt;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ldhx&amp;nbsp;&amp;nbsp; ,x&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; cphx&amp;nbsp;&amp;nbsp; #$FFFF &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; beq&amp;nbsp;&amp;nbsp;&amp;nbsp; DI1&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; jsr&amp;nbsp;&amp;nbsp;&amp;nbsp; ,x&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;DI1:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pulh&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; rti&lt;BR /&gt;&amp;nbsp; }&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;****************************Application Vector.c***********************************&lt;/P&gt;&lt;P&gt;I changed:&lt;/P&gt;&lt;P&gt;ISR(AS1_InterruptTx)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;...........&lt;/P&gt;&lt;P&gt;...........&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To:&lt;/P&gt;&lt;P&gt;void AS1_InterruptTx()&lt;BR /&gt;{&lt;/P&gt;&lt;P&gt;..........&lt;/P&gt;&lt;P&gt;..........&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;****************************************************************************************&lt;/P&gt;&lt;P&gt;Apart from that, I have kept Vectors at default place ie 0xFFC4 and I have redirected Vector table in Application code to 0xDFC4.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The value of NVPROT_INIT being 0xDE and NVOPT_INIT being 0x7E. Although this conflicts with what should be for Application code (NVOPT = 0x3E for redirection), but we can not overite to this registers as they are protected. However, whenever an interrupt comes it goes to vector table located at 0xFFC4 which further sends it to 0xDFC4.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Logically&amp;nbsp; this seems to be a convincing solution from what all I was trying, however it doesn't seem to work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Nov 2010 02:00:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-and-Vector-redirection-NVOPT-INIT-bean-issue/m-p/163621#M10105</guid>
      <dc:creator>Punit</dc:creator>
      <dc:date>2010-11-23T02:00:16Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader and Vector redirection(NVOPT_INIT) bean issue.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-and-Vector-redirection-NVOPT-INIT-bean-issue/m-p/163622#M10106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If your application is not starting, there is a problem with jumping from the bootloader code to the the start of the application code.&amp;nbsp; This needs to be handled a little differently than the re-direction of the other interrupt vectors.&amp;nbsp; For the purpose of discussion,&amp;nbsp;I will assume that the vector to the start of the application code is held at address 0xDFFE.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To implement a jump to this location might involve the following code within the bootloader.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;  asm {    ldhx  0xDFFE;  // Application startup vector    ldhx  ,x       // Fetch vector contents    jmp   ,x       // Direct jump to application startup  }&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Once the application code commences, it should never exit, so there is no need to save any register values prior to the jump.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 09:10:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-and-Vector-redirection-NVOPT-INIT-bean-issue/m-p/163622#M10106</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2020-10-29T09:10:04Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader and Vector redirection(NVOPT_INIT) bean issue.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-and-Vector-redirection-NVOPT-INIT-bean-issue/m-p/163623#M10107</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My application does start which I can say because I have a power on routine which gets executed but stops at a point when Serial communication interrupt starts.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Nov 2010 13:17:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-and-Vector-redirection-NVOPT-INIT-bean-issue/m-p/163623#M10107</guid>
      <dc:creator>Punit</dc:creator>
      <dc:date>2010-11-23T13:17:11Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader and Vector redirection(NVOPT_INIT) bean issue.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-and-Vector-redirection-NVOPT-INIT-bean-issue/m-p/163624#M10108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;well the solution lies here:&lt;/P&gt;&lt;P&gt;&lt;A __default_attr="34703" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/34703" jivemacro="thread" title="https://community.freescale.com/thread/34703"&gt;https://community.freescale.com/thread/34703&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Nov 2010 00:59:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-and-Vector-redirection-NVOPT-INIT-bean-issue/m-p/163624#M10108</guid>
      <dc:creator>Punit</dc:creator>
      <dc:date>2010-11-25T00:59:09Z</dc:date>
    </item>
  </channel>
</rss>