<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: LTIB is showing error</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/LTIB-is-showing-error/m-p/163118#M10033</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sharief,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The appropriate forum for discussion of this product is the "Other Microcontrollers/Microprocessors" forum. You will find more help there than in this 8-bit forum. Expect the two threads you have started to be moved there soon.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Dec 2009 03:04:49 GMT</pubDate>
    <dc:creator>peg</dc:creator>
    <dc:date>2009-12-23T03:04:49Z</dc:date>
    <item>
      <title>LTIB is showing error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/LTIB-is-showing-error/m-p/163117#M10032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I am trying to install gstreamer codec in IMX51 board. for that i downloaded onr document from website. &amp;nbsp;I folloed the steps accourding to that document. In that when i tried to install LTIB by giving command ./ltib. It is not working. All other things are fine. I copies all the things in /opt and i replaced the spec files. Now my error is &amp;nbsp;[code]ariem@ariem-desktop:~/Desktop/plugins/L2.6.28_4.5.1_SDK_Aug2009_source/ltib$ ./ltib&lt;BR /&gt;sh: tclsh: command not found&lt;BR /&gt;&lt;BR /&gt;ltib cannot be run because one or more of the host packages needed to run it&lt;BR /&gt;are either missing or out of date or not in ltib's standard path. Please&lt;BR /&gt;install/upgrade these packages on your host. If you have your own utilities&lt;BR /&gt;in non-standard paths, please add an entry into the .ltibrc file for example:&lt;BR /&gt;&lt;BR /&gt;%path_std&lt;BR /&gt;/usr/local/bin:/usr/bin:/bin:/usr/bin/X11:/usr/X11R6/bin:/my/own/exes&lt;BR /&gt;&lt;BR /&gt;Package Minimum ver Installed info&lt;BR /&gt;------- ----------- ---------------&lt;BR /&gt;zlib-devel 0 not installed&lt;BR /&gt;rpm 0 not installed&lt;BR /&gt;rpm-build 0 not installed&lt;BR /&gt;m4 0 not installed&lt;BR /&gt;bison 0 not installed&lt;BR /&gt;tcl 0 not installed&lt;BR /&gt;&lt;BR /&gt;Died at ./ltib line 1397.&lt;BR /&gt;traceback:&lt;BR /&gt;main::host_checks:1397&lt;BR /&gt;main:542&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Started: Tue Dec 22 18:54:26 2009&lt;BR /&gt;Ended: Tue Dec 22 18:54:27 2009&lt;BR /&gt;Elapsed: 1 seconds&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Build Failed&lt;BR /&gt;&lt;BR /&gt;Exiting on error or interrupt&lt;BR /&gt;ariem@ariem-desktop:~/Desktop/plugins/L2.6.28_4.5.1_SDK_Aug2009_source/ltib$&lt;BR /&gt;[/code]&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Dec 2009 21:29:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/LTIB-is-showing-error/m-p/163117#M10032</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-12-22T21:29:13Z</dc:date>
    </item>
    <item>
      <title>Re: LTIB is showing error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/LTIB-is-showing-error/m-p/163118#M10033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sharief,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The appropriate forum for discussion of this product is the "Other Microcontrollers/Microprocessors" forum. You will find more help there than in this 8-bit forum. Expect the two threads you have started to be moved there soon.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Dec 2009 03:04:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/LTIB-is-showing-error/m-p/163118#M10033</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2009-12-23T03:04:49Z</dc:date>
    </item>
  </channel>
</rss>