<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: programming pins MC9S12XS128</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/programming-pins-MC9S12XS128/m-p/234136#M9432</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;From datasheet: “The background debug module (BDM) sub-block is a single-wire, background debug system implemented in on-chip hardware for minimal CPU intervention. All interfacing with the BDM is done via the BKGD pin.”&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, for programming you will need MODC/BKGD pin and additionally also RESET pin.&lt;/P&gt;&lt;P&gt;Ground signal is self-evidence and some programming devices require also MCU power supply voltage (3.3V..5V).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The BKGD/MODC pin is used as a pseudo-open-drain pin. Therefore typically BDM interface drive this pin by open-drain output. In case of S12XS family, the BKGD pin has an internal pull-up device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For onboard BDM connection is typically used 6pin BDM connector (2x3 pin header with pitch 2.54mm/100mils).&lt;/P&gt;&lt;P&gt;Please look at DEMO9S12XSFAME board schematic from attachment.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Mar 2013 16:30:05 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2013-03-22T16:30:05Z</dc:date>
    <item>
      <title>programming pins MC9S12XS128</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/programming-pins-MC9S12XS128/m-p/234135#M9431</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;good afternoon .. I need to know specifically what the programming pins MC9S12XS128 freescale microcontroller programmer ... and that we could use. We are working on a module microcontroller programming universal as thesis ... thanks for your quick help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2013 17:13:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/programming-pins-MC9S12XS128/m-p/234135#M9431</guid>
      <dc:creator>alfonsovargashe</dc:creator>
      <dc:date>2013-03-21T17:13:53Z</dc:date>
    </item>
    <item>
      <title>Re: programming pins MC9S12XS128</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/programming-pins-MC9S12XS128/m-p/234136#M9432</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;From datasheet: “The background debug module (BDM) sub-block is a single-wire, background debug system implemented in on-chip hardware for minimal CPU intervention. All interfacing with the BDM is done via the BKGD pin.”&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, for programming you will need MODC/BKGD pin and additionally also RESET pin.&lt;/P&gt;&lt;P&gt;Ground signal is self-evidence and some programming devices require also MCU power supply voltage (3.3V..5V).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The BKGD/MODC pin is used as a pseudo-open-drain pin. Therefore typically BDM interface drive this pin by open-drain output. In case of S12XS family, the BKGD pin has an internal pull-up device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For onboard BDM connection is typically used 6pin BDM connector (2x3 pin header with pitch 2.54mm/100mils).&lt;/P&gt;&lt;P&gt;Please look at DEMO9S12XSFAME board schematic from attachment.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Mar 2013 16:30:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/programming-pins-MC9S12XS128/m-p/234136#M9432</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2013-03-22T16:30:05Z</dc:date>
    </item>
    <item>
      <title>Re: programming pins MC9S12XS128</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/programming-pins-MC9S12XS128/m-p/234137#M9433</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hola Alfonso!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Was this helpful?&lt;/P&gt;&lt;P&gt;Please let us know! :smileywink:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Mar 2013 18:49:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/programming-pins-MC9S12XS128/m-p/234137#M9433</guid>
      <dc:creator>Monica</dc:creator>
      <dc:date>2013-03-25T18:49:30Z</dc:date>
    </item>
  </channel>
</rss>