<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: S12G Flash Driver</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12G-Flash-Driver/m-p/229070#M9341</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I recommend you to analyze the Application Note AN3275, it has a detailed explanation on the eeprom functionality and it also has a software sample in which you can refer to source file s12eeprom.c to view the eeprom routines. I have attached the AppNote to this response.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Feb 2014 03:32:27 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2014-02-13T03:32:27Z</dc:date>
    <item>
      <title>S12G Flash Driver</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12G-Flash-Driver/m-p/229069#M9340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would really appreciate if someone knows about S12G Driver Flash spec: at first I'm unable to understand if the built-in algorithms, accessible on Flash memory via pre-defined register, run on RAM or are somewhere written in rom...Then is there their availability as done for PPC (C90FL driver executables for example) anywhere in the Freescale material? Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Feb 2014 16:13:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12G-Flash-Driver/m-p/229069#M9340</guid>
      <dc:creator>secrob</dc:creator>
      <dc:date>2014-02-12T16:13:36Z</dc:date>
    </item>
    <item>
      <title>Re: S12G Flash Driver</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12G-Flash-Driver/m-p/229070#M9341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I recommend you to analyze the Application Note AN3275, it has a detailed explanation on the eeprom functionality and it also has a software sample in which you can refer to source file s12eeprom.c to view the eeprom routines. I have attached the AppNote to this response.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2014 03:32:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12G-Flash-Driver/m-p/229070#M9341</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2014-02-13T03:32:27Z</dc:date>
    </item>
  </channel>
</rss>