<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: S12X Conversion Sequence Length and WRAP</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12X-Conversion-Sequence-Length-and-WRAP/m-p/220375#M9236</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can start conversion sequence from channel other than AN0. With default WRAP setting or on older S12 which don't have WRAP bits, you could start for example sequence of 8 channels from AN12. That would convert channels AN12 to AN15, then AN0 to AN3. I didn't try any wrapping&amp;nbsp;myself yet, but I think with wrap set to 13, you could convert AN12,AN13, then AN0 to AN5. This makes sense in case tight layout asks you to skip some ATD pins.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Sep 2010 12:56:36 GMT</pubDate>
    <dc:creator>kef</dc:creator>
    <dc:date>2010-09-02T12:56:36Z</dc:date>
    <item>
      <title>S12X Conversion Sequence Length and WRAP</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12X-Conversion-Sequence-Length-and-WRAP/m-p/220374#M9235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the difference between using the conversion sequence length and the WRAP bits?&amp;nbsp; If SCAN = 1 and MULT = 1 (continuous scan and multiple channels), won't the conversion sequence length and the WRAP bits be doing the same function?&amp;nbsp; Does one have a precendence over the other?&amp;nbsp; Can I only write to WRAP&amp;nbsp;and leave conversion sequence at the default?&amp;nbsp; Currently I just set them to be equal, i.e. wrap at AN7 and conversion length = 8.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Sep 2010 23:38:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12X-Conversion-Sequence-Length-and-WRAP/m-p/220374#M9235</guid>
      <dc:creator>maatweeb</dc:creator>
      <dc:date>2010-09-01T23:38:17Z</dc:date>
    </item>
    <item>
      <title>Re: S12X Conversion Sequence Length and WRAP</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12X-Conversion-Sequence-Length-and-WRAP/m-p/220375#M9236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can start conversion sequence from channel other than AN0. With default WRAP setting or on older S12 which don't have WRAP bits, you could start for example sequence of 8 channels from AN12. That would convert channels AN12 to AN15, then AN0 to AN3. I didn't try any wrapping&amp;nbsp;myself yet, but I think with wrap set to 13, you could convert AN12,AN13, then AN0 to AN5. This makes sense in case tight layout asks you to skip some ATD pins.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Sep 2010 12:56:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12X-Conversion-Sequence-Length-and-WRAP/m-p/220375#M9236</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-09-02T12:56:36Z</dc:date>
    </item>
    <item>
      <title>Re: S12X Conversion Sequence Length and WRAP</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12X-Conversion-Sequence-Length-and-WRAP/m-p/220376#M9237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sounds good.&amp;nbsp; Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Sep 2010 21:59:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12X-Conversion-Sequence-Length-and-WRAP/m-p/220376#M9237</guid>
      <dc:creator>maatweeb</dc:creator>
      <dc:date>2010-09-02T21:59:31Z</dc:date>
    </item>
  </channel>
</rss>