<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollersのトピック[Help]Why my PWM output is AC (sine wave) not DC??</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Help-Why-my-PWM-output-is-AC-sine-wave-not-DC/m-p/219296#M9196</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I v use S12xe, the board is i made myself, now I want to use PWM to output 2.5V DC (50% Duty), I v not use filter circuit, just direct connect with the PWM output pin, but the funny thing is the output is 2.5 v AC &amp;nbsp; (from the oscillograph, i v got a sine wave), the frequence i set to 1MHz, i v use both hardware PWM and software PWM, the situation is the same. Is some one can help me to give some advise, that maybe&amp;nbsp; where is the problem, thanks&amp;nbsp; a lo.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 04 Oct 2009 03:29:31 GMT</pubDate>
    <dc:creator>jaky0</dc:creator>
    <dc:date>2009-10-04T03:29:31Z</dc:date>
    <item>
      <title>[Help]Why my PWM output is AC (sine wave) not DC??</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Help-Why-my-PWM-output-is-AC-sine-wave-not-DC/m-p/219296#M9196</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I v use S12xe, the board is i made myself, now I want to use PWM to output 2.5V DC (50% Duty), I v not use filter circuit, just direct connect with the PWM output pin, but the funny thing is the output is 2.5 v AC &amp;nbsp; (from the oscillograph, i v got a sine wave), the frequence i set to 1MHz, i v use both hardware PWM and software PWM, the situation is the same. Is some one can help me to give some advise, that maybe&amp;nbsp; where is the problem, thanks&amp;nbsp; a lo.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Oct 2009 03:29:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Help-Why-my-PWM-output-is-AC-sine-wave-not-DC/m-p/219296#M9196</guid>
      <dc:creator>jaky0</dc:creator>
      <dc:date>2009-10-04T03:29:31Z</dc:date>
    </item>
    <item>
      <title>Re: [Help]Why my PWM output is AC (sine wave) not DC??</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Help-Why-my-PWM-output-is-AC-sine-wave-not-DC/m-p/219297#M9197</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;make sure&amp;nbsp;the&amp;nbsp;oscilloscope ground connects to ground of your system in test.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Oct 2009 09:37:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Help-Why-my-PWM-output-is-AC-sine-wave-not-DC/m-p/219297#M9197</guid>
      <dc:creator>Xbot</dc:creator>
      <dc:date>2009-10-05T09:37:47Z</dc:date>
    </item>
  </channel>
</rss>