<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Problem with USB P&amp;E multilink and HCS12A256</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Problem-with-USB-P-E-multilink-and-HCS12A256/m-p/218104#M9134</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Another strange thing is that the behaviour doesn't change with my device on or off.&lt;/P&gt;&lt;P&gt;In other words if the yellow led of USB Multilink is ON or OFF the behaviour of HiWave and of Unsecure12 is the same.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could be the USB multilink broken?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Sep 2009 21:45:08 GMT</pubDate>
    <dc:creator>LPs1978</dc:creator>
    <dc:date>2009-09-25T21:45:08Z</dc:date>
    <item>
      <title>Problem with USB P&amp;E multilink and HCS12A256</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Problem-with-USB-P-E-multilink-and-HCS12A256/m-p/218099#M9129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I bought a USB P&amp;amp;E multilink and I'm using codewarrior for HCS12 ver. 4,7.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Multilink seems to be installed properly in windows, where I see, under jungo category, a voce "Multilink 2.0"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to start a simple project with my CPU HCS12A256. I compile it and all is ok but when HiWave is launched it doesn't works. The application doesn't response to the OS and I have to terminate hiwave to wake my PC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The blu and yellow leds are on on the multilink.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another information is that I always use my hardware with Metrowerks CodeWarrior 2.0 with a classic multilink with parallel interface.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Someone has an answer for me???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Sep 2009 15:34:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Problem-with-USB-P-E-multilink-and-HCS12A256/m-p/218099#M9129</guid>
      <dc:creator>LPs1978</dc:creator>
      <dc:date>2009-09-25T15:34:40Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with USB P&amp;E multilink and HCS12A256</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Problem-with-USB-P-E-multilink-and-HCS12A256/m-p/218100#M9130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A little news. If I try to leave the HiWave blocked, after 5 minutes it show me an error "unable to find communication speed". I calculate the value of IO_DELAY_CNT properly with mi Fbus of 8MHz. I set it to 14 and then the communication starts and the unsecure procedure starts, but it doesn't success.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What can I do????&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Sep 2009 16:43:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Problem-with-USB-P-E-multilink-and-HCS12A256/m-p/218100#M9130</guid>
      <dc:creator>LPs1978</dc:creator>
      <dc:date>2009-09-25T16:43:34Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with USB P&amp;E multilink and HCS12A256</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Problem-with-USB-P-E-multilink-and-HCS12A256/m-p/218101#M9131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hiwave unsecure.cmd&amp;nbsp;isn't always working with all MCUs. Maybe try downloading Unsecure12 utility from &lt;A href="http://www.pemicro.com/" rel="nofollow" target="_blank"&gt;www.pemicro.com&lt;/A&gt;. It should work, unless&amp;nbsp;something is wrong with hardware.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Sep 2009 18:30:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Problem-with-USB-P-E-multilink-and-HCS12A256/m-p/218101#M9131</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2009-09-25T18:30:15Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with USB P&amp;E multilink and HCS12A256</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Problem-with-USB-P-E-multilink-and-HCS12A256/m-p/218102#M9132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I downloaded it but it showm me that is unable to find the correct speed. The hardware works well beacause is a device of 5 years ago. I used metrowerk 2.0 and parallel multilink since 1994 until today when I started trying working with Freescale codewarrior 4.7 and an USB multilink.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With Unsecure12 I set the clock frequency of 8mHZ that is the value of my cristal.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What's wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Sep 2009 20:20:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Problem-with-USB-P-E-multilink-and-HCS12A256/m-p/218102#M9132</guid>
      <dc:creator>LPs1978</dc:creator>
      <dc:date>2009-09-25T20:20:00Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with USB P&amp;E multilink and HCS12A256</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Problem-with-USB-P-E-multilink-and-HCS12A256/m-p/218103#M9133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unsecure12 never failed for me, various PCs with WinXP SP2&amp;nbsp;and SP3. No ideas, sorry.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Sep 2009 20:54:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Problem-with-USB-P-E-multilink-and-HCS12A256/m-p/218103#M9133</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2009-09-25T20:54:28Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with USB P&amp;E multilink and HCS12A256</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Problem-with-USB-P-E-multilink-and-HCS12A256/m-p/218104#M9134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Another strange thing is that the behaviour doesn't change with my device on or off.&lt;/P&gt;&lt;P&gt;In other words if the yellow led of USB Multilink is ON or OFF the behaviour of HiWave and of Unsecure12 is the same.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could be the USB multilink broken?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Sep 2009 21:45:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Problem-with-USB-P-E-multilink-and-HCS12A256/m-p/218104#M9134</guid>
      <dc:creator>LPs1978</dc:creator>
      <dc:date>2009-09-25T21:45:08Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with USB P&amp;E multilink and HCS12A256</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Problem-with-USB-P-E-multilink-and-HCS12A256/m-p/218105#M9135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi LPs1978,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;One way to check if the USB multilink is broken:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Download the USB-ML-12 tech summary:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/downloads/download_file.cfm?download_id=208" target="test_blank"&gt;http://www.pemicro.com/downloads/download_file.cfm?download_id=208&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Look at the startup sequence described in chapter 8. Make sure BKGD and RESET are able to toggle properly (ie. they should not be stuck at VDD or GND.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Edison&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 Sep 2009 02:44:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Problem-with-USB-P-E-multilink-and-HCS12A256/m-p/218105#M9135</guid>
      <dc:creator>EdT</dc:creator>
      <dc:date>2009-09-26T02:44:57Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with USB P&amp;E multilink and HCS12A256</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Problem-with-USB-P-E-multilink-and-HCS12A256/m-p/218106#M9136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A little news: I used a DEMOQE board to try to connect to my board and all is ok.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this the real evidence that my USB BDM is broken? What do you think?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Sep 2009 15:08:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Problem-with-USB-P-E-multilink-and-HCS12A256/m-p/218106#M9136</guid>
      <dc:creator>LPs1978</dc:creator>
      <dc:date>2009-09-28T15:08:40Z</dc:date>
    </item>
  </channel>
</rss>