<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: How to set sleep mode IN MC9S12XHZ512 controller?</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-set-sleep-mode-IN-MC9S12XHZ512-controller/m-p/214931#M8982</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;NO I am not talking about CAN module .Actually,I want to implement a function to calculate time ,which should keep on running when controller is in sleep mode or low power mode.&lt;/P&gt;&lt;P&gt;Even I didn't find any sleep mode in this controller.So which mode should I use and how to set that.&lt;/P&gt;&lt;P&gt;SARY&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Jul 2010 12:00:33 GMT</pubDate>
    <dc:creator>SARY</dc:creator>
    <dc:date>2010-07-28T12:00:33Z</dc:date>
    <item>
      <title>How to set sleep mode IN MC9S12XHZ512 controller?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-set-sleep-mode-IN-MC9S12XHZ512-controller/m-p/214929#M8980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I want to build a function wjich should keep on running even in sleep mode.Can anyone tell me how to de that?&lt;/P&gt;&lt;P&gt;How to set the sleep mode and also will the clock will keep on oscillating in sleep mode?&lt;/P&gt;&lt;P&gt;SARY&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jul 2010 14:30:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-set-sleep-mode-IN-MC9S12XHZ512-controller/m-p/214929#M8980</guid>
      <dc:creator>SARY</dc:creator>
      <dc:date>2010-07-26T14:30:06Z</dc:date>
    </item>
    <item>
      <title>Re: How to set sleep mode IN MC9S12XHZ512 controller?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-set-sleep-mode-IN-MC9S12XHZ512-controller/m-p/214930#M8981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looking at the datasheet, sleep mode seems to be specific to the CAN module.&amp;nbsp; Is that what you are talking about?&amp;nbsp; Or are you talking about wait mode or stop mode?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jul 2010 00:29:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-set-sleep-mode-IN-MC9S12XHZ512-controller/m-p/214930#M8981</guid>
      <dc:creator>isionous</dc:creator>
      <dc:date>2010-07-28T00:29:43Z</dc:date>
    </item>
    <item>
      <title>Re: How to set sleep mode IN MC9S12XHZ512 controller?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-set-sleep-mode-IN-MC9S12XHZ512-controller/m-p/214931#M8982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;NO I am not talking about CAN module .Actually,I want to implement a function to calculate time ,which should keep on running when controller is in sleep mode or low power mode.&lt;/P&gt;&lt;P&gt;Even I didn't find any sleep mode in this controller.So which mode should I use and how to set that.&lt;/P&gt;&lt;P&gt;SARY&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jul 2010 12:00:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-set-sleep-mode-IN-MC9S12XHZ512-controller/m-p/214931#M8982</guid>
      <dc:creator>SARY</dc:creator>
      <dc:date>2010-07-28T12:00:33Z</dc:date>
    </item>
    <item>
      <title>Re: How to set sleep mode IN MC9S12XHZ512 controller?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-set-sleep-mode-IN-MC9S12XHZ512-controller/m-p/214932#M8983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pseudo STOP mode can be used with the RTI enabled to provide a time base within a low power mode.&lt;/P&gt;&lt;P&gt;This is described in chapter 7 of the Reference Manual &lt;A href="http://http://cache.freescale.com/files/microcontrollers/doc/data_sheet/MC9S12XHZ512.pdf?fpsp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation" target="_self"&gt;S12XHZ-RM&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pseudo STOP mode is selected as opposed to STOP mode by setting the PSTP bit. Then when the CPU executes the STOP instruction, the device enters pseudo STOP mode instead of STOP mode. In pseudo STOP mode the oscillator continues operating....&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Setting PSTP in the CLKSEL register ensures that the oscillator continues (pseudo STOP instead of STOP mode).&lt;/P&gt;&lt;P&gt;Setting PRE in the PLLCTL register enables the RTI in pseudo STOP&lt;/P&gt;&lt;P&gt;Register RTICTL is used to set the RTI rate.&lt;/P&gt;&lt;P&gt;RTIE in the register CRGINT enables the interrupt.&lt;/P&gt;&lt;P&gt;Ensure also that the CPU CCR S bit is clear for (pseudo) STOP mode entry.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;DPB&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jul 2010 15:30:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-set-sleep-mode-IN-MC9S12XHZ512-controller/m-p/214932#M8983</guid>
      <dc:creator>DPB</dc:creator>
      <dc:date>2010-07-28T15:30:58Z</dc:date>
    </item>
  </channel>
</rss>