<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: ATD reference voltage</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ATD-reference-voltage/m-p/213589#M8944</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry, thank you for your time and the answer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Oct 2012 07:18:08 GMT</pubDate>
    <dc:creator>thommes</dc:creator>
    <dc:date>2012-10-12T07:18:08Z</dc:date>
    <item>
      <title>ATD reference voltage</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ATD-reference-voltage/m-p/213586#M8941</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to use the ATD on the MC9S12D64 with an external reference voltage. I want to use the LM336-5.0 as a 5V reference voltage. It has an operating current up to 10mA. No i want to connect this voltage to the Vdda and the Vrh Pin, but I am not sure if this is possible. What is the highest current for these two Pins?&lt;/P&gt;&lt;P&gt;Is it the 2.5mA like the digital I/O's? Then i could use it this way, or not? I'm really new in building Hardware, so i would be very thankful for an answer.&lt;/P&gt;&lt;P&gt;Just if it is important: Vregen, Vddr,Vddx, BKGD and Reset i want to supply by a different voltageregulator.&lt;/P&gt;&lt;P&gt;This is what my Power supply looks like:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="2406_2406.GIF"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/118901i7E4C61586B1FCE12/image-size/large?v=v2&amp;amp;px=999" role="button" title="2406_2406.GIF" alt="2406_2406.GIF" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="V_Regler2.GIF"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38631iD6C02227CFE0A29B/image-size/large?v=v2&amp;amp;px=999" role="button" title="V_Regler2.GIF" alt="V_Regler2.GIF" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Sorry for my bad english. Thanks and regards,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Oct 2012 08:05:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ATD-reference-voltage/m-p/213586#M8941</guid>
      <dc:creator>thommes</dc:creator>
      <dc:date>2012-10-10T08:05:45Z</dc:date>
    </item>
    <item>
      <title>Re: ATD reference voltage</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ATD-reference-voltage/m-p/213587#M8942</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The&amp;nbsp; 2.5 mA you reference is the injection current limit (i.e. when an I/O pin exceeds VDD + 0.3V or VSS - 0.3V). As long as an input pin is within&amp;nbsp; VDD + 0.3V or VSS - 0.3V it is very high impedance and will only draw leakage current levels (see specifications). For VRH, the MC9S12DJ64 Device User Guide — V01.20 in Table A-8 specifies 0.375 mA for one A/D block enabled and 0.750 mA for two A/D blocks enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would not recommend connecting the output of the LM336-5.0 to VDDA unless the main regulator has better than 2% tolerance. This is because of parameter ∆VDDX in Table A-4 which states that Voltage Difference VDDX to VDDR and VDDA is to be no more than +/- 0.1V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, make sure you have the proper bypass capacitors on all of the supplies as detailed in Table 22-1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gordon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Oct 2012 18:12:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ATD-reference-voltage/m-p/213587#M8942</guid>
      <dc:creator>GordonD</dc:creator>
      <dc:date>2012-10-11T18:12:26Z</dc:date>
    </item>
    <item>
      <title>Re: ATD reference voltage</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ATD-reference-voltage/m-p/213588#M8943</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Gordon,&lt;BR /&gt;so you would recommend, to connect the output of the 7805 to at least Vdda and only Vrh to the LM336-5.0? Then it could be possible that Vdda is smaller than Vrh, which would lead to an error, right? Or is the extern reference Voltage not necessary? Then i would just use the 7805 for everything (Vddr, Vddx, Vdda, Vrh, Vregen, BKGD and Reset). Which way would you prefer?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2012 07:17:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ATD-reference-voltage/m-p/213588#M8943</guid>
      <dc:creator>thommes</dc:creator>
      <dc:date>2012-10-12T07:17:23Z</dc:date>
    </item>
    <item>
      <title>Re: ATD reference voltage</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ATD-reference-voltage/m-p/213589#M8944</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry, thank you for your time and the answer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2012 07:18:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ATD-reference-voltage/m-p/213589#M8944</guid>
      <dc:creator>thommes</dc:creator>
      <dc:date>2012-10-12T07:18:08Z</dc:date>
    </item>
  </channel>
</rss>