<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Input capture with delay</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Input-capture-with-delay/m-p/212446#M8849</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you need to filter some noise, you should add and external hardware filter&amp;nbsp; ( minimum 2nd order low pass filer , but higher order low pass of band pass filter should be condiderated )&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 18 Jun 2011 22:36:54 GMT</pubDate>
    <dc:creator>AROK</dc:creator>
    <dc:date>2011-06-18T22:36:54Z</dc:date>
    <item>
      <title>Input capture with delay</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Input-capture-with-delay/m-p/212445#M8848</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;i am working on freescale hcs12xdg128b microcontroller.and i want to capture RF Data using input capture pinIOC2/PT2 with delay count so that i can ignore so noise. For that i have to use DLYCT register to set delay.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;my query is that if i use DLYCT = 50 Then (dly_cnt+1)4bus clock cycle means 13micros at 16mzh bus clock after detecting rising edge (if&amp;nbsp; configure at ridging edge timer interrupt) it will generate interrupt after 13 microseconds or after detecting falling edge?pls help me for correct understanding.&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;nss&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2011 18:03:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Input-capture-with-delay/m-p/212445#M8848</guid>
      <dc:creator>nss5678</dc:creator>
      <dc:date>2011-06-07T18:03:34Z</dc:date>
    </item>
    <item>
      <title>Re: Input capture with delay</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Input-capture-with-delay/m-p/212446#M8849</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you need to filter some noise, you should add and external hardware filter&amp;nbsp; ( minimum 2nd order low pass filer , but higher order low pass of band pass filter should be condiderated )&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Jun 2011 22:36:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Input-capture-with-delay/m-p/212446#M8849</guid>
      <dc:creator>AROK</dc:creator>
      <dc:date>2011-06-18T22:36:54Z</dc:date>
    </item>
  </channel>
</rss>