<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックError while downloading the code to XET256 mounted on daughter card</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-downloading-the-code-to-XET256-mounted-on-daughter/m-p/212199#M8830</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN style=": ; font-size: 3; font-family: Arial;"&gt;I have an XEP100 eval board on which i have mounted the daughter card (LFSMPB12XEIM). I have connected the debugger to the BDM connector on the daughter card. However, I am using the crystal that is mounted on the XEP100 eval board which is 4 Mhz.&lt;BR /&gt;&lt;BR /&gt;Now, when i create a sample project using Code warrior 4.7 for the target XET256, and try to download the code (there is nothing really in the sample project, it is just the empty main function that appears default when you create the project) the error message "Error while writing to FFF8....101F8" appears on the screen. When i proceed further it says "Failed to load the P&amp;amp;E_Multilink_Cyclonepro.abs" file.&lt;BR /&gt;&lt;BR /&gt;I have attached the command window details, if it sounds helpful.&lt;BR /&gt;&lt;BR /&gt;I am looking forward to any help.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Ashok&lt;BR /&gt;&lt;/SPAN&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Dec 2008 21:54:19 GMT</pubDate>
    <dc:creator>s12x_Ashok</dc:creator>
    <dc:date>2008-12-23T21:54:19Z</dc:date>
    <item>
      <title>Error while downloading the code to XET256 mounted on daughter card</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-downloading-the-code-to-XET256-mounted-on-daughter/m-p/212199#M8830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN style=": ; font-size: 3; font-family: Arial;"&gt;I have an XEP100 eval board on which i have mounted the daughter card (LFSMPB12XEIM). I have connected the debugger to the BDM connector on the daughter card. However, I am using the crystal that is mounted on the XEP100 eval board which is 4 Mhz.&lt;BR /&gt;&lt;BR /&gt;Now, when i create a sample project using Code warrior 4.7 for the target XET256, and try to download the code (there is nothing really in the sample project, it is just the empty main function that appears default when you create the project) the error message "Error while writing to FFF8....101F8" appears on the screen. When i proceed further it says "Failed to load the P&amp;amp;E_Multilink_Cyclonepro.abs" file.&lt;BR /&gt;&lt;BR /&gt;I have attached the command window details, if it sounds helpful.&lt;BR /&gt;&lt;BR /&gt;I am looking forward to any help.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Ashok&lt;BR /&gt;&lt;/SPAN&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Dec 2008 21:54:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-downloading-the-code-to-XET256-mounted-on-daughter/m-p/212199#M8830</guid>
      <dc:creator>s12x_Ashok</dc:creator>
      <dc:date>2008-12-23T21:54:19Z</dc:date>
    </item>
    <item>
      <title>Re: Error while downloading the code to XET256 mounted on daughter card</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-downloading-the-code-to-XET256-mounted-on-daughter/m-p/212200#M8831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Did you look at &lt;A href="http://forums.freescale.com/freescale/board/message?board.id=16BITCOMM&amp;amp;message.id=6655&amp;amp;query.id=57523#M6655" target="_blank"&gt;this&lt;/A&gt; thread?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The message you are getting indicates you are trying to download code at address &lt;FONT size="3"&gt;10100-101F8, which is not correct.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="3"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CarsyCat&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jan 2009 19:02:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-downloading-the-code-to-XET256-mounted-on-daughter/m-p/212200#M8831</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2009-01-05T19:02:30Z</dc:date>
    </item>
  </channel>
</rss>