<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Duplicate Entries in Interrupt Vector Locations (Table 1-12)? in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Duplicate-Entries-in-Interrupt-Vector-Locations-Table-1-12/m-p/211684#M8800</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;First of all, thanks for the quick reply.&amp;nbsp; Let's see if I understood.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Let's take duplicate entry &lt;EM&gt;Vector base + $D2&lt;/EM&gt;.&amp;nbsp; The table shows both &lt;EM&gt;Reserved&lt;/EM&gt; and assigned to &lt;EM&gt;ATD0&lt;/EM&gt;.&amp;nbsp; This means that there should be a derivative which features ATD1 and not ATD0.&amp;nbsp; And in fact, table E-5 shows that 9S12XDG128 does have peripheral ATD1 and not ATD0.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The table entries are then correct, even if duplicate entries are shown.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Jun 2011 14:19:37 GMT</pubDate>
    <dc:creator>lorcap</dc:creator>
    <dc:date>2011-06-07T14:19:37Z</dc:date>
    <item>
      <title>Duplicate Entries in Interrupt Vector Locations (Table 1-12)?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Duplicate-Entries-in-Interrupt-Vector-Locations-Table-1-12/m-p/211682#M8798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just downloaded the revision 2.21 (October 2009) of HCS12X microcontroller data sheet, named MC9S12XDP512RMV2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seems to me that table 1-12 on page 73, which shows the interrupt vector locators, contains some duplicate entries.&amp;nbsp; For example, "Vector base + $D2" is both enlisted as dedicated to ADT0 and reserved.&amp;nbsp; Same for entries "Vector base + $BC", $AE-$98, $8A-$88, $86-$84, and $82.&amp;nbsp; Am I wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jun 2011 16:10:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Duplicate-Entries-in-Interrupt-Vector-Locations-Table-1-12/m-p/211682#M8798</guid>
      <dc:creator>lorcap</dc:creator>
      <dc:date>2011-06-03T16:10:31Z</dc:date>
    </item>
    <item>
      <title>Re: Duplicate Entries in Interrupt Vector Locations (Table 1-12)?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Duplicate-Entries-in-Interrupt-Vector-Locations-Table-1-12/m-p/211683#M8799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Reference Manual covers different devices of the XA, XB and XD Families as listed in Appendix E.&lt;/P&gt;&lt;P&gt;Some of these devices feature a reduced peripheral module set, as shown in Appendix E-5.&lt;/P&gt;&lt;P&gt;For those derivatives without the full peripheral module set, the corresponding vector locations are reserved.&lt;/P&gt;&lt;P&gt;This is the reason for the duplicate location entries.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This should be mentioned in the document.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We shall fix this for the next revision.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;DPB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2011 04:39:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Duplicate-Entries-in-Interrupt-Vector-Locations-Table-1-12/m-p/211683#M8799</guid>
      <dc:creator>DPB</dc:creator>
      <dc:date>2011-06-07T04:39:15Z</dc:date>
    </item>
    <item>
      <title>Re: Duplicate Entries in Interrupt Vector Locations (Table 1-12)?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Duplicate-Entries-in-Interrupt-Vector-Locations-Table-1-12/m-p/211684#M8800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;First of all, thanks for the quick reply.&amp;nbsp; Let's see if I understood.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Let's take duplicate entry &lt;EM&gt;Vector base + $D2&lt;/EM&gt;.&amp;nbsp; The table shows both &lt;EM&gt;Reserved&lt;/EM&gt; and assigned to &lt;EM&gt;ATD0&lt;/EM&gt;.&amp;nbsp; This means that there should be a derivative which features ATD1 and not ATD0.&amp;nbsp; And in fact, table E-5 shows that 9S12XDG128 does have peripheral ATD1 and not ATD0.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The table entries are then correct, even if duplicate entries are shown.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2011 14:19:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Duplicate-Entries-in-Interrupt-Vector-Locations-Table-1-12/m-p/211684#M8800</guid>
      <dc:creator>lorcap</dc:creator>
      <dc:date>2011-06-07T14:19:37Z</dc:date>
    </item>
    <item>
      <title>Re: Duplicate Entries in Interrupt Vector Locations (Table 1-12)?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Duplicate-Entries-in-Interrupt-Vector-Locations-Table-1-12/m-p/211685#M8801</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Your understanding is correct.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The documentation is not wrong, it is just not very good because the table should include at least a footnote to explain the double entries for single locations.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;DPB&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2011 22:25:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Duplicate-Entries-in-Interrupt-Vector-Locations-Table-1-12/m-p/211685#M8801</guid>
      <dc:creator>DPB</dc:creator>
      <dc:date>2011-06-07T22:25:00Z</dc:date>
    </item>
  </channel>
</rss>