<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: I have a problem with the printf fonction</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-have-a-problem-with-the-printf-fonction/m-p/211263#M8772</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The termio.c contains a routine&amp;nbsp;TERMIO_Init for the setup, it might need to be adapted for the hardware.&lt;/P&gt;&lt;P&gt;Alternatively Processor Expert (or Device Initialization) can be used to setup the sci module.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Jul 2010 04:32:20 GMT</pubDate>
    <dc:creator>CompilerGuru</dc:creator>
    <dc:date>2010-07-07T04:32:20Z</dc:date>
    <item>
      <title>I have a problem with the printf fonction</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-have-a-problem-with-the-printf-fonction/m-p/211261#M8770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a problem with the printf fonction.&lt;/P&gt;&lt;P&gt;I'm sorry for my bad english&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My program is :&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#include &amp;lt;hidef.h&amp;gt;&lt;/P&gt;&lt;P&gt;#include "derivative"&lt;/P&gt;&lt;P&gt;#include &amp;lt;stdio.h&amp;gt;&lt;/P&gt;&lt;P&gt;#include &amp;lt;termio.h&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;int x=0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;int main(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; for(;&lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif"&gt;&lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if(x&amp;lt;20)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("%d\n",x);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; x++;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;///////////////////////////////////////////////////////////////////////////////////////////&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On HyperTerminal, I don't receive the printf.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I believe that my program is in the loop "while (!(SCI.SCxSR1 &amp;amp; 0x80) )&amp;nbsp; {};" in the termio.c.&amp;nbsp; WHY ???&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;By default, what is the port used, SCI0 or SCI1 ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I configure the connection in hyperterminal, knowing that I have a MC9S12DG128 ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Julien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Jul 2010 20:49:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-have-a-problem-with-the-printf-fonction/m-p/211261#M8770</guid>
      <dc:creator>Juliendy</dc:creator>
      <dc:date>2010-07-06T20:49:14Z</dc:date>
    </item>
    <item>
      <title>Re: I have a problem with the printf fonction</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-have-a-problem-with-the-printf-fonction/m-p/211262#M8771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't see any harware initialization: somewhere in your code should be a line like:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;   Initialize_SCI();&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;.. or something similar, possibly including a baud-rate setting, parity-type, etc&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Look into demo code for your CPU&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jul 2010 00:22:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-have-a-problem-with-the-printf-fonction/m-p/211262#M8771</guid>
      <dc:creator>WadeH</dc:creator>
      <dc:date>2010-07-07T00:22:12Z</dc:date>
    </item>
    <item>
      <title>Re: I have a problem with the printf fonction</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-have-a-problem-with-the-printf-fonction/m-p/211263#M8772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The termio.c contains a routine&amp;nbsp;TERMIO_Init for the setup, it might need to be adapted for the hardware.&lt;/P&gt;&lt;P&gt;Alternatively Processor Expert (or Device Initialization) can be used to setup the sci module.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jul 2010 04:32:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-have-a-problem-with-the-printf-fonction/m-p/211263#M8772</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2010-07-07T04:32:20Z</dc:date>
    </item>
    <item>
      <title>Re: I have a problem with the printf fonction</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-have-a-problem-with-the-printf-fonction/m-p/211264#M8773</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you for your answer, it's OK for the printf.&lt;BR /&gt;The baud rate was bad in TERMIO_Init().&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Julien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jul 2010 15:30:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-have-a-problem-with-the-printf-fonction/m-p/211264#M8773</guid>
      <dc:creator>Juliendy</dc:creator>
      <dc:date>2010-07-08T15:30:49Z</dc:date>
    </item>
  </channel>
</rss>