<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: HD44780 'C' Initialization Code</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209444#M8632</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would have one criticism&amp;nbsp;of the attached code.&amp;nbsp; The LCD connections occupy PTA0 to PTA5 in the example.&amp;nbsp; This leaves PTA6 and PTA7 that may be used for other purposes.&amp;nbsp; However, the sample code does not preserve the previous state of these bits but always writes a zero.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This problem can be avoided by first clearing bit 0 to 5, and then or-ing the required new state of these bits.&amp;nbsp; The following modified code sample shows this process.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Additionally, the naming of the function LCDWrite8bitMode() seems a little confused to me, since only the upper nybble is actually being written (the LCD inputs for the lower nybble are actually unconnected or grounded).&amp;nbsp; I prefer the alternative function name LCDWriteInit() that is used only during initialisation of the display.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;/**********************************************************************/ // Used for LCD initialisation, prior to 4-bit mode currentvoid LCDWriteInit( byte data) {   byte shifted;      PTAD &amp;amp;= 0xC0;               // Clear bits 0-5   PTAD |= (byte)(data &amp;gt;&amp;gt; 2);  // Align data nibble to proper location   PTAD |= ENBIT;              // Raise EN line   lcd_delay( EN_DELAY);   PTAD &amp;amp;= ~ENBIT;             // Lower EN line   lcd_delay( DELAY40US);      // Delay for command completion}  /**********************************************************************/ // Write command/data byte// rs = 0 for command byte, otherwise data bytevoid LCDWriteByte( byte data, byte rs) {   byte high, low;      // Two nybbles must be separately written   // High nybble:   PTAD &amp;amp;= 0xC0;                       // Clear bits 0-5   if (rs)      PTAD |= 0x01;                    // Set RS line   PTAD |= (byte)((data &amp;amp; 0xf0) &amp;gt;&amp;gt; 2); // High nybble   PTAD |= ENBIT;                      // Raise EN line   lcd_delay( EN_DELAY);   PTAD &amp;amp;= ~ENBIT;                     // Lower EN line    // Low nybble:   PTAD &amp;amp;= 0xC1;                       // Clear bits 1-5 (RS unchanged)   PTAD |= (byte)((data &amp;amp; 0x0F) &amp;lt;&amp;lt; 2); // Low nybble   PTAD |= ENBIT;                      // Raise EN line   lcd_delay( EN_DELAY);   PTAD &amp;amp;= ~ENBIT;                     // Lower EN line   lcd_delay( DELAY40US);              // Delay for command completion}&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 12 Jun 2011 21:00:12 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2011-06-12T21:00:12Z</dc:date>
    <item>
      <title>HD44780 'C' Initialization Code</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209439#M8627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Friends!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working with&amp;nbsp;the HD44780 LCD display with the MC9S12DG128 and I was wondering if anyone might know where I may be able to find a set of initialization code for this LCD in 'C'? Thank you so very much for your time and I wish you a most wondrous day.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sincerely,&lt;/P&gt;&lt;P&gt;Jon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 May 2011 22:32:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209439#M8627</guid>
      <dc:creator>jonathan_abbati</dc:creator>
      <dc:date>2011-05-25T22:32:24Z</dc:date>
    </item>
    <item>
      <title>Re: HD44780 'C' Initialization Code</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209440#M8628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is code for 4 bit mode.. it is written for the JM but you should be able to get what you need. Teak the delays for you clock speed....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;/* *  LCD - Writes to LCD  *   *  This assumes an HD44780 or compatible LCD. 4 bit interface *  It's been tested on several, and some LCDs seem to need more delay time *  If you get garbage characters, try increasing the delay. *  PTA0 = RS (data/command) (Pin 4 on LCD module) *  PTA1 = EN  (Write pulse) (Pin 6, also called E) *  PTA2 = Data 4  (Pin 11)     *  PTA3 = Data 5  (Pin 12) *  PTA4 = Data 6  (Pin 13)  *  PTA5 = Data 7  (Pin 14) *  Pins 1 &amp;amp; 5 should be 0V on the LCD module *  Pin 5 is R/W and we only use W so ground it *  Pin 3 should go to ground thru a 1K resistor *  Pin 15 is the positive side of the back light LED and can be connected to +5 *  Pin 16 is the ground side of the back light LED, and should go to ground thru a  *  100OHM or higher resistor. You could also hook up a PWM signal here. *  (note: The resistor can be on either side of the LED. You MUST have a resistor) *  thru a transistor for variable back light. *   *  jdonelson 12/10  */// Delay constants for 48MHz clock.// Set to work with CF, too long for 08.#define ENBIT (0x02)#define DELAY40US (104)#define DELAY4_1MS (10761)#define DELAY100US (262)#define LCDWIDTH (16)#define EN_DELAY    (90)static int lcd_width = 0;static int lcd_lines = 0;static void lcd_delay(word count); void InitLCD(int width); static void LCDWrite8BitMode(byte data);void LCDWriteByte(byte data, byte rs);void LCDWriteLine(char *string, byte line);void LCDClear(void);void SetCursorLCD( byte pos);/* *  */static void lcd_delay(word count) {   word i  = 0;   for( i = 0; i &amp;lt; count ; ++i) {      asm {         nop         nop         nop         nop         nop         nop         nop         nop         nop      }   }}int LCDGetWidth(void){ return lcd_width;}/* *  */void LCDInit(int width,int lines) {   int i;   lcd_width = width;  lcd_lines = lines;  // Set bits to output  // PTA0 = RS (0=cmd,1=data) PTA1=EN lo-high-lo to write  // PTA2-5 =Data bits 4-7  PTADD |= 0x3F;  // Enable pull ups.     PTAPE |= 0x3F;  // Write all low;  PTAD &amp;amp;= ~0x3f;    // Need to do this in case still powering up.  // Should be 20MS  for( i = 0 ; i &amp;lt; 250 ; ++i)    lcd_delay(DELAY100US);  // See HD44780 spec. It tells you to do this...  LCDWrite8BitMode(0x30);  // tell it once  lcd_delay(DELAY4_1MS);  LCDWrite8BitMode(0x30);  // tell it twice  lcd_delay(DELAY4_1MS);  LCDWrite8BitMode(0x30);  // tell it thrice  lcd_delay(DELAY4_1MS);  // This sets 4 bit mode, but you can't write the low nibble yet.  LCDWrite8BitMode(0x20);  lcd_delay(DELAY4_1MS);   // Now it's set to 4 bit mode.  // 0 0 1 DL | N F X X  // N = 2/1 line, DL = 8/4 bit F=5x10/5x8  LCDWriteByte(0x28, 0); // last function set: 4-bit mode, 2 lines, 5x8 matrix  lcd_delay(DELAY4_1MS);  // 0 0 0 0 | 1 D C B  // D= Display on off, C = Cursor, B-Blink  LCDWriteByte(0x0c, 0); // display on, cursor off, blink off  lcd_delay(DELAY4_1MS);  LCDWriteByte(0x01, 0); // display clear  lcd_delay(DELAY4_1MS);  // 0 0 0 0 | 0 1 I/D  S  // I/D = Increment/Decrement S = Shift  LCDWriteByte(0x06, 0); // cursor auto-increment, disable display shift  lcd_delay(DELAY4_1MS);  for( i = 0 ; i &amp;lt; lines ; ++i)  {   LCDWriteLine("",(byte) i);  }  }//// Used to write while LCD is still in 8 bit mode.//static void LCDWrite8BitMode(byte data) {  byte shifted;  // Shift the high nibble into proper place  shifted =(byte) (data &amp;gt;&amp;gt; 2);   // Pulse EN line  PTAD = shifted;   // raise the strobe  PTAD |= ENBIT;  // We need thighs because we are too fast.  lcd_delay(EN_DELAY);  // Lower the strobe  PTAD &amp;amp;= ~ENBIT;   // Delay for command to complete.  lcd_delay(DELAY40US);} //// Write 8 bits, 4 bits at a time.//void LCDWriteByte(byte data, byte rs) {  byte high, low;    // Need to do 2x 4 bit writes  // Extract the high nibble and the lo nibble and  // shift them into proper bit positions.  // 'or' in the command/data flag.  high =(byte) (((data &amp;amp; 0xf0) &amp;gt;&amp;gt; 2) | (rs &amp;amp; 0x01)) ;  // Write, sets EN=0  PTAD = high;   // Raise EN bit to strobe data.  PTAD |= ENBIT;   lcd_delay(EN_DELAY);  // Clear EN bit  PTAD &amp;amp;= ~ENBIT;   // Now do lo nibble.  low = (byte) (((data &amp;amp; 0x0f) &amp;lt;&amp;lt; 2) | (rs &amp;amp; 0x01)) ;  PTAD = low;   PTAD |= ENBIT;   lcd_delay(EN_DELAY);  PTAD &amp;amp;= ~ENBIT;   // Delay for command to complete.  lcd_delay(DELAY40US);} void LCDWriteLine(char *string, byte line) { byte i=0; byte cmd=0; // Set up which line to write on. // Set "Cursor Address" command. // 1 A A A | A A A A // AAAAAAA can be 00H to 27H  // for the first line, and 40H to 67H for the second line. switch(line)  {  case 0:   cmd = 0x80;   break;  case 1:   cmd = 0xc0;   break;  case 2:   cmd = 0x94;   break;  case 3:   cmd = 0xD4;  default:   ; }  LCDWriteByte( cmd, 0);  // write as command // Clear the line first for( i = 0 ; i &amp;lt; lcd_width ; ++i)  LCDWriteByte( ' ', 1); LCDWriteByte( cmd, 0);  // write as command  // Send out the whole line... for( i = 0; string[i]  &amp;amp;&amp;amp;  i &amp;lt; lcd_width; i++)  {  if( string[i] == '\r' || string[i] == '\n')   continue;  LCDWriteByte( string[i], 1);  }}void LCDWriteBuffer(char *string, int count, byte line) { byte i=0; byte cmd=0; // Set up which line to write on. // Set "Cursor Address" command. // 1 A A A | A A A A // AAAAAAA can be 00H to 27H  // for the first line, and 40H to 67H for the second line. switch(line)  {  case 0:   cmd = 0x80;   break;  case 1:   cmd = 0xc0;   break;  case 2:   cmd = 0x94;   break;  case 3:   cmd = 0xD4;  default:   ; }  LCDWriteByte( cmd, 0);  // write as command // Clear the line first for( i = 0 ; i &amp;lt; lcd_width ; ++i)  LCDWriteByte( ' ', 1); LCDWriteByte( cmd, 0);  // write as command // Send out the whole line... for( i = 0; i &amp;lt; count  &amp;amp;&amp;amp;  i &amp;lt; lcd_width; i++)  {  if( string[i] == '\r' || string[i] == '\n')   continue;  LCDWriteByte( string[i], 1);  }} void SetCursorLCD( byte pos){ LCDWriteByte( pos | 0x80, 0);}&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 May 2011 22:59:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209440#M8628</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2011-05-25T22:59:54Z</dc:date>
    </item>
    <item>
      <title>Re: HD44780 'C' Initialization Code</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209441#M8629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you so much Jim! I greatly appreciate it. I am going to work with it and see if I can get it to work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 May 2011 00:52:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209441#M8629</guid>
      <dc:creator>jonathan_abbati</dc:creator>
      <dc:date>2011-05-26T00:52:27Z</dc:date>
    </item>
    <item>
      <title>Re: HD44780 'C' Initialization Code</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209442#M8630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jim&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Apology to Jon for hijacking his thread.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am interested in using this initialisation for a HD44780 module.&lt;/P&gt;&lt;P&gt;Forgive me if i sound very amateurish..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I included this file as LCD.c in my project and from main i init the LCD and when i add the&lt;/P&gt;&lt;P&gt;LCDWriteLine﻿(char *string,byte line)&amp;nbsp; inside my main ,my compiler posts a syntax error.&lt;/P&gt;&lt;P&gt;I declared a char string[ ] = {"test"} ;&amp;nbsp; (is that right?)&lt;/P&gt;&lt;P&gt;Can you please educate me with the correct syntax of LCDWriteLine﻿ in main() ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;will be much appreciated&lt;/P&gt;&lt;P&gt;Thanks and regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jun 2011 15:45:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209442#M8630</guid>
      <dc:creator>abicash</dc:creator>
      <dc:date>2011-06-10T15:45:01Z</dc:date>
    </item>
    <item>
      <title>Re: HD44780 'C' Initialization Code</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209443#M8631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got it...silly mistake...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks if you took a look&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jun 2011 16:54:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209443#M8631</guid>
      <dc:creator>abicash</dc:creator>
      <dc:date>2011-06-10T16:54:38Z</dc:date>
    </item>
    <item>
      <title>Re: HD44780 'C' Initialization Code</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209444#M8632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would have one criticism&amp;nbsp;of the attached code.&amp;nbsp; The LCD connections occupy PTA0 to PTA5 in the example.&amp;nbsp; This leaves PTA6 and PTA7 that may be used for other purposes.&amp;nbsp; However, the sample code does not preserve the previous state of these bits but always writes a zero.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This problem can be avoided by first clearing bit 0 to 5, and then or-ing the required new state of these bits.&amp;nbsp; The following modified code sample shows this process.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Additionally, the naming of the function LCDWrite8bitMode() seems a little confused to me, since only the upper nybble is actually being written (the LCD inputs for the lower nybble are actually unconnected or grounded).&amp;nbsp; I prefer the alternative function name LCDWriteInit() that is used only during initialisation of the display.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;/**********************************************************************/ // Used for LCD initialisation, prior to 4-bit mode currentvoid LCDWriteInit( byte data) {   byte shifted;      PTAD &amp;amp;= 0xC0;               // Clear bits 0-5   PTAD |= (byte)(data &amp;gt;&amp;gt; 2);  // Align data nibble to proper location   PTAD |= ENBIT;              // Raise EN line   lcd_delay( EN_DELAY);   PTAD &amp;amp;= ~ENBIT;             // Lower EN line   lcd_delay( DELAY40US);      // Delay for command completion}  /**********************************************************************/ // Write command/data byte// rs = 0 for command byte, otherwise data bytevoid LCDWriteByte( byte data, byte rs) {   byte high, low;      // Two nybbles must be separately written   // High nybble:   PTAD &amp;amp;= 0xC0;                       // Clear bits 0-5   if (rs)      PTAD |= 0x01;                    // Set RS line   PTAD |= (byte)((data &amp;amp; 0xf0) &amp;gt;&amp;gt; 2); // High nybble   PTAD |= ENBIT;                      // Raise EN line   lcd_delay( EN_DELAY);   PTAD &amp;amp;= ~ENBIT;                     // Lower EN line    // Low nybble:   PTAD &amp;amp;= 0xC1;                       // Clear bits 1-5 (RS unchanged)   PTAD |= (byte)((data &amp;amp; 0x0F) &amp;lt;&amp;lt; 2); // Low nybble   PTAD |= ENBIT;                      // Raise EN line   lcd_delay( EN_DELAY);   PTAD &amp;amp;= ~ENBIT;                     // Lower EN line   lcd_delay( DELAY40US);              // Delay for command completion}&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Jun 2011 21:00:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209444#M8632</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2011-06-12T21:00:12Z</dc:date>
    </item>
    <item>
      <title>Re: HD44780 'C' Initialization Code</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209445#M8633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;While it's generally not a bad idea to do this in general, bits A6/A7 are not pinned on the 64 pin JM, which this code was orginally written for. So it was not really an ovesight, though perhaps not the best method&lt;/P&gt;&lt;P&gt;It's called&amp;nbsp;LCDWrite8bitMode()﻿ because the chip is still in 8 bit mode and it is actually writing 8 bit commands, so I found it to be clear. I supppose LCDSet4bitMode would have been even better.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Jun 2011 21:36:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209445#M8633</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2011-06-12T21:36:59Z</dc:date>
    </item>
    <item>
      <title>Re: HD44780 'C' Initialization Code</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209446#M8634</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to run this on a QG8 and a HD44780 but am unable to get it up.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using PTA3,PTA﻿2,PTA﻿1,PTA﻿0 as data pins and PTB7 = RS , PTB6 = EN&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I dont understand if i am missing the initialisation or data?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can someone help?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;EDIT : have changed the delay for 8MHz bus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jul 2011 13:27:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209446#M8634</guid>
      <dc:creator>abicash</dc:creator>
      <dc:date>2011-07-08T13:27:53Z</dc:date>
    </item>
    <item>
      <title>Re: HD44780 'C' Initialization Code</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209447#M8635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The code will obviously need to be modified to reflect that different pins on PTA are used for the data, and the RS and EN control signals originate from a different port.&amp;nbsp; Perhaps you should post the modified code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jul 2011 17:32:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HD44780-C-Initialization-Code/m-p/209447#M8635</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2011-07-08T17:32:22Z</dc:date>
    </item>
  </channel>
</rss>