<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: DEMO9S12PFAME</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEMO9S12PFAME/m-p/209353#M8613</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you just open the project with the IDE and use it? If so, there might be a different board configuration in use by the project. Have you tried building a new project with the project wizard, and in doing so, is your board available as a choice?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 May 2011 21:38:25 GMT</pubDate>
    <dc:creator>J2MEJediMaster</dc:creator>
    <dc:date>2011-05-25T21:38:25Z</dc:date>
    <item>
      <title>DEMO9S12PFAME</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEMO9S12PFAME/m-p/209352#M8612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, I am a complete newbie with the Freescale products. Recently I got a DEMO board ( DEMO9S12PFAME ) and the corresponding CodeWarrior Evaluation CDs ( Code Warrior Versio 5.9.0 )&lt;/P&gt;&lt;P&gt;There were some example programs when I installed the Codewarrior CD. I took one of the program&lt;/P&gt;&lt;P&gt;"Freescale\CodeWarrior for HCS12 V4.7\(CodeWarrior_Examples)\HCS12X\HCS12X_LED\". I am using the USB InCircuit Debugger ( not an external debugger like PEMicro or BDI or Softtec ) to program and debug the code. In the code Warrior, I pressed Project -&amp;gt; Debug. The board got connected and there was a lot of output message on the Command Window.&lt;/P&gt;&lt;P&gt;It looked like that it identifed the board and started flashing. But, then in the end, it gave an error message&lt;/P&gt;&lt;P&gt;"Error while writing to E08000 to E08200&lt;BR /&gt;Information: No Memory at this address.&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;I went to check the map file and I saw that this memory was allocated to the .text section i.e ROM in the&amp;nbsp; linker command file. Then I clicked on inDART-HCS12 -&amp;gt; Flash and it showed the MCUID&amp;nbsp; Family as 0x02E9. Unfortunately, there is no hint of the memory location E08000 in this tool ( Non Volatile memory Control ).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone tell me what is wrong here?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 May 2011 16:41:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEMO9S12PFAME/m-p/209352#M8612</guid>
      <dc:creator>infoclog</dc:creator>
      <dc:date>2011-05-25T16:41:07Z</dc:date>
    </item>
    <item>
      <title>Re: DEMO9S12PFAME</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEMO9S12PFAME/m-p/209353#M8613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you just open the project with the IDE and use it? If so, there might be a different board configuration in use by the project. Have you tried building a new project with the project wizard, and in doing so, is your board available as a choice?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 May 2011 21:38:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEMO9S12PFAME/m-p/209353#M8613</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2011-05-25T21:38:25Z</dc:date>
    </item>
    <item>
      <title>Re: DEMO9S12PFAME</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEMO9S12PFAME/m-p/209354#M8614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;YEs, I loaded the .mcp project and thats a LED Blinking program. When I click on inDART-HCS12-&amp;gt;MCUConfiguraiton, I selected the MCU configuration DEMO9S12PFAME﻿. When I select that then it shows a info that this configuration is "Starter Kit for Freescale MC9S12P128.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I guess it really communicates with the hardware but the only problem is the unrecognised memory location.&lt;/P&gt;&lt;P&gt;I have attached the attachment and please search for the word "Failure".&lt;/P&gt;&lt;P&gt;Sometimes there is also an error message INVALID BP.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Maybe someone can see the attached file and let me know where could be the problem.﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 May 2011 23:27:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEMO9S12PFAME/m-p/209354#M8614</guid>
      <dc:creator>infoclog</dc:creator>
      <dc:date>2011-05-25T23:27:10Z</dc:date>
    </item>
    <item>
      <title>Re: DEMO9S12PFAME</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEMO9S12PFAME/m-p/209355#M8615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Seem the patch for S12P of CW4.7 is not exist. Let try to download the patch CW12_V4_7_HCS12_P128_SP.exe﻿ from&amp;nbsp;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S12P&amp;amp;fsrch=1&amp;amp;sr=5" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S12P&amp;amp;fsrch=1&amp;amp;sr=5&lt;/A&gt;﻿ to see if it works.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 May 2011 15:10:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEMO9S12PFAME/m-p/209355#M8615</guid>
      <dc:creator>Hubo</dc:creator>
      <dc:date>2011-05-26T15:10:41Z</dc:date>
    </item>
    <item>
      <title>Re: DEMO9S12PFAME</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEMO9S12PFAME/m-p/209356#M8616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The solution is here.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;&lt;A href="http://www.freescale.com/webapp/search/Serp.jsp?sessionChecker=T9KfNpQDqJpLQhzvXHfJrmMl8nJBwH6SM6wJJLlvNMXGhRZDNyfg%21734780889%211306411171914&amp;amp;qt2=AN3937&amp;amp;SEARCH_OPERATOR=Contains&amp;amp;Go=%C2%A0&amp;amp;attempt=-1&amp;amp;QueryText=AN3937&amp;amp;svi=217.110.68.82.1305729554291836&amp;amp;baseUrl=http://www.freescale.com/webapp&amp;amp;PART_NUMBER=AN3937&amp;amp;" rel="nofollow noopener noreferrer" target="_blank"&gt;http://www.freescale.com/webapp/search/Serp.jsp?sessionChecker=T9KfNpQDqJpLQhzvXHfJrmMl8nJBwH6SM6wJJLlvNMXGhRZDNyfg!734780889!1306411171914&amp;amp;qt2=AN3937&amp;amp;SEARCH_OPERATOR=Contains&amp;amp;Go=%C2%A0&amp;amp;attempt=-1&amp;amp;QueryText=AN3937&amp;amp;svi=217.110.68.82.1305729554291836&amp;amp;baseUrl=http://www.freescale.com/webapp&amp;amp;PART_NUMBER=AN3937&amp;amp;&lt;/A&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the entire example codes are found when you look for the keyword "AN3937" in the &lt;A href="http://www.freescale.com" rel="nofollow noopener noreferrer" target="_blank"&gt;www.freescale.com&lt;/A&gt; website. The results will show a Zip fileand a pdf file which contains all the example codes and their description for running the board. and it works !!!&lt;/P&gt;&lt;P&gt;It is impossible how hidden the files are.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 May 2011 20:44:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/DEMO9S12PFAME/m-p/209356#M8616</guid>
      <dc:creator>infoclog</dc:creator>
      <dc:date>2011-05-26T20:44:07Z</dc:date>
    </item>
  </channel>
</rss>