<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic problem with CAN on EVB9S12XEP100 in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-with-CAN-on-EVB9S12XEP100/m-p/206740#M8439</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have EVB9S12XEP100 and I am using MSCAN. It was ok and I was able to send and receive CAN messages very well.&lt;/P&gt;&lt;P&gt;But now I have a problem : there isn't any signal on CANH, the signal is right on CANL (CAN0H and CAN1H are linked, CAN0L and CAN1L too, to have ACK). I have an interface CANUSB that doesn't see anything on the bus.&lt;/P&gt;&lt;P&gt;I have noticed that there isn't any signal on TX and RX on the MCU for MSCAN0 and MSCAN1.&lt;/P&gt;&lt;P&gt;It is the same code I was using before and was ok. all the other things are ok.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;what could be the problem ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Jun 2010 19:42:45 GMT</pubDate>
    <dc:creator>hasaur</dc:creator>
    <dc:date>2010-06-14T19:42:45Z</dc:date>
    <item>
      <title>problem with CAN on EVB9S12XEP100</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-with-CAN-on-EVB9S12XEP100/m-p/206740#M8439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have EVB9S12XEP100 and I am using MSCAN. It was ok and I was able to send and receive CAN messages very well.&lt;/P&gt;&lt;P&gt;But now I have a problem : there isn't any signal on CANH, the signal is right on CANL (CAN0H and CAN1H are linked, CAN0L and CAN1L too, to have ACK). I have an interface CANUSB that doesn't see anything on the bus.&lt;/P&gt;&lt;P&gt;I have noticed that there isn't any signal on TX and RX on the MCU for MSCAN0 and MSCAN1.&lt;/P&gt;&lt;P&gt;It is the same code I was using before and was ok. all the other things are ok.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;what could be the problem ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jun 2010 19:42:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-with-CAN-on-EVB9S12XEP100/m-p/206740#M8439</guid>
      <dc:creator>hasaur</dc:creator>
      <dc:date>2010-06-14T19:42:45Z</dc:date>
    </item>
    <item>
      <title>Re: problem with CAN on EVB9S12XEP100</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-with-CAN-on-EVB9S12XEP100/m-p/206741#M8440</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the EVB9S12X has 2type of tranceivers for SJA1054 , you can only use the LowSpeed Mode( lower than 125Kbps )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;you can use HS mode on CAN2&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jun 2010 15:48:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-with-CAN-on-EVB9S12XEP100/m-p/206741#M8440</guid>
      <dc:creator>VickLiui</dc:creator>
      <dc:date>2010-06-17T15:48:37Z</dc:date>
    </item>
  </channel>
</rss>