<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Programm EEPROM MC9S12XDP512 without BDM in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Programm-EEPROM-MC9S12XDP512-without-BDM/m-p/205484#M8344</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If I understood you properly, EEPROM works in special mode (with BDM connected), and doesn't work in normal mode. ECLKDIV register is write-once in normal modes. Make sure your code initializes ECLKDIV using single write operation. For example setting/clearing PRDIV8 bit, then writing other ECLKDIV bits is bad and won't work in normal modes.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Backdoor access has nothing to do with write protection.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Aug 2009 17:54:37 GMT</pubDate>
    <dc:creator>kef</dc:creator>
    <dc:date>2009-08-06T17:54:37Z</dc:date>
    <item>
      <title>Programm EEPROM MC9S12XDP512 without BDM</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Programm-EEPROM-MC9S12XDP512-without-BDM/m-p/205483#M8343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In my program it is necessary to save current customisations in EEPROM. I work with microprocessor MC9S12XDP512. Has written the program I start it in a debug mode with connected BDM modul, all perfectly works. I disable BDM modul I include the device, it passes in a state an error of operation with EEPROM. I can not understand why so occurs (((((. I think that probably occurs from for that that a normal operating mode of the microprocessor the writeprotect is installed. Read datasheet there it is written that it can be removed with the help backdoor key access, but I have not found what data series it would be necessary to write what to remove protection (((( &amp;nbsp; Prompt as to be????&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2009 12:55:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Programm-EEPROM-MC9S12XDP512-without-BDM/m-p/205483#M8343</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-08-06T12:55:24Z</dc:date>
    </item>
    <item>
      <title>Re: Programm EEPROM MC9S12XDP512 without BDM</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Programm-EEPROM-MC9S12XDP512-without-BDM/m-p/205484#M8344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If I understood you properly, EEPROM works in special mode (with BDM connected), and doesn't work in normal mode. ECLKDIV register is write-once in normal modes. Make sure your code initializes ECLKDIV using single write operation. For example setting/clearing PRDIV8 bit, then writing other ECLKDIV bits is bad and won't work in normal modes.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Backdoor access has nothing to do with write protection.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2009 17:54:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Programm-EEPROM-MC9S12XDP512-without-BDM/m-p/205484#M8344</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2009-08-06T17:54:37Z</dc:date>
    </item>
    <item>
      <title>Re: Programm EEPROM MC9S12XDP512 without BDM</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Programm-EEPROM-MC9S12XDP512-without-BDM/m-p/205485#M8345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks kef, in it also there was a problem))))&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2009 13:11:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Programm-EEPROM-MC9S12XDP512-without-BDM/m-p/205485#M8345</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-08-07T13:11:48Z</dc:date>
    </item>
  </channel>
</rss>