<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Flash protection in 9S12X</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-protection-in-9S12X/m-p/204390#M8286</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your comments.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have decided to use a method based on your first suggestion. I generate the two S-record files, remove the first line of one, the last line of the other, and merge them, using a combination of sed commands and cat. Then I download the resultant S-record and this seems to work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks again&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Jun 2010 16:11:42 GMT</pubDate>
    <dc:creator>jmv</dc:creator>
    <dc:date>2010-06-02T16:11:42Z</dc:date>
    <item>
      <title>Flash protection in 9S12X</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-protection-in-9S12X/m-p/204388#M8284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using Code Warrior 4.7 for S12X&amp;nbsp; and am trying to prevent Hiwave from erasing the top 4k of flash, which I use as a boot loader and subsequently set in my code as protected. Hiwave erases all the flash, which means I lose my boot loader every time I download anything from Hiwave. I can see no way of specifying a range of flash addresses that you wish Hiwave to leave alone.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any suggestions?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Jun 2010 22:05:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-protection-in-9S12X/m-p/204388#M8284</guid>
      <dc:creator>jmv</dc:creator>
      <dc:date>2010-06-01T22:05:12Z</dc:date>
    </item>
    <item>
      <title>Re: Flash protection in 9S12X</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-protection-in-9S12X/m-p/204389#M8285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Instead of preventing flash erase you may include bootloader image in your project output files (S records files and *.abs ELF file). To do so you need to&lt;/P&gt;&lt;P&gt;1) copy bootloader S-records into project \bin folder. I guess&amp;nbsp;any folder from project access path will work.&lt;/P&gt;&lt;P&gt;2) add&amp;nbsp;line to prm file&lt;/P&gt;&lt;P&gt;&amp;nbsp;HEXFILE bootloader_S19_file_name.s19&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Multilink/Cyclone connection has AEFSKIPERASING command, which can be added into one of *.cmd files. This commadn allows to skip erase of whole flash blocks or EEPROM blocks. This is not what you want. I guess flash loader uses mass erase command instead of erase sector by sector. Mass erase is faster. If that's the case, then flash protection won't help here, because mass erase doesn't work if any portion of flash array is write protected.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Jun 2010 23:37:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-protection-in-9S12X/m-p/204389#M8285</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-06-01T23:37:01Z</dc:date>
    </item>
    <item>
      <title>Re: Flash protection in 9S12X</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-protection-in-9S12X/m-p/204390#M8286</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your comments.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have decided to use a method based on your first suggestion. I generate the two S-record files, remove the first line of one, the last line of the other, and merge them, using a combination of sed commands and cat. Then I download the resultant S-record and this seems to work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks again&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jun 2010 16:11:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-protection-in-9S12X/m-p/204390#M8286</guid>
      <dc:creator>jmv</dc:creator>
      <dc:date>2010-06-02T16:11:42Z</dc:date>
    </item>
  </channel>
</rss>