<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Interrupt problem with card S12X. Help pls!</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Interrupt-problem-with-card-S12X-Help-pls/m-p/202048#M8174</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi kef&lt;/P&gt;&lt;P&gt;I made some changes following your suggestions (PITCE = 0x01; // enable only the chanel 0 timer)&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also add the address interrupt vector in the .prm file&lt;/P&gt;&lt;P&gt;VECTOR ADDRESS 0xFF7A PIT0_ISR&lt;/P&gt;&lt;P&gt;but i have still the problem.&lt;/P&gt;&lt;P&gt;when i debug, the caution ILLEGAL_BP always appears and i cannot jump into ISR&lt;/P&gt;&lt;P&gt;best rergards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 May 2010 23:34:08 GMT</pubDate>
    <dc:creator>glad86</dc:creator>
    <dc:date>2010-05-19T23:34:08Z</dc:date>
    <item>
      <title>Interrupt problem with card S12X. Help pls!</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Interrupt-problem-with-card-S12X-Help-pls/m-p/202046#M8172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello, i'm newbie with MCU MC9S12XDP512.&lt;/P&gt;&lt;P&gt;I want to enable an interrupt PIT on chanel 0 to send a message via port CAN0 , and I did the following configurations&lt;/P&gt;&lt;P&gt;// Configuration des PIT&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; PITCE = 0x07;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Activation des canaux 0, 1 et 2 du PIT&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PITMUX = 0x02;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Timer 0 et 2 avec microtime base 0 &amp;amp; Timer 1 avec microtime base 1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PITMTLD0 = 7;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // prediviseur toute les 1us&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PITLD0 = 999;&amp;nbsp;&amp;nbsp;&amp;nbsp; // IT toute les 1ms du PIT0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PITLD2 = 65535;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Chargement du PIT2 à sa valeur max -&amp;gt; IT toute les 65,5ms&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PITMTLD1 = 79;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // prediviseur toute les 10us&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PITLD1 = 19999;&amp;nbsp;&amp;nbsp;&amp;nbsp; // IT toute les 200ms du PIT1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PITINTE = 0x07;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Activation des interruptions de rebouclage pour les Timer 0, 1 et 2&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PITCFLMT = 0xA3;&amp;nbsp;&amp;nbsp; // Chargement des Micro Timer 0 et 1&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;//&amp;nbsp; enable portCAN and interrupt&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; can0_init();&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; EnableInterrupts;&lt;/P&gt;&lt;P&gt;//&amp;nbsp; ISR on channel 0&lt;/P&gt;&lt;P&gt;#pragma CODE_SEG __NEAR_SEG NON_BANKED&lt;BR /&gt;&lt;BR /&gt;interrupt void PIT0_ISR(void)&lt;BR /&gt;{&lt;/P&gt;&lt;P&gt;if(MSCAN0_CheckTxBufReady()==1)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;MSCAN0_Tx(&amp;amp;msg);&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PITTF = 0x01;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;#pragma CODE_SEG DEFAULT&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;// The problem is when i debug my program, i met the caution : ILLEGAL_BP and the interrupt cannot execute. I think my module CAN works well because when i don't use the interrupt with channel 0,&amp;nbsp; it doesn"t happen like that.&lt;/P&gt;&lt;P&gt;can anyone help me pls!&lt;/P&gt;&lt;P&gt;best rerards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 May 2010 16:11:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Interrupt-problem-with-card-S12X-Help-pls/m-p/202046#M8172</guid>
      <dc:creator>glad86</dc:creator>
      <dc:date>2010-05-19T16:11:34Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt problem with card S12X. Help pls!</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Interrupt-problem-with-card-S12X-Help-pls/m-p/202047#M8173</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;PITINTE = 0x07;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Activation des interruptions de rebouclage pour les Timer 0, 1 et 2&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seems you enabled interrupts for 3 PIT channels. But I see only one PIT0_ISR defined.&amp;nbsp; Hope PIT1 and PIT2 ISRs are also defined.&lt;/P&gt;&lt;P&gt;Did you setup PIT0-PIT2 interrupt vectors?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 May 2010 22:25:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Interrupt-problem-with-card-S12X-Help-pls/m-p/202047#M8173</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-05-19T22:25:24Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt problem with card S12X. Help pls!</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Interrupt-problem-with-card-S12X-Help-pls/m-p/202048#M8174</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi kef&lt;/P&gt;&lt;P&gt;I made some changes following your suggestions (PITCE = 0x01; // enable only the chanel 0 timer)&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also add the address interrupt vector in the .prm file&lt;/P&gt;&lt;P&gt;VECTOR ADDRESS 0xFF7A PIT0_ISR&lt;/P&gt;&lt;P&gt;but i have still the problem.&lt;/P&gt;&lt;P&gt;when i debug, the caution ILLEGAL_BP always appears and i cannot jump into ISR&lt;/P&gt;&lt;P&gt;best rergards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 May 2010 23:34:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Interrupt-problem-with-card-S12X-Help-pls/m-p/202048#M8174</guid>
      <dc:creator>glad86</dc:creator>
      <dc:date>2010-05-19T23:34:08Z</dc:date>
    </item>
  </channel>
</rss>