<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックStrange AxIDE driver problem for MC9S12HY64 demo board</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Strange-AxIDE-driver-problem-for-MC9S12HY64-demo-board/m-p/200536#M8096</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I can scarcely believe it, but when I went to install the AxIDE utility today for the MC9S12HY64 demo board, it failed at the point where one has to pick the target directory. The default is a directory on the C drive, but in my case since I have a dual boot Linux / XP system, the hard drive is the E: drive instead. I click on the icon to browse for the target folder and the wizard then exits with a message that the C drive is not available. I basically have no opportunity to browse or even edit the C to E drive letter in the path. It is as if the fixed drive is "hard wired" to C drive in the code.... Anyone know a workaround or updated driver utility that does not have this problem ? The executable I am having a problem with is AxIDE385.exe Dated 7/26/2004 9:59am Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 15 May 2010 23:59:34 GMT</pubDate>
    <dc:creator>KeithO</dc:creator>
    <dc:date>2010-05-15T23:59:34Z</dc:date>
    <item>
      <title>Strange AxIDE driver problem for MC9S12HY64 demo board</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Strange-AxIDE-driver-problem-for-MC9S12HY64-demo-board/m-p/200536#M8096</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I can scarcely believe it, but when I went to install the AxIDE utility today for the MC9S12HY64 demo board, it failed at the point where one has to pick the target directory. The default is a directory on the C drive, but in my case since I have a dual boot Linux / XP system, the hard drive is the E: drive instead. I click on the icon to browse for the target folder and the wizard then exits with a message that the C drive is not available. I basically have no opportunity to browse or even edit the C to E drive letter in the path. It is as if the fixed drive is "hard wired" to C drive in the code.... Anyone know a workaround or updated driver utility that does not have this problem ? The executable I am having a problem with is AxIDE385.exe Dated 7/26/2004 9:59am Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 May 2010 23:59:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Strange-AxIDE-driver-problem-for-MC9S12HY64-demo-board/m-p/200536#M8096</guid>
      <dc:creator>KeithO</dc:creator>
      <dc:date>2010-05-15T23:59:34Z</dc:date>
    </item>
    <item>
      <title>Re: Strange AxIDE driver problem for MC9S12HY64 demo board</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Strange-AxIDE-driver-problem-for-MC9S12HY64-demo-board/m-p/200537#M8097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It sounds like you need to file a Servce Request on that. Click &lt;A href="https://www.freescale.com/webapp/servicerequest.create_SR.framework" rel="nofollow" target="_self"&gt;here&lt;/A&gt; to submit an on-line service request.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 May 2010 20:57:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Strange-AxIDE-driver-problem-for-MC9S12HY64-demo-board/m-p/200537#M8097</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2010-05-17T20:57:58Z</dc:date>
    </item>
  </channel>
</rss>