<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic EMUL instruction cycle ?error? in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/EMUL-instruction-cycle-error/m-p/200407#M8092</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have noticed that the instruction cycle count in the disassembly listing shows that the EMUL instruction uses one clock cycle, 0000&amp;nbsp; 13&amp;nbsp; [1]&amp;nbsp; EMUL, however the instruction matrix for the 9S12 says EMUL uses 3 clocks.&amp;nbsp; Is there a file that CodeWarrior uses that can be corrected so that the listing will be correct?&amp;nbsp; Or is it true that the EMUL instruction does such a fast multiply?\&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 18 Jul 2009 05:42:04 GMT</pubDate>
    <dc:creator>TSCeric</dc:creator>
    <dc:date>2009-07-18T05:42:04Z</dc:date>
    <item>
      <title>EMUL instruction cycle ?error?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/EMUL-instruction-cycle-error/m-p/200407#M8092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have noticed that the instruction cycle count in the disassembly listing shows that the EMUL instruction uses one clock cycle, 0000&amp;nbsp; 13&amp;nbsp; [1]&amp;nbsp; EMUL, however the instruction matrix for the 9S12 says EMUL uses 3 clocks.&amp;nbsp; Is there a file that CodeWarrior uses that can be corrected so that the listing will be correct?&amp;nbsp; Or is it true that the EMUL instruction does such a fast multiply?\&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Jul 2009 05:42:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/EMUL-instruction-cycle-error/m-p/200407#M8092</guid>
      <dc:creator>TSCeric</dc:creator>
      <dc:date>2009-07-18T05:42:04Z</dc:date>
    </item>
    <item>
      <title>Re: EMUL instruction cycle ?error?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/EMUL-instruction-cycle-error/m-p/200408#M8093</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which derivative are you using?&lt;/P&gt;&lt;P&gt;And how do you create the disassembly listing.&lt;/P&gt;&lt;P&gt;While S12's need (out of my memory) 3 cycles, S12X cores are faster and do only need a single cycle.&lt;/P&gt;&lt;P&gt;So could be that the disassembler is configured (or defaults to) an S12X.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Jul 2009 12:46:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/EMUL-instruction-cycle-error/m-p/200408#M8093</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2009-07-18T12:46:18Z</dc:date>
    </item>
  </channel>
</rss>