<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: How much current can I source to drive PWM using MC9S12DP256 (Dragon12 board from Wytec)</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-much-current-can-I-source-to-drive-PWM-using-MC9S12DP256/m-p/199108#M7995</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Jim,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks for the response.&amp;nbsp; It looks like the MAX source/sink current is +/-25mA.&amp;nbsp; Due to the relatively small source current, it looks like I'll have to use a darlington pair transistor to reach the high current needs of the solenoid.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Mar 2008 03:21:06 GMT</pubDate>
    <dc:creator>Sully81</dc:creator>
    <dc:date>2008-03-04T03:21:06Z</dc:date>
    <item>
      <title>How much current can I source to drive PWM using MC9S12DP256 (Dragon12 board from Wytec)</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-much-current-can-I-source-to-drive-PWM-using-MC9S12DP256/m-p/199106#M7993</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I am using Wytec's Dragon12 board to drive PWM for some 24V (5 Ohm, MAX 2 Amp) solenoids.&amp;nbsp; I am looking to spec out the transistor circuit to drive the coil but need to know how much current I can safely pull source from the MC9S12DP256 chip.&amp;nbsp; Can anyone point in the right direction to find this?&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Mar 2008 23:30:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-much-current-can-I-source-to-drive-PWM-using-MC9S12DP256/m-p/199106#M7993</guid>
      <dc:creator>Sully81</dc:creator>
      <dc:date>2008-03-03T23:30:13Z</dc:date>
    </item>
    <item>
      <title>Re: How much current can I source to drive PWM using MC9S12DP256 (Dragon12 board from Wytec)</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-much-current-can-I-source-to-drive-PWM-using-MC9S12DP256/m-p/199107#M7994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Do you mean the MC9S12DP256 spec sheet?&lt;BR /&gt;&lt;BR /&gt;You should have got a copy with the board.&lt;BR /&gt;&lt;BR /&gt;Also, if you look on the schematic there should be a circuit that drives a relay, which you can copy except with a higher rated transistor.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Mar 2008 01:25:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-much-current-can-I-source-to-drive-PWM-using-MC9S12DP256/m-p/199107#M7994</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-03-04T01:25:37Z</dc:date>
    </item>
    <item>
      <title>Re: How much current can I source to drive PWM using MC9S12DP256 (Dragon12 board from Wytec)</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-much-current-can-I-source-to-drive-PWM-using-MC9S12DP256/m-p/199108#M7995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Jim,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks for the response.&amp;nbsp; It looks like the MAX source/sink current is +/-25mA.&amp;nbsp; Due to the relatively small source current, it looks like I'll have to use a darlington pair transistor to reach the high current needs of the solenoid.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Mar 2008 03:21:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-much-current-can-I-source-to-drive-PWM-using-MC9S12DP256/m-p/199108#M7995</guid>
      <dc:creator>Sully81</dc:creator>
      <dc:date>2008-03-04T03:21:06Z</dc:date>
    </item>
    <item>
      <title>Re: How much current can I source to drive PWM using MC9S12DP256 (Dragon12 board from Wytec)</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-much-current-can-I-source-to-drive-PWM-using-MC9S12DP256/m-p/199109#M7996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Yes, you could use a darlington transistor, or alternatively a power MOSFET with a suitable maximum current rating, provided it is capable of fully switching&amp;nbsp;with an input level of less than 5 volts.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;For either method,&amp;nbsp;if switching operation is infrequent relative to the switching time, dissipation should not be a major issue.&amp;nbsp; Both methods will also require suppression of inductive voltage surges.&amp;nbsp; The simplest method is to use a diode in parallel with the solenoid winding.&amp;nbsp; The diode should have a repetitive peak current rating equal or greater than the solenoid operating current.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If the MOSFET solution is used, a small series resistance in the gate circuit will limit the charging current into the gate-source capacitance, to be supplied by the MCU pin.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Mar 2008 11:07:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-much-current-can-I-source-to-drive-PWM-using-MC9S12DP256/m-p/199109#M7996</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-03-04T11:07:42Z</dc:date>
    </item>
  </channel>
</rss>