<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Other nice MCUs... in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Other-nice-MCUs/m-p/124319#M76</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;P&gt;Hi,&lt;BR /&gt;I recently worked on a customer project using an Atmel AT91SAMX256.&lt;BR /&gt;I'm quite impressed about this MCU because it has none of the inconveniences we have to fight with on S12 derivatives.&lt;BR /&gt;There's no paging, a really fast 32-bit ARM7 CPU (that can be used in little- or big endian mode!!). There's no need for an XGATE because of an DMA mechanism that tranfers memory from/to all peripherals, a highly configurable (variable shift register width, automatic delays, etc.) SPI with four chip select lines.&lt;BR /&gt;It has integrated USB support, 64K RAM (non-paged!!!), a built-in boot ROM and many more, but all for nearly the same price as an S12XA256!&lt;BR /&gt;The only disadvantage is the lower GPIO count.&lt;BR /&gt;There might be other disadvantages (e.g. higher current consumption), but until now I'm very surprised about that nice multi-purpose MCU.&lt;BR /&gt;Cheers,&lt;BR /&gt;-&amp;gt; pittbull&lt;/P&gt;&lt;P&gt;Message Edited by Alban on &lt;SPAN class="date_text"&gt;2007-02-25&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;06:30 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 25 Feb 2007 05:08:20 GMT</pubDate>
    <dc:creator>pittbull</dc:creator>
    <dc:date>2007-02-25T05:08:20Z</dc:date>
    <item>
      <title>Other nice MCUs...</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Other-nice-MCUs/m-p/124319#M76</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;P&gt;Hi,&lt;BR /&gt;I recently worked on a customer project using an Atmel AT91SAMX256.&lt;BR /&gt;I'm quite impressed about this MCU because it has none of the inconveniences we have to fight with on S12 derivatives.&lt;BR /&gt;There's no paging, a really fast 32-bit ARM7 CPU (that can be used in little- or big endian mode!!). There's no need for an XGATE because of an DMA mechanism that tranfers memory from/to all peripherals, a highly configurable (variable shift register width, automatic delays, etc.) SPI with four chip select lines.&lt;BR /&gt;It has integrated USB support, 64K RAM (non-paged!!!), a built-in boot ROM and many more, but all for nearly the same price as an S12XA256!&lt;BR /&gt;The only disadvantage is the lower GPIO count.&lt;BR /&gt;There might be other disadvantages (e.g. higher current consumption), but until now I'm very surprised about that nice multi-purpose MCU.&lt;BR /&gt;Cheers,&lt;BR /&gt;-&amp;gt; pittbull&lt;/P&gt;&lt;P&gt;Message Edited by Alban on &lt;SPAN class="date_text"&gt;2007-02-25&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;06:30 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 25 Feb 2007 05:08:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Other-nice-MCUs/m-p/124319#M76</guid>
      <dc:creator>pittbull</dc:creator>
      <dc:date>2007-02-25T05:08:20Z</dc:date>
    </item>
    <item>
      <title>Re: Other nice MCUs... Wrong Board in Wrong Forum.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Other-nice-MCUs/m-p/124320#M77</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hello, I&amp;nbsp;removed the content of previous message. But then restored it for several reasons.&lt;/P&gt;&lt;P&gt;Post&amp;nbsp;about a&amp;nbsp;32-Bit ATMEL Microcontroller.&lt;/P&gt;&lt;P&gt;If there is no board to talk about Freescale&amp;nbsp;32-bit MCU here, it's not to pollute the Freescale 16-bit board with other brands of 32-bit MCUs.&lt;BR /&gt;A post&amp;nbsp;twice out of subject should have simply be deleted like others, but I wished to explain for it not to occur again.&lt;/P&gt;&lt;P&gt;It is normal a 32-bit MCU does not need paging for 64KB. That is a 16-bit address. MAC7xxx series is also a ARM7 core series that would not need paging scheme.&lt;/P&gt;&lt;P&gt;Alban.&lt;/P&gt;&lt;P&gt;Message Edited by Alban on &lt;SPAN class="date_text"&gt;2007-02-25&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;06:38 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Feb 2007 02:21:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Other-nice-MCUs/m-p/124320#M77</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-02-26T02:21:17Z</dc:date>
    </item>
  </channel>
</rss>