<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Setting CAN Bit Timing parameters</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Setting-CAN-Bit-Timing-parameters/m-p/192587#M7568</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. No.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. I'm not sure if there is a standard for the SJW. The above was my personal recommendation, based on my experience of developing various CAN drivers for Freescale MSCAN and FlexCAN, then use those drivers at the bottom of various industry standard field bus protocol stacks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SJW is as large as possible in my recommendation too. It boils down to that the SJW must be of less or equal length as the post sample ("phase segment"). And if you want the sample point as close to 87.5% as possible, there's not a lot of options for the post sample, meaning there's not a lot of options for the SJW either. For the highest baudrates 1000kbps or 800kbps you can perhaps make it 3 or 4.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Feb 2013 12:33:27 GMT</pubDate>
    <dc:creator>Lundin</dc:creator>
    <dc:date>2013-02-25T12:33:27Z</dc:date>
    <item>
      <title>Setting CAN Bit Timing parameters</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Setting-CAN-Bit-Timing-parameters/m-p/192584#M7565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to implement the following CAN bit timing specification on&amp;nbsp;TWRS12G240 which has a MC9S12G240 microcontroller, the tower is using TI SN65HVD1040 transceiver.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV class="j-rte-table"&gt;&lt;TABLE border="1" cellpadding="0" cellspacing="0"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD style="border:1px solid black;"&gt;&lt;P&gt;&lt;STRONG&gt;Parameter&lt;/STRONG&gt;&lt;/P&gt;&lt;/TD&gt;&lt;TD style="border:1px solid black;"&gt;&lt;P&gt;&lt;STRONG&gt;Value&lt;/STRONG&gt;&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD style="border:1px solid black;"&gt;&lt;P&gt;Baudrate&lt;/P&gt;&lt;/TD&gt;&lt;TD style="border:1px solid black;"&gt;&lt;P&gt;500 kBaud ± 0.1%&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD style="border:1px solid black;"&gt;&lt;P&gt;Bit Time&lt;/P&gt;&lt;/TD&gt;&lt;TD style="border:1px solid black;"&gt;&lt;P&gt;2 μs&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD style="border:1px solid black;"&gt;&lt;P&gt;Number of Time Quanta per Bit-time&lt;/P&gt;&lt;/TD&gt;&lt;TD style="border:1px solid black;"&gt;&lt;P&gt;16&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD style="border:1px solid black;"&gt;&lt;P&gt;SJW (Time Quanta)*&lt;/P&gt;&lt;/TD&gt;&lt;TD style="border:1px solid black;"&gt;&lt;P&gt;3&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD style="border:1px solid black;"&gt;&lt;P&gt;SAMPLE Point (% of Bit Time)*&lt;/P&gt;&lt;/TD&gt;&lt;TD style="border:1px solid black;"&gt;&lt;P&gt;75%&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD style="border:1px solid black;"&gt;&lt;P&gt;Sampling mode&lt;/P&gt;&lt;/TD&gt;&lt;TD style="border:1px solid black;"&gt;&lt;P&gt;Single&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD style="border:1px solid black;"&gt;&lt;P&gt;Resynchronization&lt;/P&gt;&lt;/TD&gt;&lt;TD style="border:1px solid black;"&gt;&lt;P&gt;recessive to dominant&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/DIV&gt;&lt;P align="left"&gt;&amp;nbsp;&lt;/P&gt;&lt;P align="left"&gt;Bus length&lt;/P&gt;&lt;P align="left"&gt;The maximum bus length allowed is 20 meters. Twisted wires shall be used for the CAN bus&lt;/P&gt;&lt;P&gt;and the maximum specific line delay of the wire shall be 5 ns/m.&lt;/P&gt;&lt;P align="left"&gt;Transceiver Delay&lt;/P&gt;&lt;P align="left"&gt;Maximum allowed transceiver loop delay (Tx to Rx delay) for both dominant bit to recessive bit&lt;/P&gt;&lt;P&gt;and recessive bit to dominant bit is 300ns&lt;/P&gt;&lt;P align="left"&gt;Oscillator Tolerance&lt;/P&gt;&lt;P&gt;The maximum allowed oscillator tolerance of CAN source clock is ± 0.1%.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using PLL as can bus clock and pll is being generated thorugh on board 8 Mhz crystal. If&amp;nbsp;I input 32 Mhz as CAN bus clock then every parameter is matched except oscillator tolerance which comes out to be 1.21%. Now my question, can the above bit timing parameters can be realized with different bus clock value because&amp;nbsp; I am unable to come up with any combination of prescaler and bit time and time quanta. Since&amp;nbsp;bit time and time quanta per bit time is fixed there is little left that could be done.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;According to my calculations&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Prescaler comes out as 4&lt;/P&gt;&lt;P&gt;Tq =&amp;nbsp; 32Mhz/4= 8 Mhz= 125ns.&lt;/P&gt;&lt;P&gt;Prop delay of bus= 20 * 5/1000000000=100ns&lt;/P&gt;&lt;P&gt;prop_seg=&amp;nbsp;2 *(&amp;nbsp;propagation delay of transciever+ prop delay of bus)=2(230+100)=660&lt;/P&gt;&lt;P&gt;=660/125=5.28=5&lt;/P&gt;&lt;P&gt;phase_seg1=5&lt;/P&gt;&lt;P&gt;Phase_seg2=5&lt;/P&gt;&lt;P&gt;RJW =4&lt;/P&gt;&lt;P&gt;delta f=4/20*10=0.0125&lt;/P&gt;&lt;P&gt;delta f &amp;lt;min(phase_Seg1,phase_seg2)/2(13*NBT-phase_seg2)&lt;/P&gt;&lt;P&gt;=5/2*(13*16-5)=0.0123=1.23%&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Aug 2012 19:14:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Setting-CAN-Bit-Timing-parameters/m-p/192584#M7565</guid>
      <dc:creator>thecoder</dc:creator>
      <dc:date>2012-08-24T19:14:35Z</dc:date>
    </item>
    <item>
      <title>Re: Setting CAN Bit Timing parameters</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Setting-CAN-Bit-Timing-parameters/m-p/192585#M7566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CAN is somwhat picky with bit bit timing. Generally, they said in the first CAN drafts that an oscillator tolerance of 1.58% was the worst case, so I you should aim to get below that at least (I'm not sure what the ISO 11898 says). If your application relies and revolves around CAN, you should consider picking an oscillator based on the CAN baudrates you want to use. Though note that if you fiddle around with the number of tq/bit and the SJW, you might get a more accurate location of the sample point.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As for the spec on where to place the sample point etc, I would strongly recommend to follow the CANopen standard DS301, chapter 5.4. I believe you can download the standard for free if you register at CAN-In-Automation, &lt;A href="http://www.can-cia.de." rel="nofollow" target="_blank"&gt;www.can-cia.de.&lt;/A&gt; .The bit timing there is pretty much industry standard for all CAN applications. Don't follow timing specs from Freescale manuals/app notes, they are pretty obscure and non-standard. Avoid them in particular if you are implementing any of the mainstream CAN protocols like CANopen, DeviceNet or J1939.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For convenience, this is what DS301 says about 500kbps:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Valid range for location of sample point: 85% to 90%&lt;/P&gt;&lt;P&gt;Recommended location of sample point: 87.5%&lt;/P&gt;&lt;P&gt;Estimated bus length (based on sample point recommendations): 100m.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In my projects with 8MHz-ish oscillators, for MSCAN and FlexCAN both, I use the following ideal setup for 500kbps with 87,5% sample point:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;16tq where:&lt;/P&gt;&lt;P&gt;1=sync,&lt;/P&gt;&lt;P&gt;13=pre sample,&lt;/P&gt;&lt;P&gt;2=post sample,&lt;/P&gt;&lt;P&gt;SJW=2.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Aug 2012 21:03:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Setting-CAN-Bit-Timing-parameters/m-p/192585#M7566</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2012-08-24T21:03:51Z</dc:date>
    </item>
    <item>
      <title>Re: Setting CAN Bit Timing parameters</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Setting-CAN-Bit-Timing-parameters/m-p/192586#M7567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Daniel:&lt;/P&gt;&lt;P&gt;1. Do you use Processor Expert in order to set such CAN parameters?&lt;/P&gt;&lt;P&gt;I would like to set similar settings, but documentation how sample point is calculated using settings from Processor Expert is not clear for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. SJW=2 is recommended? what standard?&lt;/P&gt;&lt;P&gt;I found recommendation it should be large, 3 or 4 is possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;/Greg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Feb 2013 08:30:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Setting-CAN-Bit-Timing-parameters/m-p/192586#M7567</guid>
      <dc:creator>grzegorzK</dc:creator>
      <dc:date>2013-02-18T08:30:16Z</dc:date>
    </item>
    <item>
      <title>Re: Setting CAN Bit Timing parameters</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Setting-CAN-Bit-Timing-parameters/m-p/192587#M7568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. No.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. I'm not sure if there is a standard for the SJW. The above was my personal recommendation, based on my experience of developing various CAN drivers for Freescale MSCAN and FlexCAN, then use those drivers at the bottom of various industry standard field bus protocol stacks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SJW is as large as possible in my recommendation too. It boils down to that the SJW must be of less or equal length as the post sample ("phase segment"). And if you want the sample point as close to 87.5% as possible, there's not a lot of options for the post sample, meaning there's not a lot of options for the SJW either. For the highest baudrates 1000kbps or 800kbps you can perhaps make it 3 or 4.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Feb 2013 12:33:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Setting-CAN-Bit-Timing-parameters/m-p/192587#M7568</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2013-02-25T12:33:27Z</dc:date>
    </item>
    <item>
      <title>Re: Setting CAN Bit Timing parameters</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Setting-CAN-Bit-Timing-parameters/m-p/192588#M7569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you use PLL as clock for CAN, it will work in most of the cases. Unfortunately there is issue in lock(0..1.5%) and unlock(0.5..2.5%) range of PLL. On base of that you don’t have any guarantee that PLL clock is enough accurate.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Therefore I cannot recommend PLL clock for CAN module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In attachment you can find simple calculator for CAN timing.&lt;/P&gt;&lt;P&gt;I hope that help you.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Feb 2013 18:34:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Setting-CAN-Bit-Timing-parameters/m-p/192588#M7569</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2013-02-25T18:34:06Z</dc:date>
    </item>
    <item>
      <title>Re: Setting CAN Bit Timing parameters</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Setting-CAN-Bit-Timing-parameters/m-p/192589#M7570</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;I will study this information.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Feb 2013 07:43:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Setting-CAN-Bit-Timing-parameters/m-p/192589#M7570</guid>
      <dc:creator>grzegorzK</dc:creator>
      <dc:date>2013-02-26T07:43:44Z</dc:date>
    </item>
  </channel>
</rss>