<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: mc9s12c128 header files</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12c128-header-files/m-p/127629#M718</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The register map is the same for all S12 devices, the smaller devices are just missing parts of it (the registers are reserved instead of used).&lt;BR /&gt;&lt;BR /&gt;I really don't know why Metrowerks/Freescale made separate register maps for separate derivates, it makes no sense since they are code compatible. Why they wrote the h-file non-standard C is also a good question. If you want to use ANSI C, the only option is to write your own register map.&lt;BR /&gt;&lt;BR /&gt;I'm using my own register map called "s12reg" which is originally for DP256 but works fine with DG256, DG128, C128, C32 etc.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Mar 2007 15:50:54 GMT</pubDate>
    <dc:creator>Lundin</dc:creator>
    <dc:date>2007-03-23T15:50:54Z</dc:date>
    <item>
      <title>mc9s12c128 header files</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12c128-header-files/m-p/127628#M717</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;This may be an ignorant question but I would like to know the answer. I would like to know if there is a mc9s12c128.h header file available for programming this microprocessor? If not does the mc9s12c32.h header file work?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Mar 2007 22:25:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12c128-header-files/m-p/127628#M717</guid>
      <dc:creator>lost2007</dc:creator>
      <dc:date>2007-03-22T22:25:57Z</dc:date>
    </item>
    <item>
      <title>Re: mc9s12c128 header files</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12c128-header-files/m-p/127629#M718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The register map is the same for all S12 devices, the smaller devices are just missing parts of it (the registers are reserved instead of used).&lt;BR /&gt;&lt;BR /&gt;I really don't know why Metrowerks/Freescale made separate register maps for separate derivates, it makes no sense since they are code compatible. Why they wrote the h-file non-standard C is also a good question. If you want to use ANSI C, the only option is to write your own register map.&lt;BR /&gt;&lt;BR /&gt;I'm using my own register map called "s12reg" which is originally for DP256 but works fine with DG256, DG128, C128, C32 etc.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Mar 2007 15:50:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12c128-header-files/m-p/127629#M718</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2007-03-23T15:50:54Z</dc:date>
    </item>
  </channel>
</rss>