<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 problem connecting to DEMO9S12XEP100</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-connecting-to-DEMO9S12XEP100/m-p/187926#M7155</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm having&amp;nbsp;problems connecting to the DEMO9S12XEP100.&lt;/P&gt;&lt;P&gt;I followed all steps in the User Manual.&lt;/P&gt;&lt;P&gt;The board in standalone mode works fine, i.e. potentiometer and light sensor can be mapped to the LEDs by pushing the buttons.&lt;/P&gt;&lt;P&gt;I installed CodeWarrior Development Studio for S12(X) V5.1&lt;/P&gt;&lt;P&gt;I installed CW12 V5.1 Processor Expert v3.04 Sevice Pack from the DVD&lt;/P&gt;&lt;P&gt;I installed the "Additional Components" from the SofTec CD (there was also a service pack on there related to version 4.5 which I didn't install)&lt;/P&gt;&lt;P&gt;Driver installation after connecting the board via USB worked fine - there's no exclamation mark next to the driver in the device manager.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Problems start when I select Project&amp;gt;Debug in CodeWarrior.&lt;/P&gt;&lt;P&gt;I get an error message: "Communication Error. Make sure the USB cable is connected to the instrument and retry"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I restarted the application as well as the system, but also get the same error.&lt;/P&gt;&lt;P&gt;Later I enabled "Show Protocol" and got this:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;executing C_layout.hwl&lt;/P&gt;&lt;P&gt;!OPEN source 0 0 60 39&lt;BR /&gt;NO CONNECTION&lt;BR /&gt;!Source &amp;lt; attributes MARKS off&lt;BR /&gt;!OPEN assembly 60 0 40 31&lt;BR /&gt;!Assembly &amp;lt; attributes ADR on,CODE off,ABSADR on,SYMB off,TOPPC 0xF88C&lt;BR /&gt;!OPEN procedure 0 39 60 17&lt;BR /&gt;!Procedure &amp;lt; attributes VALUES on,TYPES off&lt;BR /&gt;!OPEN register 60 31 40 25&lt;BR /&gt;!Register &amp;lt; attributes FORMAT AUTO,COMPLEMENT None&lt;BR /&gt;!OPEN memory 60 56 40 22&lt;BR /&gt;!Memory &amp;lt; attributes FORMAT hex,COMPLEMENT None,WORD 1,ASC on,ADR on,ADDRESS 0x80&lt;BR /&gt;!OPEN data 0 56 60 22&lt;BR /&gt;!Data:1 &amp;lt; attributes SCOPE global,COMPLEMENT None,FORMAT Symb,MODE automatic,UPDATERATE 10,NAMEWIDTH 16&lt;BR /&gt;!OPEN data 0 78 60 22&lt;BR /&gt;!Data:2 &amp;lt; attributes SCOPE local,COMPLEMENT None,FORMAT Symb,MODE automatic,UPDATERATE 10,NAMEWIDTH 16&lt;BR /&gt;!OPEN command 60 78 40 22&lt;BR /&gt;!Command &amp;lt; attributes CACHESIZE 1000&lt;BR /&gt;!bckcolor 50331647&lt;BR /&gt;!font 'Courier New' 9 BLACK&lt;BR /&gt;!AUTOSIZE on&lt;BR /&gt;!ACTIVATE Data:2 Command Procedure Data:1 Source Register Assembly Memory&lt;BR /&gt;done C_layout.hwl&lt;/P&gt;&lt;P&gt;Loading Target ...&lt;BR /&gt;Communication settings:&lt;BR /&gt;SETCOMM DRIVER PROTOCOL NOPERIODICAL&lt;BR /&gt;Loading Communication DLL&lt;BR /&gt;==&amp;gt; C:\Programme\Freescale\CWS12v5.1\prog\gdi\softec_bdm12.dll&lt;BR /&gt;GDI: DiGdiOpen()==&amp;gt; DI_OK&lt;BR /&gt;GDI: DiGdiVersion()==&amp;gt; DI_OK&lt;BR /&gt;GDI: DiGdiGetFeatures()==&amp;gt; DI_OK&lt;BR /&gt;GDI: DiGdiAddCallBack(8192)==&amp;gt; DI_OK&lt;BR /&gt;GDI: DiGdiAddCallBack(16384)==&amp;gt; DI_OK&lt;BR /&gt;GDI: DiCommGetAcceptableSettings()==&amp;gt; 0&lt;BR /&gt;Initializing STARTUP command file:&lt;BR /&gt;CMDFILE STARTUP ON ".\cmd\SofTec_HCS12_startup.cmd"&lt;BR /&gt;Initializing RESET command file:&lt;BR /&gt;CMDFILE RESET ON ".\cmd\SofTec_HCS12_reset.cmd"&lt;BR /&gt;Initializing PRELOAD command file:&lt;BR /&gt;CMDFILE PRELOAD ON ".\cmd\SofTec_HCS12_preload.cmd"&lt;BR /&gt;Initializing POSTLOAD command file:&lt;BR /&gt;CMDFILE POSTLOAD ON ".\cmd\SofTec_HCS12_postload.cmd"&lt;BR /&gt;GDI: DiGdiInitIO()&lt;BR /&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_HASCOMMUNICATIONCMD)&lt;BR /&gt;GDI: DiGdiVersion()==&amp;gt; DI_OK&lt;/P&gt;&lt;P&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;/P&gt;&lt;P&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;/P&gt;&lt;P&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;/P&gt;&lt;P&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;/P&gt;&lt;P&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;BR /&gt;==&amp;gt; DI_ERR_FATAL&lt;BR /&gt;GDI: DiErrorGetMessage()==&amp;gt; 1&lt;BR /&gt;GDI: Error Message ==&amp;gt; Communication error. Make sure that the USB cable is connected to the instrument and retry.&lt;BR /&gt;Initializing STARTUP command file:&lt;BR /&gt;CMDFILE STARTUP ON ".\cmd\SofTec_HCS12_startup.cmd"&lt;BR /&gt;Initializing RESET command file:&lt;BR /&gt;CMDFILE RESET ON ".\cmd\SofTec_HCS12_reset.cmd"&lt;BR /&gt;Initializing PRELOAD command file:&lt;BR /&gt;CMDFILE PRELOAD ON ".\cmd\SofTec_HCS12_preload.cmd"&lt;BR /&gt;Initializing POSTLOAD command file:&lt;BR /&gt;CMDFILE POSTLOAD ON ".\cmd\SofTec_HCS12_postload.cmd"&lt;BR /&gt;GDI: DiDirectCommand(communication)&lt;BR /&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;/P&gt;&lt;P&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;/P&gt;&lt;P&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;/P&gt;&lt;P&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;BR /&gt;==&amp;gt; DI_OK&lt;BR /&gt;GDI: DiDirectReadNoWait()==&amp;gt; DI_OK&lt;BR /&gt;GDI: DiDirectAddMenuItem()==&amp;gt; DI_OK&lt;BR /&gt;Error: The debugger is currently not able to run&lt;BR /&gt;due to loss of contact with hardware.&lt;BR /&gt;No Link To Target&lt;/P&gt;&lt;P&gt;in&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Aug 2012 23:26:39 GMT</pubDate>
    <dc:creator>schnapp</dc:creator>
    <dc:date>2012-08-10T23:26:39Z</dc:date>
    <item>
      <title>problem connecting to DEMO9S12XEP100</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-connecting-to-DEMO9S12XEP100/m-p/187926#M7155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm having&amp;nbsp;problems connecting to the DEMO9S12XEP100.&lt;/P&gt;&lt;P&gt;I followed all steps in the User Manual.&lt;/P&gt;&lt;P&gt;The board in standalone mode works fine, i.e. potentiometer and light sensor can be mapped to the LEDs by pushing the buttons.&lt;/P&gt;&lt;P&gt;I installed CodeWarrior Development Studio for S12(X) V5.1&lt;/P&gt;&lt;P&gt;I installed CW12 V5.1 Processor Expert v3.04 Sevice Pack from the DVD&lt;/P&gt;&lt;P&gt;I installed the "Additional Components" from the SofTec CD (there was also a service pack on there related to version 4.5 which I didn't install)&lt;/P&gt;&lt;P&gt;Driver installation after connecting the board via USB worked fine - there's no exclamation mark next to the driver in the device manager.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Problems start when I select Project&amp;gt;Debug in CodeWarrior.&lt;/P&gt;&lt;P&gt;I get an error message: "Communication Error. Make sure the USB cable is connected to the instrument and retry"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I restarted the application as well as the system, but also get the same error.&lt;/P&gt;&lt;P&gt;Later I enabled "Show Protocol" and got this:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;executing C_layout.hwl&lt;/P&gt;&lt;P&gt;!OPEN source 0 0 60 39&lt;BR /&gt;NO CONNECTION&lt;BR /&gt;!Source &amp;lt; attributes MARKS off&lt;BR /&gt;!OPEN assembly 60 0 40 31&lt;BR /&gt;!Assembly &amp;lt; attributes ADR on,CODE off,ABSADR on,SYMB off,TOPPC 0xF88C&lt;BR /&gt;!OPEN procedure 0 39 60 17&lt;BR /&gt;!Procedure &amp;lt; attributes VALUES on,TYPES off&lt;BR /&gt;!OPEN register 60 31 40 25&lt;BR /&gt;!Register &amp;lt; attributes FORMAT AUTO,COMPLEMENT None&lt;BR /&gt;!OPEN memory 60 56 40 22&lt;BR /&gt;!Memory &amp;lt; attributes FORMAT hex,COMPLEMENT None,WORD 1,ASC on,ADR on,ADDRESS 0x80&lt;BR /&gt;!OPEN data 0 56 60 22&lt;BR /&gt;!Data:1 &amp;lt; attributes SCOPE global,COMPLEMENT None,FORMAT Symb,MODE automatic,UPDATERATE 10,NAMEWIDTH 16&lt;BR /&gt;!OPEN data 0 78 60 22&lt;BR /&gt;!Data:2 &amp;lt; attributes SCOPE local,COMPLEMENT None,FORMAT Symb,MODE automatic,UPDATERATE 10,NAMEWIDTH 16&lt;BR /&gt;!OPEN command 60 78 40 22&lt;BR /&gt;!Command &amp;lt; attributes CACHESIZE 1000&lt;BR /&gt;!bckcolor 50331647&lt;BR /&gt;!font 'Courier New' 9 BLACK&lt;BR /&gt;!AUTOSIZE on&lt;BR /&gt;!ACTIVATE Data:2 Command Procedure Data:1 Source Register Assembly Memory&lt;BR /&gt;done C_layout.hwl&lt;/P&gt;&lt;P&gt;Loading Target ...&lt;BR /&gt;Communication settings:&lt;BR /&gt;SETCOMM DRIVER PROTOCOL NOPERIODICAL&lt;BR /&gt;Loading Communication DLL&lt;BR /&gt;==&amp;gt; C:\Programme\Freescale\CWS12v5.1\prog\gdi\softec_bdm12.dll&lt;BR /&gt;GDI: DiGdiOpen()==&amp;gt; DI_OK&lt;BR /&gt;GDI: DiGdiVersion()==&amp;gt; DI_OK&lt;BR /&gt;GDI: DiGdiGetFeatures()==&amp;gt; DI_OK&lt;BR /&gt;GDI: DiGdiAddCallBack(8192)==&amp;gt; DI_OK&lt;BR /&gt;GDI: DiGdiAddCallBack(16384)==&amp;gt; DI_OK&lt;BR /&gt;GDI: DiCommGetAcceptableSettings()==&amp;gt; 0&lt;BR /&gt;Initializing STARTUP command file:&lt;BR /&gt;CMDFILE STARTUP ON ".\cmd\SofTec_HCS12_startup.cmd"&lt;BR /&gt;Initializing RESET command file:&lt;BR /&gt;CMDFILE RESET ON ".\cmd\SofTec_HCS12_reset.cmd"&lt;BR /&gt;Initializing PRELOAD command file:&lt;BR /&gt;CMDFILE PRELOAD ON ".\cmd\SofTec_HCS12_preload.cmd"&lt;BR /&gt;Initializing POSTLOAD command file:&lt;BR /&gt;CMDFILE POSTLOAD ON ".\cmd\SofTec_HCS12_postload.cmd"&lt;BR /&gt;GDI: DiGdiInitIO()&lt;BR /&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_HASCOMMUNICATIONCMD)&lt;BR /&gt;GDI: DiGdiVersion()==&amp;gt; DI_OK&lt;/P&gt;&lt;P&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;/P&gt;&lt;P&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;/P&gt;&lt;P&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;/P&gt;&lt;P&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;/P&gt;&lt;P&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;BR /&gt;==&amp;gt; DI_ERR_FATAL&lt;BR /&gt;GDI: DiErrorGetMessage()==&amp;gt; 1&lt;BR /&gt;GDI: Error Message ==&amp;gt; Communication error. Make sure that the USB cable is connected to the instrument and retry.&lt;BR /&gt;Initializing STARTUP command file:&lt;BR /&gt;CMDFILE STARTUP ON ".\cmd\SofTec_HCS12_startup.cmd"&lt;BR /&gt;Initializing RESET command file:&lt;BR /&gt;CMDFILE RESET ON ".\cmd\SofTec_HCS12_reset.cmd"&lt;BR /&gt;Initializing PRELOAD command file:&lt;BR /&gt;CMDFILE PRELOAD ON ".\cmd\SofTec_HCS12_preload.cmd"&lt;BR /&gt;Initializing POSTLOAD command file:&lt;BR /&gt;CMDFILE POSTLOAD ON ".\cmd\SofTec_HCS12_postload.cmd"&lt;BR /&gt;GDI: DiDirectCommand(communication)&lt;BR /&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;/P&gt;&lt;P&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;/P&gt;&lt;P&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;/P&gt;&lt;P&gt;GDI DLL called: DI_CB_MTWKS_EXTENSION_Callback(MTWKS_CB_PROJECTACCESS)&lt;BR /&gt;==&amp;gt; DI_OK&lt;BR /&gt;GDI: DiDirectReadNoWait()==&amp;gt; DI_OK&lt;BR /&gt;GDI: DiDirectAddMenuItem()==&amp;gt; DI_OK&lt;BR /&gt;Error: The debugger is currently not able to run&lt;BR /&gt;due to loss of contact with hardware.&lt;BR /&gt;No Link To Target&lt;/P&gt;&lt;P&gt;in&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Aug 2012 23:26:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-connecting-to-DEMO9S12XEP100/m-p/187926#M7155</guid>
      <dc:creator>schnapp</dc:creator>
      <dc:date>2012-08-10T23:26:39Z</dc:date>
    </item>
  </channel>
</rss>