<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックMC9S12C32 - interrupt table</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12C32-interrupt-table/m-p/127243#M655</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;I am attempting to setup the port p interrupt on a MC9S12C32 process (NanoCore from technological arts) as shown below.&amp;nbsp; I am trying to use the interrupt to read in a 1 Hz signal from a Real Time Clock therefore, I set Port P up as an input and enabled the interrupt inside the PIEP register (although just to write the declaration I should not even need to do this).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;interrupt 56 void 1Hz_handler(void) // port P5&lt;BR /&gt;// ENABLED:&lt;BR /&gt;// PURPOSE:&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;}&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV&gt;I keep getting an error stating that this is an invalid number.&amp;nbsp; I have counted up in the vector table several times and I keep getting Vportp to be 56.&amp;nbsp; Has anybody used the port p vectors?&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;--&lt;BR /&gt;Alban Edit: Part number in subject line&lt;/P&gt;&lt;P&gt;Message Edited by Alban on &lt;SPAN class="date_text"&gt;2007-03-21&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;03:33 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Mar 2007 01:33:00 GMT</pubDate>
    <dc:creator>randy_s_woods</dc:creator>
    <dc:date>2007-03-21T01:33:00Z</dc:date>
    <item>
      <title>MC9S12C32 - interrupt table</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12C32-interrupt-table/m-p/127243#M655</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;I am attempting to setup the port p interrupt on a MC9S12C32 process (NanoCore from technological arts) as shown below.&amp;nbsp; I am trying to use the interrupt to read in a 1 Hz signal from a Real Time Clock therefore, I set Port P up as an input and enabled the interrupt inside the PIEP register (although just to write the declaration I should not even need to do this).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;interrupt 56 void 1Hz_handler(void) // port P5&lt;BR /&gt;// ENABLED:&lt;BR /&gt;// PURPOSE:&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;}&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV&gt;I keep getting an error stating that this is an invalid number.&amp;nbsp; I have counted up in the vector table several times and I keep getting Vportp to be 56.&amp;nbsp; Has anybody used the port p vectors?&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;--&lt;BR /&gt;Alban Edit: Part number in subject line&lt;/P&gt;&lt;P&gt;Message Edited by Alban on &lt;SPAN class="date_text"&gt;2007-03-21&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;03:33 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2007 01:33:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12C32-interrupt-table/m-p/127243#M655</guid>
      <dc:creator>randy_s_woods</dc:creator>
      <dc:date>2007-03-21T01:33:00Z</dc:date>
    </item>
    <item>
      <title>Re: interrupt table</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12C32-interrupt-table/m-p/127244#M656</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Just a little more clarification.&amp;nbsp; When I looked in the Device user guide (MC9S12C32) it shows up as interrupt 37 when the reserved interrupts are removed from the counting.&amp;nbsp; I attempted to use 37 as the interrpt and this gives the same error "C2704:&amp;nbsp;Illegal&amp;nbsp;number".&amp;nbsp; When I looked&amp;nbsp;at the code warrior file&amp;nbsp;mc9s12c32.inc the interrupt would be 57.&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2007 02:14:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12C32-interrupt-table/m-p/127244#M656</guid>
      <dc:creator>randy_s_woods</dc:creator>
      <dc:date>2007-03-21T02:14:51Z</dc:date>
    </item>
    <item>
      <title>Re: interrupt table</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12C32-interrupt-table/m-p/127245#M657</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;P&gt;&lt;SPAN&gt;Woops! 1Hz_handler is not a valid name.....&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2007 02:42:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12C32-interrupt-table/m-p/127245#M657</guid>
      <dc:creator>randy_s_woods</dc:creator>
      <dc:date>2007-03-21T02:42:35Z</dc:date>
    </item>
  </channel>
</rss>