<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RAM Loader in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/RAM-Loader/m-p/178498#M6385</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the main application that is in FLASH, when I send a sequesce of commands I want to load from UART a loader that will be saved to RAM and at the and of uploading I decide the address to be called to run the main funcrion of the LOADER in RAM. My question is, how can I set codewarrior to compile my application all(CODE/DATA) for RAM?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Jul 2012 21:34:20 GMT</pubDate>
    <dc:creator>Mr32Bit</dc:creator>
    <dc:date>2012-07-09T21:34:20Z</dc:date>
    <item>
      <title>RAM Loader</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/RAM-Loader/m-p/178498#M6385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the main application that is in FLASH, when I send a sequesce of commands I want to load from UART a loader that will be saved to RAM and at the and of uploading I decide the address to be called to run the main funcrion of the LOADER in RAM. My question is, how can I set codewarrior to compile my application all(CODE/DATA) for RAM?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jul 2012 21:34:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/RAM-Loader/m-p/178498#M6385</guid>
      <dc:creator>Mr32Bit</dc:creator>
      <dc:date>2012-07-09T21:34:20Z</dc:date>
    </item>
  </channel>
</rss>