<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S12X CAN bus timing in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12X-CAN-bus-timing/m-p/171232#M5770</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm currently setting up the CANbus on a S12XEP100. I've use the code coming with the dev board to start with and see how everything work. i'm using a kvaser CanKing as logger. I achieve to get clear data at 125 kb/s and 250 kb/s but when i tried to increase the speed I only get error frame...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For 125 kb/s I used those value :&lt;/P&gt;&lt;P&gt;BTR0=0x07&lt;/P&gt;&lt;P&gt;BTR1=0x3a&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For 250kb/s I used those value :&lt;/P&gt;&lt;P&gt;BTR0=0x03&lt;/P&gt;&lt;P&gt;BTR1=0x3a&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i tried 500 kb/s with those value&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BTR0=0x01&lt;/P&gt;&lt;P&gt;BTR1=0x3a&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i also tried the using the setting from the device inituialization tools but get the same problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Dec 2010 06:22:03 GMT</pubDate>
    <dc:creator>Pascalfm</dc:creator>
    <dc:date>2010-12-21T06:22:03Z</dc:date>
    <item>
      <title>S12X CAN bus timing</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12X-CAN-bus-timing/m-p/171232#M5770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm currently setting up the CANbus on a S12XEP100. I've use the code coming with the dev board to start with and see how everything work. i'm using a kvaser CanKing as logger. I achieve to get clear data at 125 kb/s and 250 kb/s but when i tried to increase the speed I only get error frame...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For 125 kb/s I used those value :&lt;/P&gt;&lt;P&gt;BTR0=0x07&lt;/P&gt;&lt;P&gt;BTR1=0x3a&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For 250kb/s I used those value :&lt;/P&gt;&lt;P&gt;BTR0=0x03&lt;/P&gt;&lt;P&gt;BTR1=0x3a&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i tried 500 kb/s with those value&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BTR0=0x01&lt;/P&gt;&lt;P&gt;BTR1=0x3a&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i also tried the using the setting from the device inituialization tools but get the same problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Dec 2010 06:22:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12X-CAN-bus-timing/m-p/171232#M5770</guid>
      <dc:creator>Pascalfm</dc:creator>
      <dc:date>2010-12-21T06:22:03Z</dc:date>
    </item>
    <item>
      <title>Re: S12X CAN bus timing</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12X-CAN-bus-timing/m-p/171233#M5771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Maybe your bus driver is too slow for 500kbps, or maybe bus is not properly terminated?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Dec 2010 15:06:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12X-CAN-bus-timing/m-p/171233#M5771</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-12-21T15:06:56Z</dc:date>
    </item>
    <item>
      <title>Re: S12X CAN bus timing</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12X-CAN-bus-timing/m-p/171234#M5772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you are right, it's the transceiver speed I totally forgot about that one&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I change the chip and everything is right now&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Dec 2010 01:05:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12X-CAN-bus-timing/m-p/171234#M5772</guid>
      <dc:creator>Pascalfm</dc:creator>
      <dc:date>2010-12-22T01:05:56Z</dc:date>
    </item>
  </channel>
</rss>