<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC9S12XEP100 : ATD Resoltuion is 19.53mv with 8bit data, but LM35 has 10mv per degree celsius in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12XEP100-ATD-Resoltuion-is-19-53mv-with-8bit-data-but-LM35/m-p/171014#M5745</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Simple. Use&amp;nbsp;10 or 12bits ATD resolution.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Dec 2010 01:19:28 GMT</pubDate>
    <dc:creator>kef</dc:creator>
    <dc:date>2010-12-21T01:19:28Z</dc:date>
    <item>
      <title>MC9S12XEP100 : ATD Resoltuion is 19.53mv with 8bit data, but LM35 has 10mv per degree celsius</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12XEP100-ATD-Resoltuion-is-19-53mv-with-8bit-data-but-LM35/m-p/171013#M5744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to use LM35 temperature sensor on AN1 port of ATD0. But I wanted to convert the value from the ATD to the temperature value for which I can print on the LCD display. But LM35 has resolution of 10mv per degree celsius and ATD (8 bit resolution, VDD = 5v) has 19.53mv. Hence I how can I know whats the temperature in degree celsius? I dont want to use power supply of 3.3v but only 5v. I have to make the ATD resolution as well 10mv per degree celsius.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Looking for some inputs / suggestions&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Darshan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Dec 2010 23:41:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12XEP100-ATD-Resoltuion-is-19-53mv-with-8bit-data-but-LM35/m-p/171013#M5744</guid>
      <dc:creator>Darshan_The_Gee</dc:creator>
      <dc:date>2010-12-20T23:41:07Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S12XEP100 : ATD Resoltuion is 19.53mv with 8bit data, but LM35 has 10mv per degree celsius</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12XEP100-ATD-Resoltuion-is-19-53mv-with-8bit-data-but-LM35/m-p/171014#M5745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Simple. Use&amp;nbsp;10 or 12bits ATD resolution.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Dec 2010 01:19:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12XEP100-ATD-Resoltuion-is-19-53mv-with-8bit-data-but-LM35/m-p/171014#M5745</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-12-21T01:19:28Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S12XEP100 : ATD Resoltuion is 19.53mv with 8bit data, but LM35 has 10mv per degree celsius</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12XEP100-ATD-Resoltuion-is-19-53mv-with-8bit-data-but-LM35/m-p/171015#M5746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Darshan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you use 10-bit resolution, as Kef suggested, this will result in a resolution of 4.88mV, or slightly less than 0.5 degree.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you then wished to adjust the resolution to exactly 0.5 degree C, to simplify the calculation process, you could place a resistive voltage divider between the temperature sensor and the ATD input.&amp;nbsp; This might consist of a 820 ohm series resistor, and a 33k shunt resistor, and would provide a voltage change of 9.76mV per degree C at the ATD input.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Dec 2010 03:35:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12XEP100-ATD-Resoltuion-is-19-53mv-with-8bit-data-but-LM35/m-p/171015#M5746</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-12-21T03:35:54Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S12XEP100 : ATD Resoltuion is 19.53mv with 8bit data, but LM35 has 10mv per degree celsius</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12XEP100-ATD-Resoltuion-is-19-53mv-with-8bit-data-but-LM35/m-p/171016#M5747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;XEP100 has 1MB of flash. Conversion from ADC reading to integer degC costs well under 20 bytes of code and&amp;nbsp;about 10&amp;nbsp; bus cycles...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Dec 2010 04:17:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12XEP100-ATD-Resoltuion-is-19-53mv-with-8bit-data-but-LM35/m-p/171016#M5747</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-12-21T04:17:35Z</dc:date>
    </item>
  </channel>
</rss>