<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Drop in replacement for NE64 in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Drop-in-replacement-for-NE64/m-p/126690#M568</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I heard someone say there is a Coldfire drop in replacement for this NE64, is that true?&lt;/DIV&gt;&lt;DIV&gt;I know I'll need a new tool chain to code for it... if I did such a thing can I debug it using the same BDM module I've been using? (USB MultiLink by P&amp;amp;e)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Aug 2006 15:14:29 GMT</pubDate>
    <dc:creator>Spaceball1</dc:creator>
    <dc:date>2006-08-14T15:14:29Z</dc:date>
    <item>
      <title>Drop in replacement for NE64</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Drop-in-replacement-for-NE64/m-p/126690#M568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I heard someone say there is a Coldfire drop in replacement for this NE64, is that true?&lt;/DIV&gt;&lt;DIV&gt;I know I'll need a new tool chain to code for it... if I did such a thing can I debug it using the same BDM module I've been using? (USB MultiLink by P&amp;amp;e)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Aug 2006 15:14:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Drop-in-replacement-for-NE64/m-p/126690#M568</guid>
      <dc:creator>Spaceball1</dc:creator>
      <dc:date>2006-08-14T15:14:29Z</dc:date>
    </item>
    <item>
      <title>Re: Drop in replacement for NE64</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Drop-in-replacement-for-NE64/m-p/126691#M569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi&lt;BR /&gt;&lt;BR /&gt;The M5223X is available in 112 and 80 pin LQFP housings which are 'almost' compatible with the NE64 (without extrenal memory interface).&lt;BR /&gt;The main differences are due to JTAG and BDM which are different in the two devices.&lt;BR /&gt;It is therefore not possible to take a NE64 board and solder a M5223X in since its BDM interface requires a mod. but a NE64 board can be very easily modified to 'upgrade' to the ColdFire.&lt;BR /&gt;&lt;BR /&gt;See also the following postings showing how the uTasker (operating system with integrated TCP/IP stack and chip simulator) supports both NE64 and M5223X, enabling NE64 projects to be rebuilt of the M5223X by simply changing a compiler setting.&lt;BR /&gt;&lt;A href="http://forums.freescale.com/freescale/board/message?board.id=16BITCOMM&amp;amp;message.id=897" target="test_blank"&gt;http://forums.freescale.com/freescale/board/message?board.id=16BITCOMM&amp;amp;message.id=897&lt;/A&gt;&lt;BR /&gt;&lt;A href="http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&amp;amp;message.id=274" target="test_blank"&gt;http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&amp;amp;message.id=274&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Note that the uTasker now supports also CAN for the M5223X - see following doc:&lt;BR /&gt;&lt;A href="http://www.mjbc.ch/documents/uTasker/uTaskerCAN.PDF" target="test_blank"&gt;http://www.mjbc.ch/documents/uTasker/uTaskerCAN.PDF&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;The ColdFire evaluation boards are delivered with the USB ColdFire MULTILINK P&amp;amp;E with a 26 pin connector. If you buy the M52233DEMO costing $99 from freescale it includes the same BDM integrated into the board and also a 128k limited version of CodeWarrior.&lt;BR /&gt;&lt;BR /&gt;Since the NE64 uses a two wire BDM it is probable that your present BDM is not the same but maybe it does work with the correct connector(?).&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark Butcher&lt;BR /&gt;&lt;A href="https://community.nxp.com/www.mjbc.ch" target="test_blank"&gt;www.mjbc.ch&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Aug 2006 19:52:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Drop-in-replacement-for-NE64/m-p/126691#M569</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2006-08-14T19:52:38Z</dc:date>
    </item>
  </channel>
</rss>