<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Freescale MC9S12DP256B - Enhanced Capture Timer Module in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Freescale-MC9S12DP256B-Enhanced-Capture-Timer-Module/m-p/169531#M5614</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In my system, the Adapt9S12DP256 board will have to monitor the serial port and keep track the feedback encoder and at the same time produce step pulses to drive the motor driver. So program plan is as follows:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1.&amp;nbsp; Main program will keep track on the serial port and calculation will be conducted to calculate the number of step to drive the driver and the frequency as well. The number of step and frequency will be used in ECT module.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2.&amp;nbsp; At the same time, output compare and input capture will be used to drive the driver and count the feedback encoder respectively.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;So, is it possible to use PWM module to produce the step pulses rather than Output Compare module in my case?&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Below is the simple code to on and off two LEDs which are LED (PTP7) on my Adapt9S12DP256 board and external LED using PTT7/IOC7 every 0.5second. Just want to know whether my understanding on programming the interrupt module for two LEDs correct or not . I haven try this code because I think I left something else. Please correct me if the code is wrong.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;DIV class="msg_source_code"&gt;&lt;DIV class="text_smallest"&gt;Code:&lt;/DIV&gt;&lt;PRE&gt;#include &amp;lt;mc9s12dp256.h&amp;gt;

void TOC7_Init(void)
{&amp;nbsp; asm sei

&amp;nbsp;&amp;nbsp;&amp;nbsp; TIOS=0x80;&amp;nbsp;&amp;nbsp;&amp;nbsp; // IOS7 = 1, channel 7 is output compare
&amp;nbsp;&amp;nbsp;&amp;nbsp; TCTL1=0x40;&amp;nbsp;&amp;nbsp; // OM7 = 0, OL7 = 1, Toggle output on PTT7/IOC7
&amp;nbsp;&amp;nbsp;&amp;nbsp; TSCR2=0x0F;&amp;nbsp;&amp;nbsp; // TCRE = 1, counter reset enable
&amp;nbsp;&amp;nbsp;&amp;nbsp; // Prescaler = 128 (Timer clock freq = 25MHz/128 = 195.31kHz)

&amp;nbsp;&amp;nbsp;&amp;nbsp; TC7=48828;&amp;nbsp;&amp;nbsp;&amp;nbsp; // LED on/off duration = 48828/195.31kHz = 0.25s
&amp;nbsp;&amp;nbsp;&amp;nbsp; TIE=0x80;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Timer interrupt enable, C7I=1
&amp;nbsp;&amp;nbsp;&amp;nbsp; TSCR1=0x90;&amp;nbsp;&amp;nbsp; // Timer enable TEN=1, fast flag clear TFFCA=1
&amp;nbsp;&amp;nbsp; 
&amp;nbsp;&amp;nbsp;&amp;nbsp; asm cli;
}

void main()
{
&amp;nbsp;&amp;nbsp;&amp;nbsp; TOC7_Init();

&amp;nbsp;&amp;nbsp;&amp;nbsp; DDRP=0xFF;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Port P as output
&amp;nbsp;&amp;nbsp;&amp;nbsp; PTP=0x00;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Initialize LED off
}

// definition
#pragma interrupt_handler TOC7_ISR(); 
void TOC7_ISR(void)
{
&amp;nbsp;&amp;nbsp;&amp;nbsp; PTP ^= 0x80;&amp;nbsp; // Toggle output bit (PTP7)
}

// interrupt vector declaration
extern void TOC7_ISR();
#pragma abs_address:0xffee;
void (* TOC7_handler[])() = { TOC7_ISR };
#pragma end_abs_address
&lt;/PRE&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;/DIV&gt;&lt;STRONG&gt;I need help on this:&lt;BR /&gt;1.&amp;nbsp; Is the definition and vector declaration of the TOC7_ISR correct ?&lt;BR /&gt;2.&amp;nbsp; Should I include vectors.c file?&lt;BR /&gt;3.&amp;nbsp; "#pragma abs_address:0xffee"&amp;nbsp; Where is the 'ffee' address based on? As I know, the vector address for ECT channel 7 in the datasheet is ffe0.&lt;BR /&gt;4.&amp;nbsp; How to set the bus clock to the ECT module ? In this example, I assume it to be 25MHz.&lt;BR /&gt;5.&amp;nbsp; What is 'asm sei' and 'asm cli' ?&lt;BR /&gt;6.&amp;nbsp; Will the PTT7/IOC7 output toggle automatically when interrupt occur?&lt;BR /&gt;7.&amp;nbsp; I have enabled the counter reset. So I don't have to add&amp;nbsp; "TC7 +=&lt;/STRONG&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;STRONG&gt;48828&lt;/STRONG&gt;&lt;SPAN&gt;" &lt;/SPAN&gt;&lt;STRONG&gt;in my ISR because the counter will reset once it match TC7=48828 and interrupt occur. Then it will count again to cause the next interrupt. ( Please correct me if I'm wrong )&lt;/STRONG&gt;&lt;BR /&gt;&lt;PRE&gt;
Your help is highly appreciated.
&lt;/PRE&gt;&lt;SPAN&gt;Thanks in advance.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;best regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;yj&lt;/SPAN&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Message Edited by yj on &lt;/SPAN&gt;&lt;SPAN class="date_text"&gt;2007-12-03&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;01:17 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Oct 2020 09:17:32 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2020-10-29T09:17:32Z</dc:date>
    <item>
      <title>Freescale MC9S12DP256B - Enhanced Capture Timer Module</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Freescale-MC9S12DP256B-Enhanced-Capture-Timer-Module/m-p/169531#M5614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In my system, the Adapt9S12DP256 board will have to monitor the serial port and keep track the feedback encoder and at the same time produce step pulses to drive the motor driver. So program plan is as follows:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1.&amp;nbsp; Main program will keep track on the serial port and calculation will be conducted to calculate the number of step to drive the driver and the frequency as well. The number of step and frequency will be used in ECT module.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2.&amp;nbsp; At the same time, output compare and input capture will be used to drive the driver and count the feedback encoder respectively.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;So, is it possible to use PWM module to produce the step pulses rather than Output Compare module in my case?&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Below is the simple code to on and off two LEDs which are LED (PTP7) on my Adapt9S12DP256 board and external LED using PTT7/IOC7 every 0.5second. Just want to know whether my understanding on programming the interrupt module for two LEDs correct or not . I haven try this code because I think I left something else. Please correct me if the code is wrong.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;DIV class="msg_source_code"&gt;&lt;DIV class="text_smallest"&gt;Code:&lt;/DIV&gt;&lt;PRE&gt;#include &amp;lt;mc9s12dp256.h&amp;gt;

void TOC7_Init(void)
{&amp;nbsp; asm sei

&amp;nbsp;&amp;nbsp;&amp;nbsp; TIOS=0x80;&amp;nbsp;&amp;nbsp;&amp;nbsp; // IOS7 = 1, channel 7 is output compare
&amp;nbsp;&amp;nbsp;&amp;nbsp; TCTL1=0x40;&amp;nbsp;&amp;nbsp; // OM7 = 0, OL7 = 1, Toggle output on PTT7/IOC7
&amp;nbsp;&amp;nbsp;&amp;nbsp; TSCR2=0x0F;&amp;nbsp;&amp;nbsp; // TCRE = 1, counter reset enable
&amp;nbsp;&amp;nbsp;&amp;nbsp; // Prescaler = 128 (Timer clock freq = 25MHz/128 = 195.31kHz)

&amp;nbsp;&amp;nbsp;&amp;nbsp; TC7=48828;&amp;nbsp;&amp;nbsp;&amp;nbsp; // LED on/off duration = 48828/195.31kHz = 0.25s
&amp;nbsp;&amp;nbsp;&amp;nbsp; TIE=0x80;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Timer interrupt enable, C7I=1
&amp;nbsp;&amp;nbsp;&amp;nbsp; TSCR1=0x90;&amp;nbsp;&amp;nbsp; // Timer enable TEN=1, fast flag clear TFFCA=1
&amp;nbsp;&amp;nbsp; 
&amp;nbsp;&amp;nbsp;&amp;nbsp; asm cli;
}

void main()
{
&amp;nbsp;&amp;nbsp;&amp;nbsp; TOC7_Init();

&amp;nbsp;&amp;nbsp;&amp;nbsp; DDRP=0xFF;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Port P as output
&amp;nbsp;&amp;nbsp;&amp;nbsp; PTP=0x00;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Initialize LED off
}

// definition
#pragma interrupt_handler TOC7_ISR(); 
void TOC7_ISR(void)
{
&amp;nbsp;&amp;nbsp;&amp;nbsp; PTP ^= 0x80;&amp;nbsp; // Toggle output bit (PTP7)
}

// interrupt vector declaration
extern void TOC7_ISR();
#pragma abs_address:0xffee;
void (* TOC7_handler[])() = { TOC7_ISR };
#pragma end_abs_address
&lt;/PRE&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;/DIV&gt;&lt;STRONG&gt;I need help on this:&lt;BR /&gt;1.&amp;nbsp; Is the definition and vector declaration of the TOC7_ISR correct ?&lt;BR /&gt;2.&amp;nbsp; Should I include vectors.c file?&lt;BR /&gt;3.&amp;nbsp; "#pragma abs_address:0xffee"&amp;nbsp; Where is the 'ffee' address based on? As I know, the vector address for ECT channel 7 in the datasheet is ffe0.&lt;BR /&gt;4.&amp;nbsp; How to set the bus clock to the ECT module ? In this example, I assume it to be 25MHz.&lt;BR /&gt;5.&amp;nbsp; What is 'asm sei' and 'asm cli' ?&lt;BR /&gt;6.&amp;nbsp; Will the PTT7/IOC7 output toggle automatically when interrupt occur?&lt;BR /&gt;7.&amp;nbsp; I have enabled the counter reset. So I don't have to add&amp;nbsp; "TC7 +=&lt;/STRONG&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;STRONG&gt;48828&lt;/STRONG&gt;&lt;SPAN&gt;" &lt;/SPAN&gt;&lt;STRONG&gt;in my ISR because the counter will reset once it match TC7=48828 and interrupt occur. Then it will count again to cause the next interrupt. ( Please correct me if I'm wrong )&lt;/STRONG&gt;&lt;BR /&gt;&lt;PRE&gt;
Your help is highly appreciated.
&lt;/PRE&gt;&lt;SPAN&gt;Thanks in advance.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;best regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;yj&lt;/SPAN&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Message Edited by yj on &lt;/SPAN&gt;&lt;SPAN class="date_text"&gt;2007-12-03&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;01:17 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 09:17:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Freescale-MC9S12DP256B-Enhanced-Capture-Timer-Module/m-p/169531#M5614</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2020-10-29T09:17:32Z</dc:date>
    </item>
    <item>
      <title>Re: Freescale MC9S12DP256B - Enhanced Capture Timer Module</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Freescale-MC9S12DP256B-Enhanced-Capture-Timer-Module/m-p/169532#M5615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello yj,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;This post also appears to be present within another thread.&amp;nbsp; Please do not duplicate your posts.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Dec 2007 09:28:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Freescale-MC9S12DP256B-Enhanced-Capture-Timer-Module/m-p/169532#M5615</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2007-12-03T09:28:54Z</dc:date>
    </item>
    <item>
      <title>Re: Freescale MC9S12DP256B - Enhanced Capture Timer Module</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Freescale-MC9S12DP256B-Enhanced-Capture-Timer-Module/m-p/169533#M5616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&amp;nbsp;y not supply the link then...?&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Dec 2007 13:17:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Freescale-MC9S12DP256B-Enhanced-Capture-Timer-Module/m-p/169533#M5616</guid>
      <dc:creator>Xbot</dc:creator>
      <dc:date>2007-12-06T13:17:12Z</dc:date>
    </item>
  </channel>
</rss>