<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックFlexray Frames Configuration</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray-Frames-Configuration/m-p/169199#M5604</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working with the Freescale Development Card EVB9S12XF512E. For making an communication between two flexray nodes, it needs to configuration the network.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In fact, there is a function which did that in freescale example :&lt;/P&gt;&lt;PRE&gt;/* Structure of this type contains configuration&amp;nbsp;&amp;nbsp; information of the one low level parameters set */const Fr_low_level_config_type Fr_low_level_cfg_set_00 ={&amp;nbsp;&amp;nbsp;&amp;nbsp; ..........&amp;nbsp;&amp;nbsp;&amp;nbsp; 5000,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* G_MACRO_PER_CYCLE */&amp;nbsp;&amp;nbsp;&amp;nbsp; 10,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* G_MAX_WITHOUT_CLOCK_CORRECTION_PASSIVE */&amp;nbsp;&amp;nbsp;&amp;nbsp; 14,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* G_MAX_WITHOUT_CLOCK_CORRECTION_FATAL */&amp;nbsp;&amp;nbsp;&amp;nbsp; 22,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* G_NUMBER_OF_MINISLOTS */&amp;nbsp;&amp;nbsp;&amp;nbsp; 60,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* G_NUMBER_OF_STATIC_SLOTS */&amp;nbsp;&amp;nbsp;&amp;nbsp; 4920,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* G_OFFSET_CORRECTION_START */&amp;nbsp;&amp;nbsp;&amp;nbsp; 16,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* G_PAYLOAD_LENGTH_STATIC */&amp;nbsp;&amp;nbsp;&amp;nbsp; ..........}&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;I would like to know if I'm understanding well something.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The argument G_PAYLOAD_LENGTH_STATIC represent the duration of a static frame, that right?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In my example, the argument is put at 16. That mean I can send at maximum 16 byte of data in my Flexray frames?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks you in advance for your answers, because i really need to know if am right to continu my project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Oct 2020 09:17:05 GMT</pubDate>
    <dc:creator>Kartoon67</dc:creator>
    <dc:date>2020-10-29T09:17:05Z</dc:date>
    <item>
      <title>Flexray Frames Configuration</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray-Frames-Configuration/m-p/169199#M5604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working with the Freescale Development Card EVB9S12XF512E. For making an communication between two flexray nodes, it needs to configuration the network.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In fact, there is a function which did that in freescale example :&lt;/P&gt;&lt;PRE&gt;/* Structure of this type contains configuration&amp;nbsp;&amp;nbsp; information of the one low level parameters set */const Fr_low_level_config_type Fr_low_level_cfg_set_00 ={&amp;nbsp;&amp;nbsp;&amp;nbsp; ..........&amp;nbsp;&amp;nbsp;&amp;nbsp; 5000,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* G_MACRO_PER_CYCLE */&amp;nbsp;&amp;nbsp;&amp;nbsp; 10,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* G_MAX_WITHOUT_CLOCK_CORRECTION_PASSIVE */&amp;nbsp;&amp;nbsp;&amp;nbsp; 14,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* G_MAX_WITHOUT_CLOCK_CORRECTION_FATAL */&amp;nbsp;&amp;nbsp;&amp;nbsp; 22,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* G_NUMBER_OF_MINISLOTS */&amp;nbsp;&amp;nbsp;&amp;nbsp; 60,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* G_NUMBER_OF_STATIC_SLOTS */&amp;nbsp;&amp;nbsp;&amp;nbsp; 4920,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* G_OFFSET_CORRECTION_START */&amp;nbsp;&amp;nbsp;&amp;nbsp; 16,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* G_PAYLOAD_LENGTH_STATIC */&amp;nbsp;&amp;nbsp;&amp;nbsp; ..........}&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;I would like to know if I'm understanding well something.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The argument G_PAYLOAD_LENGTH_STATIC represent the duration of a static frame, that right?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In my example, the argument is put at 16. That mean I can send at maximum 16 byte of data in my Flexray frames?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks you in advance for your answers, because i really need to know if am right to continu my project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 09:17:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray-Frames-Configuration/m-p/169199#M5604</guid>
      <dc:creator>Kartoon67</dc:creator>
      <dc:date>2020-10-29T09:17:05Z</dc:date>
    </item>
    <item>
      <title>Re: Flexray Frames Configuration</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray-Frames-Configuration/m-p/169200#M5605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The payload length is in words I think. 16 words=32 bytes. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 May 2016 15:15:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray-Frames-Configuration/m-p/169200#M5605</guid>
      <dc:creator>bobgardner</dc:creator>
      <dc:date>2016-05-11T15:15:51Z</dc:date>
    </item>
    <item>
      <title>Re: Flexray Frames Configuration</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray-Frames-Configuration/m-p/2164986#M20730</link>
      <description>Me too!!!!!!!!!&lt;BR /&gt;can you tell me how to deal with it?&lt;BR /&gt;</description>
      <pubDate>Mon, 08 Sep 2025 07:53:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray-Frames-Configuration/m-p/2164986#M20730</guid>
      <dc:creator>juunna</dc:creator>
      <dc:date>2025-09-08T07:53:35Z</dc:date>
    </item>
  </channel>
</rss>