<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: Programming multiple ppages MC9S12DP512</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Programming-multiple-ppages-MC9S12DP512/m-p/166194#M5403</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I deeply appreciate the org $4000 clue by kef. However, it took some work to flesh out the details. This note may help&lt;BR /&gt;others with a similar problem. All the unpaged org $4000 and org $C000 code, along with the vector table additions,&lt;BR /&gt;can be converted together by SRecCvt-Gui with settings input=banked, output=linear and then downloaded to Flash with&lt;BR /&gt;the Serial BootLoader. Other paged code, like $22, need the "Linear $4000-$FFFF to paged" box checked in SRecCvt-Gui&lt;BR /&gt;and downloaded with BDM POD using LOAD or FLOAD and the proper offset. Conversion of paged .S19 files with SRecCvt-Gui generates S2 addresses = 80000. On loading, an offset must be added to place the code in the proper linear address range in memory. Example, 80000 + offset 54000 =&amp;nbsp; linear address $D4000 for page $35.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Dec 2010 21:53:26 GMT</pubDate>
    <dc:creator>astro_goto</dc:creator>
    <dc:date>2010-12-08T21:53:26Z</dc:date>
    <item>
      <title>Programming multiple ppages MC9S12DP512</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Programming-multiple-ppages-MC9S12DP512/m-p/166192#M5401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My "goto" telescope built around an MC9S12DP512 programmed in assembly is working just great! The program uses floating point routines from AN974 and occupies 11463 bytes of unpaged memory (ppage $3F) plus 12745 bytes in ppage $22.&amp;nbsp; The unpaged code loads with the S12Dx512 Boot-loader v1.0.1 and a BDM POD loads ppage $22 with D-Bug12 4.0.b32 using the FLOAD 8000 ;np command. I know how to calculate the FLOAD addresses for other ppages.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;However, I am needing to write more code beyond the ~3600 bytes remaining in ppage $22 and am uncertain how to proceed.&amp;nbsp; The program uses an ORG $C000 for the unpaged Fixed Flash Array (ppage $3F) and ORG $8000 for the code in ppage $22. The last byte of code in ppage $22 must&amp;nbsp; load in $BFFF.&amp;nbsp; Anymore code will just overlap the stuff at ORG $C000. The additional proposed code must access global variables and subroutines in ppage $3F and also subroutines in ppage $22. How to calculate an ORG statement for additional ppages of code when the FTS512K4 User Guide says that ppages $20 through $3E must be accessed through the 16K window $8000-$BFFF as I'm doing for ppage $22 ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My development tool is MGTEK's MiniIDE running on a laptop PC. Downloading to the MC9SDP512 flash is with HyperTerminal.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Dec 2010 07:51:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Programming-multiple-ppages-MC9S12DP512/m-p/166192#M5401</guid>
      <dc:creator>astro_goto</dc:creator>
      <dc:date>2010-12-01T07:51:44Z</dc:date>
    </item>
    <item>
      <title>Re: Programming multiple ppages MC9S12DP512</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Programming-multiple-ppages-MC9S12DP512/m-p/166193#M5402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;page $3E is also fixed unpaged page (like paae $3F) available at $4000.&lt;/P&gt;&lt;P&gt;You could org all your code to start at $4000 and end at $Fxxx, including page window $8000-$BFFF. Reset default PPAGE value on S12 parts is 0.&amp;nbsp;In single chip modes, PPAGE=0 maps the least available page to page window. PPAGE=0 on S12DP512 is the same like PPAGE=$20, PPAGE=1 the same like PPAGE=$21 etc, only 5 least order bits of PPAGE are used. Hovewer breakpoints in page window may not work wen PPAGE&amp;lt;$20, so you may need to load $8000 to page $20 and setup PPAGE=$20 soon after reset.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Dec 2010 13:00:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Programming-multiple-ppages-MC9S12DP512/m-p/166193#M5402</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-12-01T13:00:28Z</dc:date>
    </item>
    <item>
      <title>Re: Programming multiple ppages MC9S12DP512</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Programming-multiple-ppages-MC9S12DP512/m-p/166194#M5403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I deeply appreciate the org $4000 clue by kef. However, it took some work to flesh out the details. This note may help&lt;BR /&gt;others with a similar problem. All the unpaged org $4000 and org $C000 code, along with the vector table additions,&lt;BR /&gt;can be converted together by SRecCvt-Gui with settings input=banked, output=linear and then downloaded to Flash with&lt;BR /&gt;the Serial BootLoader. Other paged code, like $22, need the "Linear $4000-$FFFF to paged" box checked in SRecCvt-Gui&lt;BR /&gt;and downloaded with BDM POD using LOAD or FLOAD and the proper offset. Conversion of paged .S19 files with SRecCvt-Gui generates S2 addresses = 80000. On loading, an offset must be added to place the code in the proper linear address range in memory. Example, 80000 + offset 54000 =&amp;nbsp; linear address $D4000 for page $35.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Dec 2010 21:53:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Programming-multiple-ppages-MC9S12DP512/m-p/166194#M5403</guid>
      <dc:creator>astro_goto</dc:creator>
      <dc:date>2010-12-08T21:53:26Z</dc:date>
    </item>
  </channel>
</rss>