<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: ECLK or two crystals in the same PCB</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ECLK-or-two-crystals-in-the-same-PCB/m-p/161424#M5079</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Thank you for your response Mac! I'ts very helpful.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I think I'm going to&amp;nbsp;use two separate crystals, temporaly in prototype. Then I will choose FEE mode.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Hernán&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Jun 2008 22:23:28 GMT</pubDate>
    <dc:creator>arcano</dc:creator>
    <dc:date>2008-06-06T22:23:28Z</dc:date>
    <item>
      <title>ECLK or two crystals in the same PCB</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ECLK-or-two-crystals-in-the-same-PCB/m-p/161422#M5077</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Hello everyone.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a project, using two MCU: MC9S12UF32 and MC9S08AW60. I need to make them work at full bus frequency: 30MHz and 20MHZ respectively.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I could use MC9S08 internal self-clocked source but I need high clock accuracy.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can I use two oscillator crystals of 12MHz and 4 MHz in the same PCB without inducting noise?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Or I can use the ECLK signal, in expanded mode, to drive the 8-bit MCU? If I do so, could I use 9S12 ECLK at 30MHz or 20MHz, driving 9S08 MCU in EXTAL pin at 15MHz or 20MHz bus frequency respectively?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I want also to use external memory, at full speed (30MHz bus frequency) if I can.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What do you recomend?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Hernán Acosta&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jun 2008 08:15:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ECLK-or-two-crystals-in-the-same-PCB/m-p/161422#M5077</guid>
      <dc:creator>arcano</dc:creator>
      <dc:date>2008-06-04T08:15:19Z</dc:date>
    </item>
    <item>
      <title>Re: ECLK or two crystals in the same PCB</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ECLK-or-two-crystals-in-the-same-PCB/m-p/161423#M5078</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello Herman,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;There shouldn't be a problem using two separate crystals, one for each MCU.&amp;nbsp; However, if you wish that the HCS12 provide a clock source for the HCS08 device, keep in mind the following -&lt;/DIV&gt;&lt;OL&gt;&lt;LI&gt;If you intend using FEE mode for the HCS08, the external frequency must not exceed 10MHz.&lt;/LI&gt;&lt;LI&gt;If you use FBE mode (bypassing the FLL), the applied frequency has a maximum limit of 40MHz, but the maximum bus frequency would only be one half this frequency.&lt;/LI&gt;&lt;/OL&gt;&lt;DIV&gt;It would also be possible for the AW60 device to output a clock signal, via the MCLK pin, potentially to drive the HCS12 device.&amp;nbsp; The maximum output frequency would be fbus/2.&amp;nbsp; However, there might be an issue (for the HCS12)&amp;nbsp;with the amount of jitter associated with the FLL signal.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jun 2008 11:51:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ECLK-or-two-crystals-in-the-same-PCB/m-p/161423#M5078</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-06-04T11:51:16Z</dc:date>
    </item>
    <item>
      <title>Re: ECLK or two crystals in the same PCB</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ECLK-or-two-crystals-in-the-same-PCB/m-p/161424#M5079</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Thank you for your response Mac! I'ts very helpful.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I think I'm going to&amp;nbsp;use two separate crystals, temporaly in prototype. Then I will choose FEE mode.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Hernán&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jun 2008 22:23:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ECLK-or-two-crystals-in-the-same-PCB/m-p/161424#M5079</guid>
      <dc:creator>arcano</dc:creator>
      <dc:date>2008-06-06T22:23:28Z</dc:date>
    </item>
  </channel>
</rss>