<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: deom9s12x board</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/deom9s12x-board/m-p/161374#M5071</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;those are debugger issues. did you plug the usb on the port provided in that evboard or are you using another debugger? if you're using softec, you should click on &amp;gt;inDart-HCs12 &amp;gt; EVBs12xep.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Nov 2010 21:18:50 GMT</pubDate>
    <dc:creator>Xbot</dc:creator>
    <dc:date>2010-11-08T21:18:50Z</dc:date>
    <item>
      <title>deom9s12x board</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/deom9s12x-board/m-p/161373#M5070</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I get the following error message(s) when I execute the sample LED project on the setup disk:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The following access path in target "P&amp;amp;E ICD" of project "DEMO9S12XDT512_LED.mcp" cannot be found:&lt;BR /&gt;{Project}prm&lt;BR /&gt;&lt;BR /&gt;The following access path in target "P&amp;amp;E ICD" of project "DEMO9S12XDT512_LED.mcp" cannot be found:&lt;BR /&gt;{Project}cmd&lt;BR /&gt;&lt;BR /&gt;The following access path in target "P&amp;amp;E ICD" of project "DEMO9S12XDT512_LED.mcp" cannot be found:&lt;BR /&gt;{Project}Sources&lt;BR /&gt;&lt;BR /&gt;The following access path in target "SofTec" of project "DEMO9S12XDT512_LED.mcp" cannot be found:&lt;BR /&gt;{Project}prm&lt;BR /&gt;&lt;BR /&gt;The following access path in target "SofTec" of project "DEMO9S12XDT512_LED.mcp" cannot be found:&lt;BR /&gt;{Project}cmd&lt;BR /&gt;&lt;BR /&gt;The following access path in target "SofTec" of project "DEMO9S12XDT512_LED.mcp" cannot be found:&lt;BR /&gt;{Project}Sources&lt;BR /&gt;&lt;BR /&gt;The following access path in target "Simulator" of project "DEMO9S12XDT512_LED.mcp" cannot be found:&lt;BR /&gt;{Project}prm&lt;BR /&gt;&lt;BR /&gt;The following access path in target "Simulator" of project "DEMO9S12XDT512_LED.mcp" cannot be found:&lt;BR /&gt;{Project}cmd&lt;BR /&gt;&lt;BR /&gt;The following access path in target "Simulator" of project "DEMO9S12XDT512_LED.mcp" cannot be found:&lt;BR /&gt;{Project}Sources&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I try to open these files I get a file does not exist error in code warrior.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I fix this problem?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Nov 2010 15:09:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/deom9s12x-board/m-p/161373#M5070</guid>
      <dc:creator>John580903</dc:creator>
      <dc:date>2010-11-08T15:09:47Z</dc:date>
    </item>
    <item>
      <title>Re: deom9s12x board</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/deom9s12x-board/m-p/161374#M5071</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;those are debugger issues. did you plug the usb on the port provided in that evboard or are you using another debugger? if you're using softec, you should click on &amp;gt;inDart-HCs12 &amp;gt; EVBs12xep.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Nov 2010 21:18:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/deom9s12x-board/m-p/161374#M5071</guid>
      <dc:creator>Xbot</dc:creator>
      <dc:date>2010-11-08T21:18:50Z</dc:date>
    </item>
    <item>
      <title>Re: deom9s12x board</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/deom9s12x-board/m-p/161375#M5072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using CodeWarrior V5.1 connected to&amp;nbsp; a demo9s12xdt512 board through a USB port.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wrote some code to only change LED1 with SW1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to download it to the target, but now it says the P&amp;amp;E Multilink is not responding.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The original code the part was shipped with turned LEDs 1 &amp;amp;2 with SW1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But now, there is no response.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Nov 2010 22:25:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/deom9s12x-board/m-p/161375#M5072</guid>
      <dc:creator>John580903</dc:creator>
      <dc:date>2010-11-08T22:25:02Z</dc:date>
    </item>
    <item>
      <title>Re: deom9s12x board</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/deom9s12x-board/m-p/161376#M5073</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As the previous poster noted, the built-in USB BDM interface is "Softec" not P&amp;amp;E.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So if you are trying to use the P&amp;amp;E build target with the built-in USB connection IT WILL NOT WORK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;James&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Nov 2010 21:53:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/deom9s12x-board/m-p/161376#M5073</guid>
      <dc:creator>jsmcortina</dc:creator>
      <dc:date>2010-11-25T21:53:41Z</dc:date>
    </item>
    <item>
      <title>Re: deom9s12x board</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/deom9s12x-board/m-p/161377#M5074</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it a new version of DEMO9S12XDT512 board? Because my DEMO9S12XDT512 board has builtin P&amp;amp;E Multilink, not Softec.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Nov 2010 22:26:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/deom9s12x-board/m-p/161377#M5074</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-11-25T22:26:51Z</dc:date>
    </item>
  </channel>
</rss>