<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S12XD document for EEprom programming (S12EETX4KV0) in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XD-document-for-EEprom-programming-S12EETX4KV0/m-p/155926#M4687</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;This may be obvious to some of you, but I can't understand the timing setting of the second example on page 25, using Figure 4-1. The osc. clk is 16 MHz and the Bus clk is 40 Mhz (Tbus=0.025 usec). I get EDIV[5:0]=10 and they get EDIV[5:0]=50. And if I used an osc. clk of 15 MHz, I would get and EDIV[5:0]=5. Where am I going wrong?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Oct 2007 13:14:42 GMT</pubDate>
    <dc:creator>Bee</dc:creator>
    <dc:date>2007-10-17T13:14:42Z</dc:date>
    <item>
      <title>S12XD document for EEprom programming (S12EETX4KV0)</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XD-document-for-EEprom-programming-S12EETX4KV0/m-p/155926#M4687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;This may be obvious to some of you, but I can't understand the timing setting of the second example on page 25, using Figure 4-1. The osc. clk is 16 MHz and the Bus clk is 40 Mhz (Tbus=0.025 usec). I get EDIV[5:0]=10 and they get EDIV[5:0]=50. And if I used an osc. clk of 15 MHz, I would get and EDIV[5:0]=5. Where am I going wrong?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2007 13:14:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XD-document-for-EEprom-programming-S12EETX4KV0/m-p/155926#M4687</guid>
      <dc:creator>Bee</dc:creator>
      <dc:date>2007-10-17T13:14:42Z</dc:date>
    </item>
    <item>
      <title>Re: S12XD document for EEprom programming (S12EETX4KV0)</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XD-document-for-EEprom-programming-S12EETX4KV0/m-p/155927#M4688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Who are "they"? I quote the EEPROM datasheet:&lt;BR /&gt;&lt;BR /&gt;"If the oscillator clock frequency is 16 MHz and the bus clock frequency is 40 MHz, ECLKDIV bits EDIV[5:0] should be set to 0x0A (001010) and bit PRDIV8 set to 1."&lt;BR /&gt;&lt;BR /&gt;You calculation for 15MHz seems to be wrong though, you should get the value INT(9.42) = 9.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2007 13:57:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XD-document-for-EEprom-programming-S12EETX4KV0/m-p/155927#M4688</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2007-10-17T13:57:34Z</dc:date>
    </item>
    <item>
      <title>Re: S12XD document for EEprom programming (S12EETX4KV0)</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XD-document-for-EEprom-programming-S12EETX4KV0/m-p/155928#M4689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks for your reply. "They" are the writers of the EEprom document (S12EETX4KV0). Apparently we have different versions. Even my Flash programming document has the same example:&lt;BR /&gt;"If the oscillator clock frequency is 16MHz and the bus clock frequency is 40MHz, FCLKDIV bits FDIV[5:0] should be set to "50" (110010) and bit PRDIV8 set to "1". The resulting FCLK frequency is then 182kHz."&lt;BR /&gt;&lt;BR /&gt;So the document must have been corrected and I am out of date.&lt;BR /&gt;&lt;BR /&gt;Thank you also for correcting my 15 MHz example.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2007 21:29:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XD-document-for-EEprom-programming-S12EETX4KV0/m-p/155928#M4689</guid>
      <dc:creator>Bee</dc:creator>
      <dc:date>2007-10-17T21:29:21Z</dc:date>
    </item>
  </channel>
</rss>