<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: problem in interfacing HCS12 with 74HC595 shift register</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-in-interfacing-HCS12-with-74HC595-shift-register/m-p/155598#M4678</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sary,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;First, let's confirm the hardware connections you are using.&amp;nbsp; The code would be based on the following 'HC595 pins:&lt;/P&gt;&lt;P&gt;Pin 14 (device 1 only) = CPU_LED_DATA&lt;/P&gt;&lt;P&gt;Pin 13 (all devices) = CPU_LED_ENABLE&lt;/P&gt;&lt;P&gt;Pin 12 (all devices) = CPU_LED_LATCH&lt;/P&gt;&lt;P&gt;Pin 11 (all devices) = CPU_LED_SRCLK&lt;/P&gt;&lt;P&gt;Pin 10 (all devices) = tied to Vdd&lt;/P&gt;&lt;P&gt;Pin 9 (device 1) -&amp;gt; Pin 14 (device 2)&lt;/P&gt;&lt;P&gt;Pin 9 (device 2) -&amp;gt; Pin 14 (device 3)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On power-up, the shift register and latches&amp;nbsp;may have arbitrary output state, so you will need to initialise by pulsing pin10 (SCLR) low, and then strobing pin 12 (RCK) to zero the output latches.&amp;nbsp; Alternatively, you might simply update the LEDs in the normal way, using a value of 0x000000, which should also zero the output latches (and presumably turn all LEDs off).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now I am assuming that the LEDs states are not changing as the data is serial shifted into the register, but change only as a result of&amp;nbsp;a positive transition of the CPU_LED_ LATCH signal, after the data shifting is complete.&amp;nbsp; The code does rely on the fact that the RCK pin is edge triggered, and would require some modification for transparent latch type.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Oct 2010 21:54:30 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2010-10-19T21:54:30Z</dc:date>
    <item>
      <title>problem in interfacing HCS12 with 74HC595 shift register</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-in-interfacing-HCS12-with-74HC595-shift-register/m-p/155595#M4675</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi everyone&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I have interfaced &lt;STRONG&gt;MC9S12XHZ512 controller with three 74hc595 IC(shift register)&lt;/STRONG&gt; to glow multiple LED from Single data input&lt;/P&gt;&lt;P&gt;The code for driving the led is somewhat like&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;SPAN style="color: #ff0000;"&gt;CPU_LED_LATCH =0;&lt;BR /&gt;&amp;nbsp; CPU_LED_ENABLE = 0;&lt;BR /&gt;ulVal is the input to drive any LED.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;ucShiftValue = (ulVal &amp;gt;&amp;gt; 16) &amp;amp; 0xff;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;uci=8;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;while (uci &amp;gt; 0)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;CPU_LED_SRCLK=0;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; if((ucShiftValue &amp;amp; 0x80)==0x80)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp; &amp;nbsp;CPU_LED_DATA=1;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; else&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CPU_LED_DATA=0;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CPU_LED_SRCLK = 1;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;ucShiftValue = ucShiftValue &amp;lt;&amp;lt; 1;&amp;nbsp;&amp;nbsp; &amp;nbsp;// Shift left or one bit&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uci--;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;ucShiftValue = (ulVal &amp;gt;&amp;gt; 8) &amp;amp; 0xff;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uci=8;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;while (uci &amp;gt; 0)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;{&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;CPU_LED_SRCLK=0;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; if((ucShiftValue &amp;amp; 0x80)==0x80)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;CPU_LED_DATA=1;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; else &amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CPU_LED_DATA=0;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CPU_LED_SRCLK = 1;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ucShiftValue = ucShiftValue &amp;lt;&amp;lt; 1;&amp;nbsp;&amp;nbsp; &amp;nbsp;// Shift left or one bit&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uci--;&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;ucShiftValue = ulVal &amp;amp; 0xff;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uci=8;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;while (uci &amp;gt; 0)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;CPU_LED_SRCLK=0;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp; if((ucShiftValue &amp;amp; 0x80)==0x80)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;CPU_LED_DATA=1;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; else &amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CPU_LED_DATA=0;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp; CPU_LED_SRCLK = 1;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;ucShiftValue = ucShiftValue &amp;lt;&amp;lt; 1;&amp;nbsp;&amp;nbsp; &amp;nbsp;// Shift left or one bit&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uci--;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CPU_LED_LATCH=1;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;The problem is the that when I am setting single LED on. I am getting fluctuating output on other LEDs also&lt;/STRONG&gt;.say if in above code ulVal=1;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I will get constant o/p on first LED and it is correct.But I am getting fluctuations on other LEDs as well.&lt;/P&gt;&lt;P&gt;DOes anyone know what is the problem ?n &lt;STRONG&gt;how can I get single LED on at at ime with no fluctions on other LEDs.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;SARY&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Oct 2010 19:06:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-in-interfacing-HCS12-with-74HC595-shift-register/m-p/155595#M4675</guid>
      <dc:creator>SARY</dc:creator>
      <dc:date>2010-10-15T19:06:15Z</dc:date>
    </item>
    <item>
      <title>Re: problem in interfacing HCS12 with 74HC595 shift register</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-in-interfacing-HCS12-with-74HC595-shift-register/m-p/155596#M4676</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sary,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I assume that you have a "daisy chain" connection for the three shift registers.&amp;nbsp; However, I cannot see a reason for your code being problematic,&amp;nbsp;but I can see where a significant simplification can&amp;nbsp;be made to the code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since you are "bit banging" the serial interface, there is no reason why all 24 bits cannot be sequentially shifted within a single loop, rather than handling as three separate bytes.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;void LED_update( unsigned long ulval)(   unsigned char uci;      CPU_LED_ENABLE = 0;  // Enable output to LEDs   CPU_LED_LATCH = 0;      for (uci = 0; uci &amp;lt; 24; uci++) {      CPU_LED_SRCLK = 0;      if (ulval &amp;amp; 0x800000)         CPU_LED_DATA = 1;      else         CPU_LED_DATA = 0;           ulval &amp;lt;&amp;lt;= 1;      CPU_LED_SRCLK = 1;    // Shift serial data into register   }      CPU_LED_LATCH = 1;  // Strobe data to output latch}
&lt;/PRE&gt;&lt;P&gt;Perhaps you&amp;nbsp;might also&amp;nbsp;confirm the operation of the various bit manipulation macros.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 08:59:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-in-interfacing-HCS12-with-74HC595-shift-register/m-p/155596#M4676</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2020-10-29T08:59:28Z</dc:date>
    </item>
    <item>
      <title>Re: problem in interfacing HCS12 with 74HC595 shift register</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-in-interfacing-HCS12-with-74HC595-shift-register/m-p/155597#M4677</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;thanks for the suggestion.I have changed the code it is working fine but the issue remains the same.with this also,all leds lit when i am setting single LED .I think that is some hadware issue,becoz this problem comes for the first time. But when I switch off&amp;nbsp; and starts again,it works fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Oct 2010 16:52:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-in-interfacing-HCS12-with-74HC595-shift-register/m-p/155597#M4677</guid>
      <dc:creator>SARY</dc:creator>
      <dc:date>2010-10-18T16:52:00Z</dc:date>
    </item>
    <item>
      <title>Re: problem in interfacing HCS12 with 74HC595 shift register</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-in-interfacing-HCS12-with-74HC595-shift-register/m-p/155598#M4678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sary,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;First, let's confirm the hardware connections you are using.&amp;nbsp; The code would be based on the following 'HC595 pins:&lt;/P&gt;&lt;P&gt;Pin 14 (device 1 only) = CPU_LED_DATA&lt;/P&gt;&lt;P&gt;Pin 13 (all devices) = CPU_LED_ENABLE&lt;/P&gt;&lt;P&gt;Pin 12 (all devices) = CPU_LED_LATCH&lt;/P&gt;&lt;P&gt;Pin 11 (all devices) = CPU_LED_SRCLK&lt;/P&gt;&lt;P&gt;Pin 10 (all devices) = tied to Vdd&lt;/P&gt;&lt;P&gt;Pin 9 (device 1) -&amp;gt; Pin 14 (device 2)&lt;/P&gt;&lt;P&gt;Pin 9 (device 2) -&amp;gt; Pin 14 (device 3)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On power-up, the shift register and latches&amp;nbsp;may have arbitrary output state, so you will need to initialise by pulsing pin10 (SCLR) low, and then strobing pin 12 (RCK) to zero the output latches.&amp;nbsp; Alternatively, you might simply update the LEDs in the normal way, using a value of 0x000000, which should also zero the output latches (and presumably turn all LEDs off).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now I am assuming that the LEDs states are not changing as the data is serial shifted into the register, but change only as a result of&amp;nbsp;a positive transition of the CPU_LED_ LATCH signal, after the data shifting is complete.&amp;nbsp; The code does rely on the fact that the RCK pin is edge triggered, and would require some modification for transparent latch type.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Oct 2010 21:54:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-in-interfacing-HCS12-with-74HC595-shift-register/m-p/155598#M4678</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-10-19T21:54:30Z</dc:date>
    </item>
    <item>
      <title>Re: problem in interfacing HCS12 with 74HC595 shift register</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-in-interfacing-HCS12-with-74HC595-shift-register/m-p/155599#M4679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;&amp;nbsp; sorry for the late reply. i have made the same coonections as you said. I think the problem is due to master reset. i have made it permanently high .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I think you are right i need to set it low first and then high to remove the flickering.&lt;/P&gt;&lt;P&gt;i willcheck this out and let u know.&lt;/P&gt;&lt;P&gt;thanks again.&lt;/P&gt;&lt;P&gt;SARY&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Oct 2010 12:53:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/problem-in-interfacing-HCS12-with-74HC595-shift-register/m-p/155599#M4679</guid>
      <dc:creator>SARY</dc:creator>
      <dc:date>2010-10-26T12:53:53Z</dc:date>
    </item>
  </channel>
</rss>