<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Easy Pulse Accumulator Question in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Easy-Pulse-Accumulator-Question/m-p/155479#M4658</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can't seem to find any documentation/code that shows to use any of the 8-bit pulse accumulators to generate an interrupt after X number of pulses have been recieved.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I see ICPAR is used to enable 8-bit pulse accumulators, but I dont see anything on how to set interrupts after X number of edges have passed.&amp;nbsp; Are there no such controlls? Does it just generate an interrupt after it overflows(255) meaning I have to avance the count in software to get it to interrupt after a specifeid number of edges have passed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any input would be grately appreicated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Feb 2009 06:22:38 GMT</pubDate>
    <dc:creator>seank</dc:creator>
    <dc:date>2009-02-24T06:22:38Z</dc:date>
    <item>
      <title>Easy Pulse Accumulator Question</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Easy-Pulse-Accumulator-Question/m-p/155479#M4658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can't seem to find any documentation/code that shows to use any of the 8-bit pulse accumulators to generate an interrupt after X number of pulses have been recieved.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I see ICPAR is used to enable 8-bit pulse accumulators, but I dont see anything on how to set interrupts after X number of edges have passed.&amp;nbsp; Are there no such controlls? Does it just generate an interrupt after it overflows(255) meaning I have to avance the count in software to get it to interrupt after a specifeid number of edges have passed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any input would be grately appreicated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Feb 2009 06:22:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Easy-Pulse-Accumulator-Question/m-p/155479#M4658</guid>
      <dc:creator>seank</dc:creator>
      <dc:date>2009-02-24T06:22:38Z</dc:date>
    </item>
    <item>
      <title>Re: Easy Pulse Accumulator Question</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Easy-Pulse-Accumulator-Question/m-p/155480#M4659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Yes, you either interrupt on every pulse, or when accumulator overflows.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Feb 2009 12:41:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Easy-Pulse-Accumulator-Question/m-p/155480#M4659</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2009-02-24T12:41:21Z</dc:date>
    </item>
  </channel>
</rss>