<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: HCS12C32 SCI inferface with GPS Module</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HCS12C32-SCI-inferface-with-GPS-Module/m-p/152058#M4396</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks for the reply.&lt;BR /&gt;&lt;BR /&gt;I have tried running the C32 at 3.5V but I still suffer from the same problem where the pulses appear 'on top' of a constant voltage when the SCI RX is connected. It is like the GPS module cannot pull the line down to 0V.&lt;BR /&gt;&lt;BR /&gt;Do you understand what I mean? I will try and get some pictures tomorrow.&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;&lt;BR /&gt;Colin&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Feb 2009 03:39:12 GMT</pubDate>
    <dc:creator>Deadstar</dc:creator>
    <dc:date>2009-02-13T03:39:12Z</dc:date>
    <item>
      <title>HCS12C32 SCI inferface with GPS Module</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HCS12C32-SCI-inferface-with-GPS-Module/m-p/152056#M4394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am interfacing with a GPS module which requires a LVTTL, 4800 baud, no parity, one stop bit signal. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LVTTL level is 0-3.5V. I have two questions:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;First, do I need to boost this voltage range to 0-5V to interface.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;A problem I have is that when I connect the Tx of the GPS module to the SCI Rx on the C32, the output jumps from pulses between 0-3.5V to a steady 4V with the pulses with a peak to peak of about 400mV on top of this. Do I need some sort of circuitry to correct this?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Colin&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Feb 2009 02:23:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HCS12C32-SCI-inferface-with-GPS-Module/m-p/152056#M4394</guid>
      <dc:creator>Deadstar</dc:creator>
      <dc:date>2009-02-12T02:23:33Z</dc:date>
    </item>
    <item>
      <title>Re: HCS12C32 SCI inferface with GPS Module</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HCS12C32-SCI-inferface-with-GPS-Module/m-p/152057#M4395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;P&gt;Colin, the 9S12C32 is capable of operating at 3.3V, so if you could do that, it would solve your problem.&amp;nbsp; Otherwise, you'll likely need some sort of level-translation circuit.&amp;nbsp; It could be as simple as a transistor plus a couple of resistors...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Carl Barnes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Feb 2009 23:00:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HCS12C32-SCI-inferface-with-GPS-Module/m-p/152057#M4395</guid>
      <dc:creator>mculater</dc:creator>
      <dc:date>2009-02-12T23:00:36Z</dc:date>
    </item>
    <item>
      <title>Re: HCS12C32 SCI inferface with GPS Module</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HCS12C32-SCI-inferface-with-GPS-Module/m-p/152058#M4396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks for the reply.&lt;BR /&gt;&lt;BR /&gt;I have tried running the C32 at 3.5V but I still suffer from the same problem where the pulses appear 'on top' of a constant voltage when the SCI RX is connected. It is like the GPS module cannot pull the line down to 0V.&lt;BR /&gt;&lt;BR /&gt;Do you understand what I mean? I will try and get some pictures tomorrow.&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;&lt;BR /&gt;Colin&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Feb 2009 03:39:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HCS12C32-SCI-inferface-with-GPS-Module/m-p/152058#M4396</guid>
      <dc:creator>Deadstar</dc:creator>
      <dc:date>2009-02-13T03:39:12Z</dc:date>
    </item>
    <item>
      <title>Re: HCS12C32 SCI inferface with GPS Module</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HCS12C32-SCI-inferface-with-GPS-Module/m-p/152059#M4397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello Colin,&lt;BR /&gt;&lt;BR /&gt;Is there any possibility that there is an external pull-up resistor on the MCU pin?&amp;nbsp; If so, the symptoms would indicate that it may be substantially too low in value, perhaps a component error on the board.&lt;BR /&gt;&lt;BR /&gt;What level of sink current can the GPS unit provide at its output pin?&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mac&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Feb 2009 09:20:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HCS12C32-SCI-inferface-with-GPS-Module/m-p/152059#M4397</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2009-02-13T09:20:09Z</dc:date>
    </item>
    <item>
      <title>Re: HCS12C32 SCI inferface with GPS Module</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HCS12C32-SCI-inferface-with-GPS-Module/m-p/152060#M4398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Mac,&lt;BR /&gt;&lt;BR /&gt;Thanks for the advice. I cut the traces between the MCU and the on-board DB9 connector and voila it works. &lt;BR /&gt;&lt;BR /&gt;Thanks a lot; these solutions always seem simple one you know about them.&lt;BR /&gt;&lt;BR /&gt;Colin&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Feb 2009 20:22:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HCS12C32-SCI-inferface-with-GPS-Module/m-p/152060#M4398</guid>
      <dc:creator>Deadstar</dc:creator>
      <dc:date>2009-02-13T20:22:00Z</dc:date>
    </item>
  </channel>
</rss>