<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: differences between spi on mc9s256a and mc9s256cfu ? in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/differences-between-spi-on-mc9s256a-and-mc9s256cfu/m-p/150411#M4238</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I assumed he ment porting from S12A to S12C since those are similar. Regardless, the advise is still to check the erratas for the earlier masks since that's the only difference.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Oct 2007 13:28:52 GMT</pubDate>
    <dc:creator>Lundin</dc:creator>
    <dc:date>2007-10-04T13:28:52Z</dc:date>
    <item>
      <title>differences between spi on mc9s256a and mc9s256cfu ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/differences-between-spi-on-mc9s256a-and-mc9s256cfu/m-p/150405#M4232</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;the problem began when the mc9s256a (bat wing logo) was discontuined and i started using the mc9s256cfu part (new freescale logo). i have cpu's running on a single spi bus. all cpu are slaves except when changed to master to speek to other cpu's. this is a polled system with each cpu addressed. the only way i can get the mc9s256cfu to receive data is to invert both cpol and cpha when setting up slave. in testing i install 256a and it works, same board with 256cfu and will not work. then i clear cpol, and cpha bits and the 256cfu then works. no other changes are made to the other cpu's on the buss.&lt;/DIV&gt;&lt;DIV&gt;thanks&lt;/DIV&gt;&lt;DIV&gt;joe&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Sep 2007 22:24:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/differences-between-spi-on-mc9s256a-and-mc9s256cfu/m-p/150405#M4232</guid>
      <dc:creator>joegibson</dc:creator>
      <dc:date>2007-09-26T22:24:03Z</dc:date>
    </item>
    <item>
      <title>Re: differences between spi on mc9s256a and mc9s256cfu ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/differences-between-spi-on-mc9s256a-and-mc9s256cfu/m-p/150406#M4233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I would suspect that the early chips in the A family had silicon bugs that the C family is missing. I think there was an errata related to the SPI flags in the early masks, I would take a closer look at those.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2007 13:18:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/differences-between-spi-on-mc9s256a-and-mc9s256cfu/m-p/150406#M4233</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2007-09-27T13:18:31Z</dc:date>
    </item>
    <item>
      <title>Re: differences between spi on mc9s256a and mc9s256cfu ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/differences-between-spi-on-mc9s256a-and-mc9s256cfu/m-p/150407#M4234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Thanks Lundin, I will do that.&lt;/DIV&gt;&lt;DIV&gt;joe&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2007 20:04:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/differences-between-spi-on-mc9s256a-and-mc9s256cfu/m-p/150407#M4234</guid>
      <dc:creator>joegibson</dc:creator>
      <dc:date>2007-09-27T20:04:00Z</dc:date>
    </item>
    <item>
      <title>Re: differences between spi on mc9s256a and mc9s256cfu ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/differences-between-spi-on-mc9s256a-and-mc9s256cfu/m-p/150408#M4235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Difficult to comment as these references do not exist.&lt;BR /&gt;&lt;BR /&gt;CFU means Commercial temperature and FU stands for the package (80QFP).&lt;BR /&gt;256 probably means 256KB of flash memory.&lt;BR /&gt;MC9S is not enough to determine a family.&lt;BR /&gt;&lt;BR /&gt;As no S08 has a that big flash yet, we can only think about 1 &lt;U&gt;large&lt;/U&gt; family of products: S12.&lt;BR /&gt;Still letters are missing:&lt;BR /&gt;MC9S12&lt;B&gt;??&lt;/B&gt;256CFU&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Alban.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2007 20:34:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/differences-between-spi-on-mc9s256a-and-mc9s256cfu/m-p/150408#M4235</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-09-27T20:34:27Z</dc:date>
    </item>
    <item>
      <title>Re: differences between spi on mc9s256a and mc9s256cfu ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/differences-between-spi-on-mc9s256a-and-mc9s256cfu/m-p/150409#M4236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;part # MC9S12A256BCFU (OLD PART)&amp;nbsp;AND MC9S12A256CFUE (NEW PART)&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Sep 2007 04:33:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/differences-between-spi-on-mc9s256a-and-mc9s256cfu/m-p/150409#M4236</guid>
      <dc:creator>joegibson</dc:creator>
      <dc:date>2007-09-28T04:33:51Z</dc:date>
    </item>
    <item>
      <title>Re: differences between spi on mc9s12a256 and mc9s12a256E ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/differences-between-spi-on-mc9s256a-and-mc9s256cfu/m-p/150410#M4237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hello Joe,&lt;BR /&gt;&lt;BR /&gt;The difference, the "E", here means that the new part is lead free / RoHS compliant.&lt;BR /&gt;&lt;BR /&gt;For you to read the Mask Set Errata sheet (MSE), you can look into keyword search for the mask set.&lt;BR /&gt;Mask is written underneath the part number and is formatted: &lt;BR /&gt;&lt;BR /&gt;0X00X&lt;BR /&gt;with 0 a digit between 0 and 9.&lt;BR /&gt;with X a letter between A and Z&lt;BR /&gt;&lt;BR /&gt;&lt;B&gt;EDIT&lt;/B&gt;: I was pinpointed to the "B" in the part you had before and I just didn't see.&lt;BR /&gt;This means this part has older flash generation (see datasheet for actual numbers) and probably other module enhancements.&lt;BR /&gt;There are quite a few posts on here about the SPI and they could be of great help to you ?&lt;BR /&gt;&lt;BR /&gt;Alban.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by Alban on &lt;SPAN class="date_text"&gt;2007-09-28&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;11:47 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Sep 2007 13:50:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/differences-between-spi-on-mc9s256a-and-mc9s256cfu/m-p/150410#M4237</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-09-28T13:50:30Z</dc:date>
    </item>
    <item>
      <title>Re: differences between spi on mc9s256a and mc9s256cfu ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/differences-between-spi-on-mc9s256a-and-mc9s256cfu/m-p/150411#M4238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I assumed he ment porting from S12A to S12C since those are similar. Regardless, the advise is still to check the erratas for the earlier masks since that's the only difference.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Oct 2007 13:28:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/differences-between-spi-on-mc9s256a-and-mc9s256cfu/m-p/150411#M4238</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2007-10-04T13:28:52Z</dc:date>
    </item>
  </channel>
</rss>