<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 SCI Problem: Rx-Tx</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/SCI-Problem-Rx-Tx/m-p/125732#M423</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello Forum!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am trying to develop a program related to SCI.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using Codewarrior IDE. Target is P&amp;amp;E Multilink CyclonePro. I have a MC9S12XDT256-based development board. For debugging (using BDM), I use WinIdea2006 (ic3000HS emulator).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The logic I try to implement is as follows: A tester keeps on sending a sequence of bytes to the controller over SCI1 at 4800 baud. On receiving &amp;amp; recognising the correct pattern, the controller sends back an acknowledge at the same baud. On receiving the acknowkledgement from the controller, the tester stops sending the start/wake-up pattern &amp;amp; actual communication starts. SCI1 is given to K-Line. This means that the communication is finally through K-Line.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The tester is working fine. I receive the start pattern in the controller. Then I send the ack. byte.I put the byte on SCI1DRL after reading SCI1SR1 while TDRE is asserted.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Till reception, everything is fine. Once I send the data, the Tx interrupt takes really long time &amp;amp; COP-service triggers a reset. My loop time is 10ms &amp;amp; COP reaction time is around 52ms.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Also I see that the tester keeps on sending the wakeup sequence even after I send the ack. byte from the controller. This means that the tester is not receiving what I am sending.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any help on what might be going wrong with the Tx will be highly appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;With warm regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Saurav&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Mar 2007 22:57:14 GMT</pubDate>
    <dc:creator>saurav</dc:creator>
    <dc:date>2007-03-09T22:57:14Z</dc:date>
    <item>
      <title>SCI Problem: Rx-Tx</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/SCI-Problem-Rx-Tx/m-p/125732#M423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello Forum!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am trying to develop a program related to SCI.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using Codewarrior IDE. Target is P&amp;amp;E Multilink CyclonePro. I have a MC9S12XDT256-based development board. For debugging (using BDM), I use WinIdea2006 (ic3000HS emulator).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The logic I try to implement is as follows: A tester keeps on sending a sequence of bytes to the controller over SCI1 at 4800 baud. On receiving &amp;amp; recognising the correct pattern, the controller sends back an acknowledge at the same baud. On receiving the acknowkledgement from the controller, the tester stops sending the start/wake-up pattern &amp;amp; actual communication starts. SCI1 is given to K-Line. This means that the communication is finally through K-Line.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The tester is working fine. I receive the start pattern in the controller. Then I send the ack. byte.I put the byte on SCI1DRL after reading SCI1SR1 while TDRE is asserted.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Till reception, everything is fine. Once I send the data, the Tx interrupt takes really long time &amp;amp; COP-service triggers a reset. My loop time is 10ms &amp;amp; COP reaction time is around 52ms.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Also I see that the tester keeps on sending the wakeup sequence even after I send the ack. byte from the controller. This means that the tester is not receiving what I am sending.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any help on what might be going wrong with the Tx will be highly appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;With warm regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Saurav&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Mar 2007 22:57:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/SCI-Problem-Rx-Tx/m-p/125732#M423</guid>
      <dc:creator>saurav</dc:creator>
      <dc:date>2007-03-09T22:57:14Z</dc:date>
    </item>
    <item>
      <title>Re: SCI Problem: Rx-Tx</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/SCI-Problem-Rx-Tx/m-p/125733#M424</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;We designed a product using an HCS12 processor (A128B)&amp;nbsp;and had to work around an problem with the silicon- Cannot use TX and RX interrupt on one SCI channel.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Check the errata sheet for the processor you are using.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Mar 2007 21:22:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/SCI-Problem-Rx-Tx/m-p/125733#M424</guid>
      <dc:creator>YeOldeBDM</dc:creator>
      <dc:date>2007-03-12T21:22:58Z</dc:date>
    </item>
    <item>
      <title>Re: SCI Problem: Rx-Tx</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/SCI-Problem-Rx-Tx/m-p/125734#M425</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;That should only apply to the old B mask sets that are not longer made. The OP is using S12X.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Mar 2007 14:32:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/SCI-Problem-Rx-Tx/m-p/125734#M425</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2007-03-13T14:32:34Z</dc:date>
    </item>
  </channel>
</rss>