<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: One code on two different boards</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/One-code-on-two-different-boards/m-p/149838#M4201</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems you added wrong library. You have project created for small memory model and added library made for banked memory model.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(&lt;EM&gt;I think y&lt;/EM&gt;ou should copy-paste also error descriptions for L1822 and L1115, since all here are humans and not everyone remembers what are these errors)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Jul 2011 00:48:24 GMT</pubDate>
    <dc:creator>kef</dc:creator>
    <dc:date>2011-07-15T00:48:24Z</dc:date>
    <item>
      <title>One code on two different boards</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/One-code-on-two-different-boards/m-p/149837#M4200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello;&lt;/P&gt;&lt;P&gt;I used CMD-12DP512 "&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.axman.com%2F%3Fq%3Dnode%2F292" rel="nofollow" target="_blank"&gt;http://www.axman.com/?q=node/292&lt;/A&gt;" with keypad and LCD, I used AXIDE to complie it. Now I want to use the codes that I developed for this micro in another board CSMB-12C128 "&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.axman.com%2F%3Fq%3Dnode%2F327" rel="nofollow" target="_blank"&gt;http://www.axman.com/?q=node/327&lt;/A&gt;" which compiles in codewarrior although doesn't have LCD and keypad.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I created a new project and paste my code in main.asm file. There are two include files ,1- Dp256reg.asm (for all registers), 2-&amp;nbsp; LCD_SER.asm . When I compiled it, there were lots of error, I fixed them, and at the end there were two errors:&lt;/P&gt;&lt;P&gt;1- L1822, 2-L1115.&lt;/P&gt;&lt;P&gt;I add float library, to fix error L1822, but the number of errors went to 50. with two different code errors:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Link Error&amp;nbsp;&amp;nbsp; : L1401: Incompatible memory model: SMALL in previous file (Lcd_Ser.asm.o) and BANKED in file ASSERT.C.o(ansib.lib)&lt;/LI&gt;&lt;LI&gt;Link Error&amp;nbsp;&amp;nbsp; : L1301: Cannot open file C:\Program Files\Freescale\CWS12v5.1\lib\hc12c\lib\ansib.lib&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Any idea, can any body help me?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;I can give you the code for test if you have time!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2011 23:59:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/One-code-on-two-different-boards/m-p/149837#M4200</guid>
      <dc:creator>Idontunderstand</dc:creator>
      <dc:date>2011-07-14T23:59:18Z</dc:date>
    </item>
    <item>
      <title>Re: One code on two different boards</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/One-code-on-two-different-boards/m-p/149838#M4201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems you added wrong library. You have project created for small memory model and added library made for banked memory model.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(&lt;EM&gt;I think y&lt;/EM&gt;ou should copy-paste also error descriptions for L1822 and L1115, since all here are humans and not everyone remembers what are these errors)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jul 2011 00:48:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/One-code-on-two-different-boards/m-p/149838#M4201</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2011-07-15T00:48:24Z</dc:date>
    </item>
  </channel>
</rss>