<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: CPMUAPITR on s12p</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CPMUAPITR-on-s12p/m-p/149444#M4169</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Why not add the external crystal, I think this is cheaper than testing every unit at say 0 and +50degC to calibrate both internal die temperature and internal oscillator, but +/-1.5% is good enough except perhaps for 1Mbit/sec CAN.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The cost and toughness advantage of no crystal are attractive especially in hostile environments where this part excels. &amp;nbsp;Like all engineering you must balance price and performance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Fast55&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 08 Nov 2009 21:31:25 GMT</pubDate>
    <dc:creator>Fast</dc:creator>
    <dc:date>2009-11-08T21:31:25Z</dc:date>
    <item>
      <title>CPMUAPITR on s12p</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CPMUAPITR-on-s12p/m-p/149443#M4168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to determine if it is possible to use the internal clock on the s12p.&amp;nbsp; How accurate is the internal clock on the s12p when trimmed at the factory using&amp;nbsp; &lt;STRONG&gt;CPMUAPITR&lt;/STRONG&gt;?&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I guess one would have to know what the tolerance is on a typical oscillator.&amp;nbsp; If an oscillator has a frequency of 4Mhz and a tolerance of 100ppm, does this mean 4Mhz+/- .01%?&amp;nbsp; If so, the internal oscillator would have to be trimmed extremely well to be similar.&amp;nbsp; If it is similar to s08 products, the accuracy is around +/-5%.&amp;nbsp; Not good enough for my application (need .5%).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks in advance&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;sp&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 4; font-family: Arial;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Oct 2009 03:21:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CPMUAPITR-on-s12p/m-p/149443#M4168</guid>
      <dc:creator>sprince</dc:creator>
      <dc:date>2009-10-27T03:21:25Z</dc:date>
    </item>
    <item>
      <title>Re: CPMUAPITR on s12p</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CPMUAPITR-on-s12p/m-p/149444#M4169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Why not add the external crystal, I think this is cheaper than testing every unit at say 0 and +50degC to calibrate both internal die temperature and internal oscillator, but +/-1.5% is good enough except perhaps for 1Mbit/sec CAN.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The cost and toughness advantage of no crystal are attractive especially in hostile environments where this part excels. &amp;nbsp;Like all engineering you must balance price and performance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Fast55&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 08 Nov 2009 21:31:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CPMUAPITR-on-s12p/m-p/149444#M4169</guid>
      <dc:creator>Fast</dc:creator>
      <dc:date>2009-11-08T21:31:25Z</dc:date>
    </item>
  </channel>
</rss>