<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: SPI Data Register</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/SPI-Data-Register/m-p/145075#M3846</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I think you can't write to the SPI data register in simulation time. the data in this register is sent immediately, and the content of this register will retain the data that was before which is mainly 0.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Mar 2007 00:57:44 GMT</pubDate>
    <dc:creator>prog_ram</dc:creator>
    <dc:date>2007-03-06T00:57:44Z</dc:date>
    <item>
      <title>SPI Data Register</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/SPI-Data-Register/m-p/145074#M3845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;When I&amp;nbsp;try to use the SPI on the nanocore 12 i canot right to the data register in codewariores time simulator. I think that this is the reason why I cant get the SPI to Work because I cant right to The Data Register. I am configuring the SPI as A master. The slave device is a serial in parallell out shift register. Also I have no need for The SS Line when I am not using it is there some voltage leval i have to put it to or is there a setting in a register that i need to set.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Feb 2007 22:04:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/SPI-Data-Register/m-p/145074#M3845</guid>
      <dc:creator>Assembly</dc:creator>
      <dc:date>2007-02-12T22:04:02Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Data Register</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/SPI-Data-Register/m-p/145075#M3846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I think you can't write to the SPI data register in simulation time. the data in this register is sent immediately, and the content of this register will retain the data that was before which is mainly 0.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Mar 2007 00:57:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/SPI-Data-Register/m-p/145075#M3846</guid>
      <dc:creator>prog_ram</dc:creator>
      <dc:date>2007-03-06T00:57:44Z</dc:date>
    </item>
  </channel>
</rss>