<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Simultaneous sampling and the 56F8356</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Simultaneous-sampling-and-the-56F8356/m-p/143959#M3642</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The 56F8356 have two 8-channel ADC's. Each of them can be configured for simultaneous conversion. In this case ADC can capture two different channels at the&lt;BR /&gt;same time - i.e. you can run 4 conversion almost simultaneous (for both ADC). "Almost" - because first you need to run conversion one of the ADC, after that second conversion.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Jan 2007 17:20:52 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2007-01-31T17:20:52Z</dc:date>
    <item>
      <title>Simultaneous sampling and the 56F8356</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Simultaneous-sampling-and-the-56F8356/m-p/143958#M3641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am a little confused by the literature and have a simple question.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I need to sample 9 signals simultaneously. I know with 56F8356 I can convert 2 samples simultaneously, but I am having a hard time determining how many I can actually sample simultaneously.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It seems like it says only two, but this does not make much sense because I think I see 4 S/H circuits.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So I would like to know how many samples I can take simultaneously. Thank you.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Jan 2007 00:50:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Simultaneous-sampling-and-the-56F8356/m-p/143958#M3641</guid>
      <dc:creator>Charlie</dc:creator>
      <dc:date>2007-01-31T00:50:45Z</dc:date>
    </item>
    <item>
      <title>Re: Simultaneous sampling and the 56F8356</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Simultaneous-sampling-and-the-56F8356/m-p/143959#M3642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The 56F8356 have two 8-channel ADC's. Each of them can be configured for simultaneous conversion. In this case ADC can capture two different channels at the&lt;BR /&gt;same time - i.e. you can run 4 conversion almost simultaneous (for both ADC). "Almost" - because first you need to run conversion one of the ADC, after that second conversion.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Jan 2007 17:20:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Simultaneous-sampling-and-the-56F8356/m-p/143959#M3642</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2007-01-31T17:20:52Z</dc:date>
    </item>
  </channel>
</rss>