<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CANRIER/CSCIE interrupt in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CANRIER-CSCIE-interrupt/m-p/143931#M3640</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;If the CAN node is not connected to a network, nobody will acknowledge the transmission.&lt;BR /&gt;&lt;BR /&gt;When there is not ACK, a Receive Error occurs, incrementing the RX ERROR counter.&lt;BR /&gt;After a while, the module will switch to Error Passive and then Bus Off stopping all transmission.&lt;BR /&gt;&lt;BR /&gt;Chico.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Jan 2007 19:12:19 GMT</pubDate>
    <dc:creator>Nabla69</dc:creator>
    <dc:date>2007-01-30T19:12:19Z</dc:date>
    <item>
      <title>CANRIER/CSCIE interrupt</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CANRIER-CSCIE-interrupt/m-p/143930#M3639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi, am having a problem with CANRIER/CSCIE&lt;/DIV&gt;&lt;DIV&gt;when I set&lt;BR /&gt;CANRIER = 0x7F;&lt;/DIV&gt;&lt;DIV&gt;and try to transmitt to a CAN-network that is not connected, the debugger says Event Occured.&lt;BR /&gt;What should I do?&lt;BR /&gt;I have redirrected all CAN error interrupts to a xgate routine.&lt;/DIV&gt;&lt;DIV&gt;Thanks In advance&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jan 2007 19:00:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CANRIER-CSCIE-interrupt/m-p/143930#M3639</guid>
      <dc:creator>patti</dc:creator>
      <dc:date>2007-01-30T19:00:00Z</dc:date>
    </item>
    <item>
      <title>Re: CANRIER/CSCIE interrupt</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CANRIER-CSCIE-interrupt/m-p/143931#M3640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;If the CAN node is not connected to a network, nobody will acknowledge the transmission.&lt;BR /&gt;&lt;BR /&gt;When there is not ACK, a Receive Error occurs, incrementing the RX ERROR counter.&lt;BR /&gt;After a while, the module will switch to Error Passive and then Bus Off stopping all transmission.&lt;BR /&gt;&lt;BR /&gt;Chico.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jan 2007 19:12:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CANRIER-CSCIE-interrupt/m-p/143931#M3640</guid>
      <dc:creator>Nabla69</dc:creator>
      <dc:date>2007-01-30T19:12:19Z</dc:date>
    </item>
  </channel>
</rss>