<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: print debug values in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/print-debug-values/m-p/142072#M3409</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;i realized i could use printf, but the linker gives an error:&lt;BR /&gt;&lt;BR /&gt;Segment overflow: .x_internal_ROM&lt;BR /&gt;Reserved size is 0x00002000 -- Overflow 0x00000174&lt;BR /&gt;Link failed.&lt;BR /&gt;&lt;BR /&gt;is there a way i can incread this size? i'm not very familiar with codewarrior yet.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Jul 2006 21:59:01 GMT</pubDate>
    <dc:creator>makuz</dc:creator>
    <dc:date>2006-07-05T21:59:01Z</dc:date>
    <item>
      <title>print debug values</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/print-debug-values/m-p/142071#M3408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i'm a beginner trying to program the motorola 56f8300demo board using codewarrior 7.0 for freescale 56800/e hybrid controllers.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i'm trying to experiment with the demo example applications and i would like to print out the values read back from the e-field sensor of the board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i only found a way using log messages to achieve this. i put a log eventpoint after the command that reads the e-field value. the problem is that the execution becomes very slow, probably because the printing of the log messages halt the microcontroller. i also tried the data visualization of codewarrior, but it is even slower. is there any other way to do this in a more clever, faster way or this is the usual way to do it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;any help would be appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks in advance,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;gabor&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jul 2006 16:54:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/print-debug-values/m-p/142071#M3408</guid>
      <dc:creator>makuz</dc:creator>
      <dc:date>2006-07-05T16:54:24Z</dc:date>
    </item>
    <item>
      <title>Re: print debug values</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/print-debug-values/m-p/142072#M3409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;i realized i could use printf, but the linker gives an error:&lt;BR /&gt;&lt;BR /&gt;Segment overflow: .x_internal_ROM&lt;BR /&gt;Reserved size is 0x00002000 -- Overflow 0x00000174&lt;BR /&gt;Link failed.&lt;BR /&gt;&lt;BR /&gt;is there a way i can incread this size? i'm not very familiar with codewarrior yet.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jul 2006 21:59:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/print-debug-values/m-p/142072#M3409</guid>
      <dc:creator>makuz</dc:creator>
      <dc:date>2006-07-05T21:59:01Z</dc:date>
    </item>
  </channel>
</rss>