<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I/O problem with 9s12DP512 in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-O-problem-with-9s12DP512/m-p/125539#M340</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hy,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I use an 9s12DP512 to replace the 256 in a new board...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have an strange problem with the port K, specially with the PK4 pin:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;all the others pin could work in input or output...but when i try to use the PK4 oin in output it don't work...i coud just use it in input....is that normal??? or did i forget something, i haven't found sommething about it in the datasheets...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If somebody know's...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your help....&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Wish.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Mar 2007 17:04:51 GMT</pubDate>
    <dc:creator>wishmerill</dc:creator>
    <dc:date>2007-03-08T17:04:51Z</dc:date>
    <item>
      <title>I/O problem with 9s12DP512</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-O-problem-with-9s12DP512/m-p/125539#M340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hy,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I use an 9s12DP512 to replace the 256 in a new board...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have an strange problem with the port K, specially with the PK4 pin:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;all the others pin could work in input or output...but when i try to use the PK4 oin in output it don't work...i coud just use it in input....is that normal??? or did i forget something, i haven't found sommething about it in the datasheets...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If somebody know's...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your help....&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Wish.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Mar 2007 17:04:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-O-problem-with-9s12DP512/m-p/125539#M340</guid>
      <dc:creator>wishmerill</dc:creator>
      <dc:date>2007-03-08T17:04:51Z</dc:date>
    </item>
    <item>
      <title>Re: I/O problem with 9s12DP512</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-O-problem-with-9s12DP512/m-p/125540#M341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;You've looked at the datasheet for the MC9S12XDP512 (MC9S12XDP512V2.pdf), right? Odd. Looks like Port K could be set to either GPIO or extended bus mode (where PK6:0 are output), according to Chapter 22 in the datasheet, Table 22-1. But input only? Only on PK7, in the extended bus mode. It sounds like something strange might be connected to that pin.&lt;BR /&gt;&lt;BR /&gt;---Tom&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Mar 2007 23:41:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-O-problem-with-9s12DP512/m-p/125540#M341</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2007-03-08T23:41:36Z</dc:date>
    </item>
    <item>
      <title>Re: I/O problem with 9s12DP512</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-O-problem-with-9s12DP512/m-p/125541#M342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;That's right,&lt;BR /&gt;I think the same so i've deconnected this pin from the electronics and it's the same problem....i can't use PK4 as an output... the others pin work well. I don't have this problem with the 9s12dp256...i'm transfering an application from one micro to the other...&lt;BR /&gt;I'm not working in an special mode, just normal single chip mode....&lt;BR /&gt;&lt;BR /&gt;Thank's for your help&lt;BR /&gt;&lt;BR /&gt;Wish&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Mar 2007 23:53:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-O-problem-with-9s12DP512/m-p/125541#M342</guid>
      <dc:creator>wishmerill</dc:creator>
      <dc:date>2007-03-08T23:53:25Z</dc:date>
    </item>
  </channel>
</rss>